高電圧D/Aコンバータ(≧20V)
高電圧D/Aコンバータ(≧20V)
高電圧出力アンプを内蔵したアナログ・デバイセズのD/Aコンバータ製品には、シング/クワッド・チャンネルのAD5501/AD5504があり、DAC出力範囲は0V~30Vまたは0V~60Vです。AD5535は32チャンネルDACで、出力範囲は0~50Vまたは0~200Vです。
高電圧出力アンプを内蔵したアナログ・デバイセズのD/Aコンバータ製品には、シング/クワッド・チャンネルのAD5501/AD5504があり、DAC出力範囲は0V~30Vまたは0V~60Vです。AD5535は32チャンネルDACで、出力範囲は0~50Vまたは0~200Vです。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}