UART
UART
ADI公司提供先进的小尺寸SPI/I2C (I2C) UART系列产品。我们的UART系列包括单通道、双通道或四通道选项,还包括集成RS-232或RS-485收发器的UART。这些产品经过优化,可以处理工业和移动应用中使用的许多不同的通信协议。ADI的UART非常适合设计中需要额外的输入/输出资源的应用。我们的UART采用SPI和I2C接口,允许通过既有的I2C或SPI总线增加通信通道。这通常称为UART桥接功能。
ADI公司提供先进的小尺寸SPI/I2C (I2C) UART系列产品。我们的UART系列包括单通道、双通道或四通道选项,还包括集成RS-232或RS-485收发器的UART。这些产品经过优化,可以处理工业和移动应用中使用的许多不同的通信协议。ADI的UART非常适合设计中需要额外的输入/输出资源的应用。我们的UART采用SPI和I2C接口,允许通过既有的I2C或SPI总线增加通信通道。这通常称为UART桥接功能。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}