AD4858FMCZ Unboxing Video
The EVAL-AD4858FMCZ is designed to demonstrate the performance of the AD4858 and provide access to many included configuration options that are accessed via an easy to use ACE plug-in graphical interface. The AD4858 is a fully buffered, 8-channel simultaneous sampling, 20-bit, 1 MSPS data acquisition system (DAS) with differential, wide common mode range inputs.
The EVAL-AD4858FMCZ on-board components include also the following:
- The LTC6655 high precision, low drift, 4.096 V voltage reference (not used by default)
- The LT1761, low noise, 1.8 V, 2.5 V, and 5 V low dropouts (LDOs)
- The LT8330 low quiescent current (IQ) boost converter
This video provides details on how to get started using the EVAL-AD4858FMCZ evaluation platform hardware and software. For additional information, see the AD4858 data sheet and user guide, which should be consulted in conjunction with this video when using the EVAL-AD4858FMCZ.
AD4858FMCZ Unboxing Video
The EVAL-AD4858FMCZ is designed to demonstrate the performance of the AD4858 and provide access to many included configuration options that are accessed via an easy to use ACE plug-in graphical interface. The AD4858 is a fully buffered, 8-channel simultaneous sampling, 20-bit, 1 MSPS data acquisition system (DAS) with differential, wide common mode range inputs.
The EVAL-AD4858FMCZ on-board components include also the following:
- The LTC6655 high precision, low drift, 4.096 V voltage reference (not used by default)
- The LT1761, low noise, 1.8 V, 2.5 V, and 5 V low dropouts (LDOs)
- The LT8330 low quiescent current (IQ) boost converter
This video provides details on how to get started using the EVAL-AD4858FMCZ evaluation platform hardware and software. For additional information, see the AD4858 data sheet and user guide, which should be consulted in conjunction with this video when using the EVAL-AD4858FMCZ.
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}