LT7200S:18V入力、±5A出力、同期整流方式/モノリシックのクワッド降圧レギュレータ

    2023年05月17日

    「LT7200S」は、同期整流方式/モノリシックのクワッド降圧レギュレータです。効率に優れた製品であり、各チャンネルで5Aの負荷電流をソース/シンクすることができます。このような柔軟性が得られることから、コンパクトなレイアウトの基板によって複雑なシステムに対する給電を実現可能です。入力電圧は2.9V~18Vなので、3.3V、5V、12Vの電源を使用するアプリケーションに対応できます。​
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
      LT7200S:18V入力、±5A出力、同期整流方式/モノリシックのクワッド降圧レギュレータ

      2023年05月17日

      「LT7200S」は、同期整流方式/モノリシックのクワッド降圧レギュレータです。効率に優れた製品であり、各チャンネルで5Aの負荷電流をソース/シンクすることができます。このような柔軟性が得られることから、コンパクトなレイアウトの基板によって複雑なシステムに対する給電を実現可能です。入力電圧は2.9V~18Vなので、3.3V、5V、12Vの電源を使用するアプリケーションに対応できます。​