Overview

Product Details

The AD-PZSDR2400TDD-EB is a 2.4GHz TDD analog module designed to work with the AD9361, a high performance, highly integrated RF transceiver intended for use in RF applications, such as 3G and 4G base station and test equipment applications, and software defined radios. The AD-PZSDR2400TDD-EB is affectionately dubbed the first 'RF personality card'. It plugs into the ADRV1CRR-FMC carrier card. 35mm U.FL coaxial cables connect the card to the ADRV9361-Z7035 SDR SOM providing access to the transmit and receive inputs of the AD9361. Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found on the wiki page.


The purpose of the AD-PZSDR2400TDD-EB is to provide the user with a path to condition the transmit or receive signals of the AD9361. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch HMC546 controlled by the FPGA and accompanying software. The transmit path consists of a 2.4GHz filter, half watt driver amplifier ADL5324 and 2 watt power amplifier HMC921. The receive path consists of the same 2.4GHz filter as well as a low loss LNA HMC669.

Getting Started

To start using the AD-PZSDR2400TDD-EB, you must have the ADRV1CRR-FMC carrier card along with the ADRV9361-Z7035 SDR SOM and some 35mm U.FL coaxial cables. Plug the AD-PZSDR2400TDD-EB onto the carrier, connect the UFL cables between the SOM and the 2400TDD board and you are ready to use the board.

Reference Board

Reference Board: AD-PZSDR2400TDD-EB

Pin Hover over the colored pins to learn more about Analog Devices' products used on this board
ADM7171-5

1A LDO

ADP7104

0.5A LDO

ADP7104

0.5A LDO

ADM7171-5

1A LDO

ADP2384

4A Switch Regulator

ADL5324

1/4W Pre-AMP

HMC921

2W PA

ADL5324

1/4W Pre-AMP

HMC921

2W PA

HMC669

LNA w/ Bypass

HMC669

LNA w/ Bypass

HMC546

RF Switch

HMC546

RF Switch

System Requirements

The AD-PZSDR2400TDD-EB board plugs into the ADRV1CRR-FMC carrier card, so that would be the requirement to be able to operate this board. The software needed is already built in the SD card that we provide with the ADRV9361-Z7035 SDR SOM.