MAX96724F

推荐新设计使用

四通道GMSL2/1到CSI-2解串器

超小的4路输入GMSL解串器支持高达8百万像素成像器

产品模型
4
产品技术资料帮助

ADI公司所提供的资料均视为准确、可靠。但本公司不为用户在应用过程中侵犯任何专利权或第三方权利承担任何责任。技术指标的修改不再另行通知。本公司既没有含蓄的允许,也不允许借用ADI公司的专利或专利权的名义。本文出现的商标和注册商标所有权分别属于相应的公司。

产品详情

  • 车规级高速链路
    • 最大插入损耗:-21.0dB(3.0GHz,6Gbps)
    • 最大插入损耗:-19.5dB(1.5GHz,3Gbps)
    • 自动适应通道条件的变化
    • 工作环境温度:-40°C至+105°C
  • 四路可独立配置GMSL输入
    • 6/3Gbps GMSL2和3.12Gbps GMSL1链路速率
    • 187.5Mbps/1Mbps (GMSL2/1)反向链路速率
    • 支持GMSL2/1像素和隧道混合输入
  • 2x4或4x2通道MIPI CSI-2 v1.3输出
    • MIPI D-PHY v1.2额定速率:2.5Gbps/通道
    • C-PHY v1.0额定速率:5.7Gbps/通道
    • 聚合和复制功能
    • D-PHY/C-PHY支持16/32虚拟通道
  • D-PHY(成像器)至C-PHY (SoC)自动转换
  • 从反向信号获取的参考时钟(RoR)
  • 双向反向通道支持
    • 9个可配置GPIO
    • 2个I2C端口,速率高达1Mbps
  • 符合ASIL-B标准(MAX96724/F)
  • 易用特性
  • 减少BOM并节省空间
    • 小型8x8mm TQFN标准和可湿侧面封装
    • 小尺寸同轴电缆供电(PoC)
MAX96724F
四通道GMSL2/1到CSI-2解串器
提问

参考资料

了解更多

软件资源

找不到您所需的软件或驱动?

申请驱动/软件

工具及仿真模型


评估套件

eval board
MAX96724/F/R EVKIT

MAX96724、MAX96724F和MAX96724R的评估套件

特性和优点

  • MAX96724解串器接受来自串行器的GMSL数据,并将其转换为MIPI CSI-2数据信号。
    • 向后兼容,接受GMSL-1串行数据
    • 四路输入可以混搭GMSL-1和GMSL-2
    • 输出符合MIPI D-PHY v1.2和CSI-2 v1.3规范
  • Windows 10® 或更高版本兼容软件支持
  • USB控制接口(随附电缆)
  • 功能强大、易于使用的GUI,支持全方位器件特性评估
  • 评估板由USB、12V壁式适配器或外部电源供电
  • 经过验证的PCB布局
  • 装配完成且经过测试

产品详情

MAX96724 DPHY评估套件(EV套件)提供了一个设计可靠的平台,采用标准FAKRA同轴电缆或MATE-AX电缆来评估MAX96724、MAX96724F和MAX96724R器件的性能。这些解串器支持高带宽、千兆多媒体串行链路(GMSL-1或GMSL-2),并提供扩频和全双工控制通道功能。该评估套件包括一个简单易用的Windows 10®或更高版本兼容图形用户界面(GUI),用于评估器件特性。该评估套件已安装板载MAX96724、MAX96724F或MAX96724R IC。

如需使用标准FAKRA同轴电缆完成GMSL-2评估,请订购MAX96724同轴电缆评估套件以及配套的串行器板,例如MAX9295A同轴电缆评估套件。有关所有GMSL-2功能的详细信息,包括如何使用器件的信息,请参阅ADI公司GMSL客户门户文件夹中的最新GMSL-2用户指南。有关如何使用GMSL2器件进行定制硬件设计的更多信息,请参阅ADI公司GMSL客户门户文件夹中的最新GMSL2硬件设计指南。

应用

  • 高分辨率摄像头系统
  • 先进驾驶辅助系统(ADAS)

eval board
AD-GMSL522-SL

GMSL Carrier Board

特性和优点

  • GMSL2 prototyping system supporting the NVIDIA Jetson™ SoCs
  • On-board MAX96724 that allows 4x GMSL2/1 camera inputs that allows for camera module bring-up, debug, and video streaming
  • On-board MAX96717 that can be used for camera emulation and head-unit debug
  • Enables development of GMSL applications with NVIDIA Jetson™ SoC
  • SAMTEC connector that allows connection of any GMSL DPHY EV Kit to the NVIDIA Jetson™
  • Additional inputs: USB, Ethernet, PCIe, and microSD card

产品详情

The AD-GMSL522-SL is a GMSL-enabled NVIDIA Jetson Xavier™ NX-based carrier board and software solution that allows for simple camera to display conversion. This solution creates a scalable, user friendly, GMSL platform for receiving and transmitting data over a gigabit multimedia serial link (GMSL). The platform enables demonstrations and ecosystem development by serving as a hardware platform for software development.

The AD-GMSL522-SL supports two forms of camera input -- either straight CSI data coming through a SAMTEC connector, or via camera modules using GMSL2 or GMSL1 technology to connect to the on-board MAX96724 via COAX connectors. GMSL evaluation kits or any camera utilizing the standard 15- or 22-pin Raspberry Pi connector can be connected here using the AD-GMSLCAMRPI-SL adapter board.

The AD-GMSL522-SL package includes software tools to enable customers in their development of GMSL applications. Among these tools are modified L4T kernels that support certain camera modules and documentation that allows any user to update these kernels for their specific hardware needs.

The design incorporates the MAX96724GTN/VY+ Quad tunneling GMSL2/1 to CSI-2 deserializer and MAX96717GTJ/VY+ CSI-2 to GMSL2 serializer and provides a reliable platform to evaluate high-bandwidth GMSL.

There are two system options available for purchase: the AD-GMSL522-SL which is the base carrier board and does not include the NVIDIA SoM, and the AD-GMSL522-SOM-SL which is the carrier board including the NVIDIA Jetson Xavier™ NX SoM.

APPLICATIONS

  • ADAS Camera Solutions
  • Sensor Fusion ECU
  • Driver and Occupant Monitoring
  • In-cabin Infotainment

eval board
AD-GMSLCAMRPI-ADP#

GMSL EV Kit Adapter Board

特性和优点

  • Allows utilization of GMSL serializer EV kits with a wide range of cameras having 15-pin or 22-pin ribbon cable connectors such as the RPI Camera
  • Allows utilization of GMSL deserializer EV kits with various processing platforms supporting the 15-pin or 22-pin ribbon cable camera connector, such as the Raspberry Pi or the Nvidia development platforms

产品详情

The AD-GMSLCAMRPI-ADP# enables connecting GMSL serializer and deserializer EV kits to a wide range of cameras and processing platforms supporting industry standard ribbon cable connectors. The adapter consists of three sections that can be broken apart from each other, having with the following functionalities:

  • Two ribbon cable adapters containing a 15-pin and a 22-pin connector routed to each other. The 15-pin connector supports 2 MIPI lanes, while the 22-pin connector supports 4 MIPI lanes.
  • A GMSL serializer EV kit adapter with two 22-pin ribbon cable connectors, for connecting cameras to either of the input MIPI ports of the GMSL serializers
  • A GMSL deserializer EV kit adapter with a22-pin ribbon cable connector connected to each of the output MIPI ports, for connecting to Raspberry Pi and Nvidia development platforms, or other processing platform supporting the 15-pin or 22-pin ribbon cable connector. A USB Type-A connector is available to supply 5V @ 4A.

For a detailed look at all GMSL-2 features, including information on how to use the parts, see the newest GMSL-2 User Guide found in Analog Devices’ GMSL customer portal folder. For more information on how to design customized hardware with GMSL2 devices, see the newest GMSL2 Hardware Design Guide in Analog Devices’ GMSL customer portal folder. Finally, in the similar folders, evkit documentation and guides can be found.

APPLICATIONS

  • High-Resolution Camera Systems
  • Autonomous Guided Vehicles
  • Advanced Driver Assistance Systems (ADAS)

MAX96724/F/R EVKIT
MAX96724、MAX96724F和MAX96724R的评估套件
AD-GMSL522-SL
GMSL Carrier Board
AD-GMSLCAMRPI-ADP#
GMSL EV Kit Adapter Board

最新评论

近期浏览