製品概要

機能と利点

  • フル機能の評価用ADRV9026無線カード
    • ADRV9026-HB/PCBZ(帯域幅2.8GHz~6GHz用)
    • ADRV9026-MB/PCBZ(帯域幅650MHz~2.8GHz用)
    • ADRV9026-MB/PCBZ(帯域幅75MHz~1000MHz用)
  • 4 × 4広帯域RFトランシーバー・プラットフォーム(650MHz~6GHzの周波数範囲で動作)
  • 個別のパワー・ドーター・カードにより、高効率電源ソリューションを実現するリファレンス設計が可能
  • FPGAマザーボード(ADS9-V2EBZ)へのFMCコネクタ
  • 回路図、レイアウト、部品表、API、評価用ソフトウェアを含む

製品概要

ADRV9026無線カードは、クワッド・チャンネル広帯域RFトランシーバーADRV9026をご紹介するために設計された無線カードです。この無線カードを使用すると、デバイス評価用の4 × 4トランシーバー・プラットフォームを使用できます。独立した高効率電源回路ボードや高性能クロッキング・ソリューションなど、この無線カードの動作に必要なペリフェラルはすべて無線ボードに搭載されています。無線カードの1つをFMCコネクタでFPGAマザーボードADS9-V2EBZに接続すれば、全機能内蔵型ADRV9026評価用プラットフォームの完成です。ADRV9026評価用キットはADRV9010の性能評価にも使用できます。

はじめに

 

ソフトウェア

評価用ソフトウェア

ADRV9026 Released Software SW6.4.0.19
The ADRV9026 software package contains the GUI software, the API source code, the firmware file, and the gain tables. The GUI software enables transceiver testing using the evaluation board and the Windows GUI. The API source code is intended for use in a customer system and can be integrated with the rest of the customer code and compiled for the target system. The firmware file in binary format is used by the ARM® processor on the transceivers. The gain tables include the receiver gain tables and transmitter attenuation table. Note that the files within the zip must be used together. For example, the ARM files from one zip file cannot be used with the API files from another version.
ZIP
2481 M
ADRV9026/ADRV9029 - SDCARD
The ADRV9026-SDCARD included with the evaluation kit was up to date at the time of packaging the kit. If an update is necessary, the user will be prompted to update the image when connecting to the GUI. If the card does not function properly or users would like to create their own SD card, this image file can be downloaded and used to write a new card or overwrite the ADRV9026-SDCARD included with the evaluation kit. To program a card using this image, follow the programming instructions after downloading the image to a local drive. Note that a 16 GB minimum SD card is required when programming a new card.
PDF
584.37 K
ADRV9026/ADRV9029 Release Build Software Release Notes SW6.4.0.19
The SW6.4.0.19 RELEASE build provides updates in the ARM firmware, stream files, API, and GUI software to support ADRV9026/ADRV9029.

設計ツール

ZIP
13.85 M
ADRV9026/ADRV9029 Design File Package (Last Updated 10/2021)
The Design File Package includes the eval board schematics, BOM, layout, IBIS, BSDL models, JCOM models, S-parameters Material Declaration, and Symbols and Footprints.

ハードウェア (1)

開発 プラットフォーム