Two Wide Input Range Monolithic Switching Regulators Make it Easy to Fit Boost, Flyback, SEPIC and Inverting Topologies into Tight Spaces
Two Wide Input Range Monolithic Switching Regulators Make it Easy to Fit Boost, Flyback, SEPIC and Inverting Topologies into Tight Spaces
by
Bin Zhang
Jul 1 2011
The LT3957 and LT3958 are high power monolithic switching regulators that can generate a positive or a negative output from a wide range of input voltages. The LT3957 operates over an input range of 3V to 40V, making it suitable for everything from portable electronics to automotive and industrial applications. The LT3958 extends the input voltage to 80V for high voltage telecommunications supplies. Both produce high power from a small footprint as shown by the boost converter layout in Figure 1.

Figure 1. A 10V–40V input, 48V output boost converter board.
These versatile switching regulators can be configured as boost, flyback, SEPIC or inverting converters. The LT3957 and LT3958 feature a rugged low side N-channel power MOSFET rated for 5A/40V and 3.5A/80V respectively. A novel FBX pin architecture provides accurate regulated positive or negative output with a simple resistor divider. These ICs also include soft-start, frequency foldback, input undervoltage lockout, adjustable frequency and synchronous switching.
Features
By integrating the power MOSFET and LDO onto the die, the LT3957 and LT3958 simplify converter design, shrink the solution size and reduce cost when compared to non-monolithic solutions. The LT3957 has an integrated 40V/30mΩ N-MOSFET switch with an internally programmed current limit of 5.9A (typical). The LT3958 has an integrated 84V/90mΩ N-MOSFET switch with an internally programmed current limit of 4A (typical). Each IC has an internal high voltage LDO, which allows LT3957 to be powered from a supply as high as 40V, and for LT3958 as high as 80V.
The LT3957 and LT3958 use a constant frequency, peak current mode control scheme, providing fast transient response and an easy to stabilize feedback loop at variable inputs and outputs. The switching frequency can be programmed over a 100kHz to 1MHz range with a single external resistor, which allows designers to optimize component size and performance parameters, such as minimum/maximum duty cycle and efficiency.
At the heart of each of the LT3957 and LT3958 is a pair of feedback error amplifiers: one regulates a positive output and the other, a negative output. When the converter starts up, the output voltage ramps positive or negative depending on the topology selected. The appropriate error amplifier seamlessly takes over the feedback control, while the other becomes inactive. In this way, these parts can automatically regulate to the desired output voltage in different converter topologies.
The LT3957 and LT3958 contain several features to limit the peak switch currents and output voltage overshoot during start-up or recovery from a fault condition. The SS pin voltage modulates the peak switch current, thereby allowing the output capacitor to charge gradually toward its final value while preventing switch current from reaching current limit. Selection of a capacitor on the SS pin determines the start-up/restart time. The frequency foldback function reduces the switching frequency when FBX voltage is close to 0V to ensure that the IC maintains control over the switch current. An overvoltage protection function protects both the positive and negative output converters from excessive output voltage overshoot. The internal power switch is turned off immediately when the FBX pin voltage exceeds the positive regulated voltage by 8% (typical), or negative regulated voltage by 11% (typical).
A 3V–6V Input, 12V Output Boost Converter
Figure 2 shows a 3V–6V input, 12V output boost power supply using the LT3957. To ensure the 3V minimum operation voltage, the voltage drop across the internal LDO is eliminated by connecting the INTVCC pin directly to VIN pin through a 10Ω resistor (given that the maximum VIN operating voltage of 6V is below INTVCC’s maximum voltage rating of 8V). Figure 3 shows the efficiency of this converter.

Figure 2. A high efficiency and very compact 3V–6V input, 12V output boost converter.

Figure 3. Efficiency of the converter in Figure 2.
A 12V–45V Input, –5V Output Flyback Converter
The LT3957 or LT3958 can be configured as a flyback converter for applications where the converters have multiple outputs, isolated outputs or high input/output voltage conversion ratios. The flyback converter has a very low parts count for multiple outputs, and with prudent selection of transformer turns ratio it can have high output/input voltage conversion ratios with a desirable duty cycle.
The frequency foldback feature of the LT3957 and LT3958 provides robust output short-circuit protection. Each IC’s FBX feature allows the flyback converter to easily produce either positive or negative outputs. Figure 4 shows a LT3958 in a flyback converter that operates from a 12V to 45V input and delivers 2A to a –5V output. Figure 5 shows the efficiency of this converter at different input voltages.

Figure 4. A simple and compact 12V to 45V input, –5V output flyback converter takes advantage of the LT3958’s rugged 84V-rated MOSFET and the novel FBX pin architecture.

Figure 5. Efficiency of the converter in Figure 4.
A 9V–36V Input, 24V Output SEPIC Converter
Figure 6 shows the LT3958 in a 9V to 36V input, 24V output SEPIC converter. This topology allows for the input to be higher, equal or lower than the desired output voltage. In a SEPIC converter, no DC path exists between the input and output, which is an advantage for applications requiring the output to be disconnected from the input source when the circuit is shut down. This design can sustain an indefinite output short-circuit condition due to its topology and the frequency foldback feature. Figure 7 shows the efficiency of this converter at different input voltages.

Figure 6. A simple and compact 9V–36V input, 24V output SEPIC converter with short-circuit protection.

Figure 7. Efficiency of the converter in Figure 6.
A 4V–15V Input, –5V Output Inverting Converter
An inverting converter is similar to the SEPIC converter in that it can step up or step down the input, but with a negative output. It also offers output disconnect and short-circuit protection. Figure 8 shows a 4V–15V input, –5V output inverting converter using LT3957 as the switching regulator. Figure 9 shows the efficiency of this converter at different input voltages.

Figure 8. A simple and compact 4V–15V input, –5V output inverting converter with short-circuit protection.

Figure 9. Efficiency of the converter in Figure 8.
Conclusion
The LT3957 and LT3958 are versatile monolithic switching regulators that can be configured as boost, flyback, SEPIC or inverting converters accepting a wide range of input voltages. By integrating the power MOSFET and LDO, they greatly simplify converter design, shrink solution size and reduce costs. These ICs also offer low shutdown current, soft-start, frequency foldback, input UVLO, adjustable frequency and synchronization. The combination of these features makes the LT3957 and LT3958 suitable for a variety of applications ranging from battery portable electronics to automotive, industrial and telecommunications power supplies.
About The Authors