Supercapacitor Charger and Ideal Diode for Power Supply Ride-Through Systems

Jan 1 2012

Supercapacitors, capacitors with up to 100F of charge storage, are emerging as an alternative to batteries in applications where the importance of power delivery trumps that of total energy storage. Supercapacitors have a number of advantages over batteries that make them a superior solution when short term, high power is needed, such as in power ride-through applications. These advantages include lower effective series resistance (ESR) and enhanced durability in the face of repeated charging.

Like batteries, supercapacitors have some specialized application needs that make using a dedicated IC desirable.

Supercapacitor technology can now offer capacitors as large as 100F, but the maximum working voltage on these capacitors is 2.7V or less. Because most systems require operating voltages higher than this, many supercapacitors are supplied as a pair of capacitors within a single, center-tapped package. The LTC4425 is designed to charge two stacked supercapacitors and provide a regulated output voltage for the system load.

The LTC4425 Architecture

The LTC4425 has two modes of operation: Normal and LDO.

Normal Mode

In Normal mode, the LTC4425 can be thought of as an ideal diode with current limit and supercapacitor-specific functions (see Figure 1). If we ignore everything but the ideal diode controller, MPSNS and MPSW, the LTC4425 behaves like an ideal diode. MPSW is turned on whenever VOUT is lower than VIN by more than 15mV.

Figure 1. Block diagram of the LTC4425.

A fraction (1/1000) of the current in the VOUT pin is impressed on the resistor attached to the PROG pin and the resultant voltage is compared to a reference voltage. When the voltage on the PROG pin reaches the reference voltage, no additional current is allowed to flow out of the VOUT pin.

In Normal mode, the regulation function is not controlled by the output voltage alone, but by VIN – VOUT (see Figure 2). Normal mode is selected by connecting the FB pin to VIN. In Normal mode, as long as VIN – VOUT is greater than 0.75V, the charge current is 1/10 the programmed value. As the VIN – VOUT voltage decreases from 0.75V to 0.25V, the charge current increases linearly to the programmed value at VIN – VOUT = 0.25V. For VIN – VOUT voltages less than 0.25V, but greater than 15mV, the VOUT current is 1000/RPROG, and can be as high as 2A. However, the MPSW device has an RDS(ON) of approximately 50mΩ, so when VIN – VOUT is small enough, this resistance may limit the current. For VIN – VOUT voltages less than 15mV, the ideal diode shuts off, reducing the current out of VOUT to a small leakage current.

Figure 2. Supercapacitor charge current profile in Normal mode is designed to prevent inrush currents.

LDO Mode

In LDO mode the regulation function is not controlled by VIN – VOUT, but by feedback from the output voltage. LDO mode is chosen by connecting an output voltage divider to the FB pin to set the maximum output voltage. In LDO mode, the LTC4425 behaves like a voltage regulator supplying up the programmed current to the load and to charge the supercapacitor. If the supercapacitor is at the desired voltage, the LTC4425 continues to supply the load current up to the programmed maximum current.

If the desired supercapacitor voltage is as close to VIN as possible, then ground the FB pin. This means that the loop will never reach regulation, but the output voltage will track the input voltage within 15mV or IV(OUT) × RDS(ON), whichever is larger.

The LTC4425 limits the current available to the VOUT pin. Usually this current is used to charge the supercapacitor, but could also go to a load. In LDO mode, the current is limited in two ways, the PROG pin, and thermal limiting.

The PROG reference voltage, used in LDO mode, is 1V, and the fraction of the VOUT current that is impressed on the resistor attached to the PROG pin is 1/1000. So the current limit is 1000/RPROG, and can be as high as 2A.

If one imagines charging a 100F capacitor, even at 2A, the voltage changes at 20mV/s. And, during this charging process there is significant dissipation, usually several watts. If a portion of the VOUT current is going to a system load, then the time to charge the supercapacitor is extended. The LTC4425 has a linear thermal regulation loop that limits the current from VOUT, such that the die temperature remains below 105°C. This is a linear circuit meant for usage under normal operating conditions, not a protection circuit that is only there to prevent damage.

LTC4425 Features

Voltage Clamps

There are voltage clamps on each of the stacked output supercapacitors, from VOUT to VMID, and from VMID to ground. The purpose of these voltage clamps is to ensure that the supercapacitors cannot be charged above their rated voltages. The clamp voltage on each of the stacked supercapacitors can be selected to be 2.45V or 2.70V, via the SEL pin.

Suppose that the input voltage is 6V, and the FB pin is grounded, so that the LTC4425 is in LDO mode and trying to charge the supercapacitor to the input voltage. The clamps will activate whenever either of the stacked supercapacitors exceed the clamp voltage.

To keep the power dissipation in the clamp circuitry in check, the LTC4425 automatically reduces the charge current to 1/10 of the programmed value whenever either of the stacked supercapacitors approaches the clamp voltage.

Leakage Balancer

The LTC4425 detects any imbalance in the stacked supercapacitors by comparing VMID to VOUT. When the LTC4425 detects an imbalance, it sinks or sources current from the VMID pin to balance the supercapacitor.

The LTC4425 leakage balancer is primarily intended to account for the effects of self, or system leakage, and so the maximum sink or source current is around 1mA. Nevertheless, the interaction of the voltage clamps and leakage balancer will eventually correct even quite large imbalances. The supercapacitor may become unbalanced during charging because one capacitor in the stack is larger or smaller than the other. For the same charge current, the larger capacitor will be a lower voltage than the smaller capacitor. So, the smaller capacitor may activate its voltage clamp before the larger capacitor finishes charging, unbalancing the stack.

The leakage balancer will then engage and slowly bring the stack back into balance.

PFO Output

The LTC4425 monitors and reports conditions of VIN and VOUT depending on the mode. PFO goes low if the PFI pin is below 1.2V or (VIN – VOUT) > 250mV (in Normal mode) or VFB < 1.11V (in LDO mode), so PFO can be used to switch the load to the supercapacitor if there is a loss of VIN (see Figure 3).

This is especially useful if the load current is much higher than the maximum current the LTC4425 can supply. PFO can be used to switch the load to the supercapacitor only in the absence of VIN.

Figure 3. Charging 2-cell series supercapacitor from Li-ion source. PFO monitors VIN such that power is only switched to the supercap if VIN fails.

Note that PFO monitors either an input fault, or it indicates a low output voltage at the FB pin. If the FB pin is grounded—that is, setup in LDO mode to charge the supercapacitor to VIN—then PFO is permanently asserted low, masking any faults on VIN.

Supercapacitor-Based Ride-Through System

Many electronics systems require a short-term power backup system that allows them to ride through brief interruptions in power. In a similar vein, some systems need time to save states, or empty volatile memory or perform other housekeeping tasks when power is abruptly removed. For example, a hard drive may need to park the heads, so that they don’t land on the media surface. This is an electromechanical system that requires 20ms–100ms of continuous power before it can completely shut down.

Another example involves the effect of large electrical machines on power systems. If a large electric motor is started, such as a commercial building air conditioner or elevator, the mains supply may collapse for several line cycles. Usually the input supply stores only enough energy for between a half a cycle and one cycle. Devices powered by the input supply need a way to operate normally until the mains recovers.

Ride-through applications can certainly be implemented with battery backup, but in many cases, it requires a very large battery array to satisfy the ride-through power requirements. Although batteries can store a lot of energy, they cannot supply much power per volume due to their significant source impedance. Batteries also have relatively short lives, 2~3 years, and their care and feeding requirements are substantial.

Supercapacitors, on the other hand, are well suited to short-power-burst, ride-through applications. Their low source impedance allows them to supply significant power for a relatively short time, and they are considerably more robust than batteries.

Ride-Through Application Setup

Figure 4 shows a complete power interruption ride-through system using the LTC4425, LTC4416, LTC3539 and LTC3606. Figure 5 shows the layout. This design can hold up a 3.3V rail at 200mA for almost eight seconds.

Figure 4. Complete supercapacitor-based power ride-through system.

Figure 5. Front and back board layout used to test the circuit in Figure 4.

The LTC3606 is a micropower buck regulator that produces 3.3V. The LTC4416 provides a dual ideal diode-OR function to ensure maximum efficiency when switching from the regular input to the supercapacitor. The LTC3539 is a micropower boost regulator with output disconnect. This boost regulator operates down to 0.5V, and can support loads of 1.3A × VOUT/VIN at its output. The supercapacitor is a CAP-XX HS206F, 0.55F, 5.5V capacitor.

Ride-Through Application Measured Results and Operation Details

Figure 6 shows the waveforms if the LTC3539 boost circuit is disabled. Run time, from input power off to output regulator voltage dropping to 3V, is 4.68s. Figure 7 shows the waveforms if the LTC3539 boost circuit is operational. Run time, from input power off to output regulator dropping to 3V, is 7.92s.

Figure 6. If the boost regulator is disabled in the circuit of Figure 4, the ride-through applications can support a 0.67W load for about 4.68s.

Figure 7. With boost regulator enabled in the circuit of Figure 4, the ride-through applications can support a 0.67W load for about 7.92s.

When the LTC3539 boost regulator is disabled, as soon as input power falls, the LTC4416 based ideal diodes switch the input energy supply for the LTC3539 buck regulator to the supercapacitor. In Figure 6, the voltage across the supercap (VSC) linearly decreases due to the constant power load of 200mA at 3.3V on the buck regulator (VOUT).

When the input voltage to the LTC3539 reaches the dropout voltage of the regulator, the output voltage is seen to track the input voltage. At 4.68s after input power removal, the voltage on the supercap reaches 3.0V plus the dropout voltage, and VOUT drops below 3V. The buck regulator continues to track the supercap voltage down until it reaches 2V, whereupon the buck regulator shuts off.

In Figure 7, the voltage across the supercap (VSC) linearly decreases due to the constant power load of 200mA at 3.3V on the buck regulator. When VSC reaches 3.4V, the regulation point of the boost regulator, the boost regulator begins switching. This shuts off the ideal diode and disconnects the buck regulator from the supercapacitor. The energy input to the buck regulator is now the boost regulator’s output of 3.4V. VSC remains at 3.4V, but the supercap begins to discharge exponentially, because as the input voltage of the boost regulator drops, it must draw higher and higher current to sustain its output at 3.4V.

Because the input of the buck regulator remains at 3.4V, its output remains in regulation. When the boost regulator reaches its input UVLO it shuts off, and its output immediately collapses. Since its input voltage has now collapsed, the buck regulator shuts off.

Energy Scavenging in the Ride-Through Application

What voltage should the boost output be set to? Clearly, operation is identical, with or without the boost circuit enabled until the input dropout of the buck regulator is reached. One goal in the design is to minimize the amount of time that the boost regulator is used in the power chain, because each additional regulation step lowers the overall efficiency. Here, we set the boost regulator output voltage as close to the buck regulator input dropout voltage as possible, or 3.4V.

The boost regulator must have a synchronous output to maximize efficiency once the boost regulator engages. This implies a boost regulator with a “blocking” output. This in turn necessitates the second ideal diode to allow the supercapacitor to power the buck regulator until the boost regulator engages. The boost regulator must operate to as low a voltage as possible to ensure that the maximum amount of energy is scavenged from the supercapacitor.

If the supercapacitor is initially charged to 5V, then the energy in the supercapacitor is:

Equation 1

The output power is 3.33V at 0.2A = 0.67W, so the percentage of the energy stored in the supercap that is extracted with a buck-only circuit is:

Equation 2

The percentage of the energy stored in the supercapacitor, extracted when the boost regulator is enabled, is:

Equation 3

The percentage of energy stored in the supercapacitor that is recovered increases from 45.1% to 77%. This allows use of a smaller, less expensive supercapacitor.

Conclusion

The power ride-through system shown here uses a 0.55F supercap to hold up power long enough for a microcontroller to complete some last gasp housekeeping tasks. One way to extend the ride-through time for a given supercapacitor is to add a boost regulator to the system, which allows for energy scavenging. The run time of a given supercapacitor can be extended by >30% if energy scavenging is used. This is particularly relevant if the supercapacitor operating voltage is reduced to ensure high temperature reliability.

In addition, the shape of the output voltage is considerably improved as the input voltage to the output regulator is now square in shape. This results in a steady 3.3V output voltage with a sharp cutoff, instead of a ramped voltage drop as the supercap drains.

About the Authors

George Barbehenn

Related to this Article

Products

Latest Media 21

Subtitle
Learn More