Design Note 448: 12-bit DAC in TSOT-23 Includes Bidirectional REF Pin for Connection to Op Amp or External High Precision Reference

Introduction

The LTC2630’s combination of a 12-bit DAC and low-drift integrated reference in a tiny SC-70 package has proven popular for a wide variety of applications. Two new DACs, the LTC2631 and LTC2640, take this winning formula and further expand its reach by adding a bidirectional REF pin and an optional I2C interface in a tiny TSOT-23.

Like their predecessor, these parts feature 1-bit INL and DNL, offer excellent load regulation driving up to 10mA loads, and can operate rail-to-rail. See Table 1 for a list of options.

Table 1. Family Characteristics. Each part has a bidirectional REF pin and is available in 12-, 10-, and 8-bit accuracy.
PART NUMBER TYPE FULL-SCALE POWER-ON RESET CODE PIN 8 FUNCTION
LTC2631-LM I2C 2.5V Midscale Select default REF
LTC2631-LZ I2C 2.5V Zero 6 add’l addresses
LTC2631-HM I2C 4.096V Midscale Select default REF
LTC2631-HZ I2C 4.096V Zero 6 add’l addresses
LTC2640-LM SPI 2.5V Midscale Select default REF
LTC2640-LZ SPI 2.5V Zero DAC Clear
LTC2640-HM SPI 4.096V Midscale Select default REF
LTC2640-HZ SPI 4.096V Zero DAC Clear

Applications Using REF Pin

The bidirectional REF pin can be used as an output, where the accurate 10ppm/°C reference is available to the rest of the application circuit, or it can be used as an input for an external reference.

To configure REF as an output, simply tie the REF_SEL pin high. As an output, the REF pin simplifies pairing the DAC with an op amp. For instance, to achieve an output range centered at 0V, drive the plus input of the op amp, with REF connected to the minus input. Avoid loading the REF pin with DC current; instead, buffer its 500Ω output with an LTC2054 or similar precision op amp.

The LT1991 precision op amp is a superb choice for amplifying or attenuating the DAC output to achieve a desired output range because it requires no precision external resistors. Its integrated, precision resistors are matched to 0.04%, allowing gain to be set by simple pin strapping (see the data sheet for a large variety of gain options). Figure 1 shows the configuration for a difference gain of 4, resulting in a ±5V output with 12-bit programmability under I2C control. Integral nonlinearity, seen in Figure 2, is better than 1LSB.

Programmable ±5V Output

Figure 1. Programmable ±5V Output.

Integral Nonlinearity of Programmable ±5V Output

Figure 2. Integral Nonlinearity of Programmable ±5V Output.

Figure 3 shows a negative output system using a similar setup, this time with the LT1991 configured as an inverting amplifier with a gain of –0.25. The 0.1μF capacitor at REF reduces the already low DAC noise by up to 20%.

Negative Output, 0V to –1.024V

Figure 3. Negative Output, 0V to –1.024V.

For applications requiring more accuracy at full scale, the LTC2631 and LTC2640 can be referenced to an external source. Figure 4 shows how, using an LT1790 low-dropout reference that’s accurate to 0.05%. Tying REF_SEL low configures the REF pin as a reference input. If reset-to-zero is needed, an LTC2640-LZ12 can be substituted. (For that option, pin 8 is rededicated as a CLR pin, and, upon powering up, External Reference mode must be selected by software command before the code is changed from zero.)

0V to 2.048V Output Derived from External Reference

Figure 4. 0V to 2.048V Output Derived from External Reference.

The REF pin enables the LTC2631 and LTC2640 to share their full-scale range with another device, as shown in Figure 5. A 16-bit LTC2453 ADC and LTC2631 DAC are referenced to the same 5V full scale. This circuit allows a variety of possible transfer functions to be applied to an input under computer control. It is easy to implement functions such as squaring and square root, or time-dependent functions such as integration or proportional-integral-derivative (PID) control in this manner, resulting in a circuit that is much simpler and more stable than a purely analog circuit.

Electronic Transfer Function Generator

Figure 5. Electronic Transfer Function Generator.

Conclusion

The LTC2631 and LTC2640 add I2C capability and a bidirectional REF pin to LTC’s family of 12-, 10-, and 8- bit DACs with an integrated reference. For applications requiring a modified output range, the LT1991 op amp with internal precision resistors is an ideal counterpart.

Authors

mark-thoren-blue-background

Mark Thoren

Mark Thoren joined Linear Technology (now part of Analog Devices) in 2001 as an applications engineer supporting precision data converters. He’s since held various roles in mixed-signal applications including developing evaluation systems, training, technical publications, and customer support. Mark is now a systems engineer in ADI’s System Development Group, where he works on reference designs and the ADI University Program. Mark has a B.S. in agricultural mechanical engineering and an M.S. in electrical engineering, both from University of Maine, Orono.

troy-seman

Troy Seman

Troy Seman was a senior design engineer in the Mixed Signal group at Linear Technology from 2002 until 2006. After earning a B.S.E.E. degree from Ohio State University, he also worked as an IC designer at Texas Instruments and IBM Microelectronics.

Kevin Wrenner

Kevin Wrenner

Kevin Wrenner has worked as an IC designer at ADI and Linear Technology since 2002. He earned B.S.E.E. and M.Eng. degrees from Cornell University. Kevin especially enjoys Nixie tubes and making stuff work.