AN-891: ADuC703x Series LIN Baud Rate Calculations

Introduction

The purpose of this application note is to familiarize the user with calculating the divisor values, COMDIV0, COMDIV1 and COMDIV2, for use with UART on the ADuC703x series devices from Analog Devices, Inc. This application note assumes that the user is familiar with Local Interconnect Network (LIN) 2.0 specifications.

This document is divided into three sections:

  • LIN Frame Header. This section explains the LIN Frame header and the Sync byte.
  • LIN Baud Rate Calculations. This section explains one approach to calculating the UART divisor values using the LIN Hardware Synchronization (LHS) functionality.
  • LIN Baud Rate Calculations Example C Code. This section provides an example of C code implementation of the calculations explained in the LIN Baud Rate Calculations section.

LIN Frame Header

A standard LIN communication frame is shown in Figure 1. It is broken down into a break symbol, a Sync byte, the protected identifier, data and a checksum.

  • The break symbol signifies the start of the LIN packet.
  • The Sync byte calibrates the slave’s baud rate.
  • The protected identifier identifies the slave.
  • The checksum is either a classic checksum, calculated over the data transmitted, or the extended checksum, which is calculated over the protected identifier and data.
Figure 1. LIN frame

The Sync byte is shown in more detail in Figure 2. The Sync byte is 0xAA transmitted at the master’s desired baud rate. The standard method for determining the master’s bit rate is to measure the time from the first falling edge to the fifth falling edge. This value is divided by eight, which gives the desired bit rate. This value is then used to calculate the UART divisor values. The calculations are described in more detail in subsequent sections. This application note assumes that the user has set up the LHS MMR to time the full eight bits of the Sync byte (LHSCON1 = 0x62).

Figure 2. LIN sync byte

LIN Baud Rate Calculations

Using the LHS system, the user gets a value in LHSVAL0 after the Sync byte is received. The LHSVAL0 contains the equivalent of 8 TBIT. This value is used to generate the values for the UART dividers COMDIV0, COMDIV1, and the fractional divider COMDIV2. For more information on the UART refer to the relevant ADuC703x data sheet.

To calculate the COMDIV0/COMDIV1 values using the standard baud rate generator, the following basic UART equation is used:

DL  20.48 MHz

Baud Rate x 2CD x 16 x 2

where:

DL is the value of COMDIV0 and COMDIV1.
CD is the clock divider.

In terms of LHSVAL0, the desired baud rate is as follows:

Desired Baud Rate  5.12 MHz x 8

LHSVAL0

(LHSVAL0 is clocked from an internal 5.12 MHz clock and it is assumed that LHSCON1 is configured to measure 8 TBIT.)

If the standard baud rate equation and the desired baud rate equation are combined,

DL  20.48 MHz x LHSVAL0

5.12 MHz x 2CD x 16 x 2 x 8
DL  LHSVAL0

2CD x 16 x 2 x 8
DL  LHSVAL0

2CD + 6

Using only the standard baud rate generator equation gives the required values of COMDIV0/COMDIV1.

For increased accuracy, use the ADuC703x fractional divider with the DL value (COMDIV0/COMDIV1) calculated previously for the standard baud rate generator. The equation using the fractional divider is as follows:

Baud Rate  20.48 MHz

DL x 2CD x 16 x 2 x ( M + N2048)

where M and N are COMDIV2 values.

M + N2048  20.48 MHz

Baud Rate x DL x 2CD x 16 x 2

Replacing Baud Rate,

M + N2048  20.48 MHz x LHSVAL0

5.12 MHz x 8 x DL x 2CD x 16 x 2

This simplifies to

M + N2048  LHSVAL0

DL x 2CD x 2 x 16 x 2
M + N2048  LHSVAL0

DL x 2CD + 6

To reduce the need for complex math used in the calculation of the fractional divider, limit the values of DL (COMDIV0/COMDIV1) to the power of two. For example, if DL = 17, use DL = 16 = 24 in the calculation of N. This automatically adjusts the value of N to compensate for the error introduced by modifying DL.

DL  2DL_Power
M + N2048  LHSVAL0

DL x 2DL_Power x 2CD + 6
M + N2048  LHSVAL0

DL x 2DL_Power + CD + 6

If M is set equal to 1,

N  211 x LHSVAL0  − 2048

2DL_Power + CD + 6
N  25 − DL_Power − CD x LHSVAL0 − 2048

For example, for a baud rate of 19,200 bps, with CD = 0, DL = 33 and LHSVAL0 = 2133, then N = 21 and the baud rate is 19,197 bps. If DL = 32 and N = 85 is used, the baud rate is then 19,203 bps.

LIN Baud Rate Calculations Example C Code

When programming in C, the preceding equations can be simply written by using the << and >> shift commands.

// DL = LHSVAL0 >> CD_Bits + 6 
iDL = LHSVAL0 >> (( POWCON & 0x7)+6);

// writing DL as 2^iDL_Power 
iDL_Power = 0; 
iDL_temp = iDL; 
while(iDL >> (iDL_Power +1 )) 
{
     iDL_Power++;
}

// Configuration of the fractional divider: 
// M = 1 
// N = LHSVAL0 × 2 ^ (5 – (iDL_Power + CD)) - 2048 
iDL_temp = iDL_Power + (POWCON & 0x7); 
if (iDL_temp > 5) 
{ 
     iDL_temp = (LHSVAL0 >> (iDL_temp -5)) - 2048; 
} 
else 
{ 
     iDL_temp= (LHSVAL0 << (5 - iDL_temp)) - 2048; 
} 

COMDIV2 = 0x8800 + iDL_temp;

COMCON0 = 0x080;   // Setting DLAB 
// Setting DIV0 and DIV1 to DL calculated 
COMDIV0 = (1<< iDL_Power) & 0xff; 
COMDIV1 = (1<< iDL_Power) & 0xff00; 
COMCON0 = 0x03;   // Setting DLAB 
COMIEN0 = 0x1;    // Enable RX interrupt

 

著者

Generic_Author_image

Aude Richard