Wideband 2-Channel Monolithic Analog Multiplier/Divider

AD539 Provides Linear, Logarithmic, Square-Law Gain Control, Signal Bandwidths to 60MHz, Control Bandwidth of 5MHz, with Low Distortion

Model AD539 is a fast, low-distortion analog multiplier-divider with two wideband signal channels controlled by common inputs providing either linear or logarithmic gain control. It is fabricated monolithically, using laser-trimmed thin-film resistors, and packaged in a 16-pin DIP. Read full article


著者

Barrie Gilbert

Barrie Gilbert

Barrie Gilbertは、アナログ・デバイセズ初のフェローであり、「アナログ・エレガンスの追求」に生涯を費やしてきました。1972 年にアナログ・デバイセズに入社し、1979 年にはフェローに選ばれました。現在、オレゴン州ビーヴァートンにあるNorthwest Labの責任者を務めています。1937 年に英国ボーンマスで生まれ、1954 年にSRDEで第1世代のトランジスタの開発に携わった後、Mullard,Ltd.、Tektronix Lab、Plessey Research Labで勤務しました。1984年からIEEEフェローを務め、数々の受賞歴もあります。保有する特許は約50 件に上り、発表した論文は40 件以上、共同執筆による著作も複数あります。また、いくつかの定期刊行物の校閲を担当しています。1997 年にはオレゴン州立大学から名誉工学博士号を授与されています。