Versatile Monolithic V/f or I/f Converter

AD537 is Easy to Use, Works from Single Supply; Outputs to Beyond 100kHz; T/f Conversion Inherent

The AD537 is a self-contained monolithic voltage-to-frequency converter fabricated on a single 74 x 118 mil (1.9 x 3mm) silicon chip and mounted in a hermetically-sealed 14-pin ceramic dual in-line package (DIP). It contains an input amplifier, a precision oscillator system, a reference generator, and a high-current output stage. Read full article



著者

Dave-Kress-Blue

David Kress

David Kress earned both his BSCE and MSCE for the Massachusetts Institute of Technology. David was first a designer of medical electronic equipment before joining Analog Devices in 1972 as an IC designer. Over the years, he has been involved in analog chip design, wafer fabrication engineering, and new product development and management. For many years David led ADI's technical support team, and he was the Director of Technical Marketing before he retired 2018.

Barrie Gilbert

Barrie Gilbert

Barrie Gilbertは、アナログ・デバイセズ初のフェローであり、「アナログ・エレガンスの追求」に生涯を費やしてきました。1972 年にアナログ・デバイセズに入社し、1979 年にはフェローに選ばれました。現在、オレゴン州ビーヴァートンにあるNorthwest Labの責任者を務めています。1937 年に英国ボーンマスで生まれ、1954 年にSRDEで第1世代のトランジスタの開発に携わった後、Mullard,Ltd.、Tektronix Lab、Plessey Research Labで勤務しました。1984年からIEEEフェローを務め、数々の受賞歴もあります。保有する特許は約50 件に上り、発表した論文は40 件以上、共同執筆による著作も複数あります。また、いくつかの定期刊行物の校閲を担当しています。1997 年にはオレゴン州立大学から名誉工学博士号を授与されています。