Quad 12-Bit Readback DAC with 40-ns Bus Access Time

AD392 Has Four Complete Double-Buffered Voltage-Output DACs; Has ±1/2-LSB Max Linearity Error, Is Guaranteed Monotonic Over Temperature

The AD392 consists of four complete double-buffered 12-bit voltage-output DACs in a single 32-pin hermetically sealed package; it has a readback capability that can be used to verify that the data latched into the DAC registers is the same as the data sent from the microprocessor, a key feature in applications such as automatic testing and robotics. Read full article



著者

Generic_Author_image

Bill Gotschewski