Monolithic Analog Trigonometric Function Generator

AD639 Computes SIN, COS, TAN, Plus Reciprocal, Inverse, and Offset Functions; Complete and Self-Contained; SINE and COSINE Accuracy Specified over ±360°

The AD639 is an analog "trigonometric microsystem" on a single silicon chip, packaged in a 16-pin DIP. From a differential voltage input, representing an angle, (20mV/°), it can be pin-programmed to generate a voltage output, accurately determined by any of the standard functions—sine, cosine, tangent, secant, cosecant, and cotangent—as well as some lesser-known variants, such as the versine and exsecant, plus a corresponding set of inverse functions. Read full article



著者

Barrie Gilbert

Barrie Gilbert

Barrie Gilbertは、アナログ・デバイセズ初のフェローであり、「アナログ・エレガンスの追求」に生涯を費やしてきました。1972 年にアナログ・デバイセズに入社し、1979 年にはフェローに選ばれました。現在、オレゴン州ビーヴァートンにあるNorthwest Labの責任者を務めています。1937 年に英国ボーンマスで生まれ、1954 年にSRDEで第1世代のトランジスタの開発に携わった後、Mullard,Ltd.、Tektronix Lab、Plessey Research Labで勤務しました。1984年からIEEEフェローを務め、数々の受賞歴もあります。保有する特許は約50 件に上り、発表した論文は40 件以上、共同執筆による著作も複数あります。また、いくつかの定期刊行物の校閲を担当しています。1997 年にはオレゴン州立大学から名誉工学博士号を授与されています。