High-accuracy, Widest Bandwidth IC Analog Multiplier

4-Quadrant AD834 Multiplies with Excellence from DC to 500 MHz; Use It for Power Measurement, Wideband Modulation & Gain Control

The AD834 is a monolithic laser-trimmed four-quadrant analog multiplier designed for use in high-frequency applications. A descendant of the AD534 general-purpose multiplier (Analog Dialogue 11-1, 1977) and a cousin of the AD539 2-channel wideband (60 MHz) multiplier (16-3, 1982), it combines 500-MHz minimum bandwidth (both inputs) and total low-frequency error less than ±2% of full scale to provide operation in all four quadrants, with low distortion, drift, and noise. Read full article



著者

Barrie Gilbert

Barrie Gilbert

Barrie Gilbertは、アナログ・デバイセズ初のフェローであり、「アナログ・エレガンスの追求」に生涯を費やしてきました。1972 年にアナログ・デバイセズに入社し、1979 年にはフェローに選ばれました。現在、オレゴン州ビーヴァートンにあるNorthwest Labの責任者を務めています。1937 年に英国ボーンマスで生まれ、1954 年にSRDEで第1世代のトランジスタの開発に携わった後、Mullard,Ltd.、Tektronix Lab、Plessey Research Labで勤務しました。1984年からIEEEフェローを務め、数々の受賞歴もあります。保有する特許は約50 件に上り、発表した論文は40 件以上、共同執筆による著作も複数あります。また、いくつかの定期刊行物の校閲を担当しています。1997 年にはオレゴン州立大学から名誉工学博士号を授与されています。