Applying a High-performance Video Operational Amplifier

Using the AD811 as an ADC input buffer, dc restorer, and sync stripper

The recently introduce Analog Devices AD811, using the most up-to-date curcuit and process technology, is the highest performer in a growing line of monolithic transimpedance amplifiers. It is intended primarily for high-speed ac applications, like its predecessors—for example, the AD844, the AD846, the OP-160/OP-260, and the AD9617/AD9618. Read full article



著者

Generic_Author_image

Dave Whitney

Generic_Author_image

Walt Jung