Optimization of EVM Performance in IQ Modulators

Introduction

EVM, or error vector magnitude, is essentially a scalar measurement of digital modulation accuracy, an important figure of merit for any source of digital modulation. This note shows how a vector signal analyzer helps optimize EVM performance of IQ modulators such as the LTC5598, a 5MHz to 1600MHz high linearity direct quadrature modulator.

Low modulator EVM is desired because the EVM degrades farther down the line—transmit up-converters, filters, power amplifiers, the communications channel, and the receiver all impair the received signal.

Figure 1. Typical 450MHz EVM Measurement Result of 0.34% RMS. For Comparison, a High-Grade Lab Signal Generator EVM Measures 0.28% RMS on the Same VSA Setup.

Figure 1. Typical 450MHz EVM Measurement Result of 0.34% RMS. For Comparison, a High-Grade Lab Signal Generator EVM Measures 0.28% RMS on the Same VSA Setup.

Test Setup

Unless otherwise noted, the following test conditions apply (See Figure 3):

  • LTC5598 IQ modulator on Linear Technology demonstration circuit DC1455A.
  • LO: 0dBm, f = 450MHz.
  • Baseband Modulation: PN9, root raised cosine (RRC) filtering, α = 0.35, symbol rate = 1Msps, 16-QAM (four bits per symbol, peak-to-average ratio 5.4dB).
  • Baseband drive: VEMF1 = 0.8V differential (1.15VP-P differential). VBIAS = 0.5V.
  • VSA measurement filter: RRC, α = 0.35.
    VSA reference filter: Root Cosine (RC).
Figure 2. EVM Test Setup. The Low-Pass Harmonic Filter Removes the Primarily Odd Output Harmonics for Accurate Output Power Measurement.

Figure 2. EVM Test Setup. The Low-Pass Harmonic Filter Removes the Primarily Odd Output Harmonics for Accurate Output Power Measurement.

16-QAM is a relatively common type of digital modulation, readily demonstrating the modulation accuracy attainable with the LTC5598. It is utilized in many wireless communication standards such as LTE/LTE-Advanced, HSDPA, EDGE Evo, CDMA2000 EV-DO, Cognitive Radio IEEE 802.22 (TV white space), PHS, and TETRA.

Figure 3. Basic Principle of the VSA. It Compares an Input Measured Signal to an Ideally Regenerated Reference Signal.

Figure 3. Basic Principle of the VSA. It Compares an Input Measured Signal to an Ideally Regenerated Reference Signal.

LTC5598 EVM Test Results

A typical EVM measurement at LO = 450MHz is shown in Figure 1, demonstrating an LTC5598 EVM of 0.34% rms, and 0.9% peak. After the harmonic filter, output power measures +0.4dBm for the same signal. By comparison, a lab-grade signal generator with the same amplitude, frequency, and digital modulation measures 0.28% rms and 0.8% peak, on the same VSA setup. This indicates that the LTC5598 modulation accuracy is nearly as good as the test equipment being used to measure it.

EVM vs IQ Drive Level

  • 16-QAM, 1Msps, RRC, raised cosine, α = 0.35 (peak-to- average ratio 5.4dB).
  • VBIAS = 0.5V DC. LO = 0dBm.

Figure 4 shows EVM increasing rapidly when the baseband inputs drive the modulator output signal peaks into compression. Even without a VSA to measure EVM, this level of maximum rms output power can be estimated by:

 Equation 1

Figure 4. EVM and RMS Output Power vs IQ Drive Level.

Figure 4. EVM and RMS Output Power vs IQ Drive Level.

Again, this is just a rough estimate. For more complex modulation schemes, even 1dB compression may be excessive, and at the same time, the crest factor will be higher, thus significantly dropping the average output power that becomes available for highly complex waveforms.

EVM vs LO Frequency

The same test conditions are used:

16-QAM, 1Msps, RRC, raised cosine, α = 0.35 (peak-to-average ratio 5.4dB). VEMF = 0.8V differential (1.15VP-P differential), VBIAS = 0.5V.

Figure 5 illustrates how the LTC5598 modulation accuracy is affected near the ends of the IQ Modulator frequency range specification. EVM is lowest at midband frequencies from 30MHz to 700MHz. At LO frequency below 30MHz, EVM is reduced with stronger LO drive (consult the LTC5598 data sheet).

Figure 5. LTC5598 EVM vs LO Frequency. At Low LO Frequencies, EVM Can Be Improved with Higher LO Drive Power and/or Quadrature Phase Error Correction within the Baseband.

Figure 5. LTC5598 EVM vs LO Frequency. At Low LO Frequencies, EVM Can Be Improved with Higher LO Drive Power and/or Quadrature Phase Error Correction within the Baseband.

At both LO frequency extremes, the main contributor to LTC5598 EVM is quadrature phase error, as shown in Table 1. Some IQ gain imbalance is also present, but generally not much of a contributor to overall EVM. Where necessary, either or both of these error terms can be corrected open-loop in baseband, or in some transmit chains as part of an existing closed-loop PA pre-distortion correction system2.

Slightly higher EVM may be perfectly acceptable in some systems, for example when simple, low-order digital modulation schemes are used.

Table 1. LTC5598 Quadrature Phase and Gain Imbalance Errors (LO Drive = 0dBm). Sideband Suppression is the Aggregate Effect Of Both
LO FREQUENCY (MHz) QUADRATURE PHASE ERROR (DEG.) IQ GAIN IMBALANCE (dB) SIDEBAND SUPPRESSION (dB)
5 4.3 0.14 28
10 3.6 0.01 30
20 1.2 0.02 40
40 −0.3 0.03 50
1600 −1.2 0.05 39

Tips for Lowest IQ Modulation EVM

  • Use "clean" IQ baseband source:
    • IQ DAC clock should be low phase noise and jitter.
    • Be sure DAC reconstruction filter does not encroach upon the baseband bandwidth.
    • Be sure the baseband IQ signal paths have sufficiently flat frequency response.
  • Use a "clean" LO signal source:
    • LO phase noise adds random phase error, increasing EVM. This type of error cannot be later removed.
    • LO harmonics will give rise to quadrature phase error. For best results, adhere to the modulator datasheet recommendation regarding LO harmonic content.

Conclusion

The LTC5598 provides excellent digital modulation accuracy across many popular VHF and UHF communications bands. In some cases, EVM is comparable to that of a lab-grade signal generator. Where desired or necessary, baseband correction of quadrature phase and/or gain may be implemented for enhanced accuracy.

Notes

Note 1. VEMF is the differential IQ baseband amplitude, as indicated on the Rohde & Schwarz AMIQ software. Actual I and Q voltage (peak-to-peak differential) measures as shown.

Note 2. While the subject of pre-distortion correction (Pre-D) is beyond the scope of this document, suffice it to say that the Pre-D will have its own receiver that can effectively measure transmit EVM and make adaptive corrections to the baseband waveforms to minimize error. The Pre-D does not know or care where the error originates (modulator, PA, or both).

About the Authors

Petrus Stroet
Petrus (Peter) Stroet received the M.S. degree in electrical engineering from the University of Twente, The Netherlands, in 1994 and subsequently followed a two-year designers program at the same university. He joined Phil...
Bruce Hemp
Bruce Hemp graduated in 1980 from California State University, Fullerton with his B.S. degree in engineering. He has held various systems, board-level, and applications engineering positions. Since 2012, Hemp has been a se...

Related to this Article

Latest Media 21

Subtitle
Learn More