SIGNALS+ NEWSLETTER SUBSCRIPTION
Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.
Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.
You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!
ClosePALMSENS ENABLES ELECTROCHEMICAL BIOSENSOR POINT-OF-CARE DIAGNOSTICS
TAPPING THE POTENTIAL OF POTENTIOSTATS
It’s no surprise that COVID-19 has generated a wave of interest and innovation in electrochemical biosensor development. With better biosensing sensors and readers, healthcare providers have a quick aid to make the correct diagnosis and treatment—not only for COVID, but also for many other diseases ranging from malaria and tuberculosis to bacterial infections.
It’s not that electrochemical biosensor innovators have overlooked this need. The opportunity here is self-evident. But to create a better testing solution, expertise in electrochemistry is not enough; measurement and sensing expertise are also needed. For example, a potentiostat is an electric circuit that senses changes in a cell’s resistance and adjusts the current accordingly through an auxiliary electrode. This device is an essential piece of electronic hardware for control and measuring in most electroanalytical experiments. But basic or not, for those innovating in the electrochemical biosensor space, recognizing the electrochemical signature of a virus or bacteria is likely the easy part, while building products or readers like a potentiostat could take years of research, and trial and error.
The EmStat Pico potentiostat module by Analog Devices, Inc. (ADI) and PalmSens eliminates the need for potentiostat knowledge when creating electrochemical biosensor technology—and with it, the need for biosensor innovators to spend time and money to either hire experts or become experts themselves. By partnering with PalmSens on this standalone potentiostat module, ADI has helped fill in the gaps so innovators can get lifesaving products to market more quickly.
AT A GLANCE
COMPANY
Founded in 2001 by Dr. Kees van Velzen, PalmSens provides a comprehensive range of instruments for most types of electrochemistry with an emphasis on mobility. Their mission is to make electrochemistry easier, more portable, and more accessible for novice and advanced researchers and entrepreneurs.
APPLICATIONS
- Healthcare
- Environmental monitoring
- Food safety
- Veterinary care
- Condition monitoring
CHALLENGE
Combine PalmSens’ electrochemical biosensor technology with ADI’s leading signal processing expertise to create a potentiostat that is faster, smaller, and lower power than its laboratory equivalent without sacrificing accuracy—and make it easy for innovators to implement, even if they have never designed with potentiostats.
GOAL
Develop an electrochemical biosensor platform that helps innovators fill in technical gaps so they can see their mission bear fruit and bring lifesaving tech to market faster.
FIRST TO MARKET: QSM AND THE OTTER EQ

Boston-based QSM Diagnostics develops point-of-care veterinary diagnostics for the rapid identification of bacterial infections. The company has several decades of experience in the development and commercialization of sensors and medical devices.
In 2016, QSM began working with Analog Garage to develop a low cost, portable electrochemical biosensor reader that could deliver the same results as traditional veterinary reference lab equipment, right there in the clinic. Later, when ADI and PalmSens released the EmStat Pico, QSM quickly saw the potential for this newer, smaller potentiostat module to save significant resources in product development compared to designing a similar product in-house.
“Why reinvent the wheel?”
Ed Goluch, CEO, QSM
“We’ve put all our efforts into the testing chemistry and didn’t have to worry about the electronics that were going to perform that measurement,” said Ed Goluch, CEO, QSM. “Why reinvent the wheel?”
QSM’s Otter eQ is one of the first products incorporating EmStat Pico by ADI and PalmSens to reach the market and demonstrates the versatility of a potentiostat as a biosensor reader for point-of-care applications—today, for your dog; tomorrow, for everyone else.
BIOSENSORS IN THE VETERINARY LAB
In dogs, some ear infections are worse than others. Those caused by the bacteria Pseudomonas aeruginosa can be tricky to detect and require a different course of treatment. But to determine whether this type of bacteria is the culprit, vets must send samples away to a laboratory and wait for results, meanwhile treating your family pet the best they can with incomplete data.

A POTENTIOSTAT IN YOUR POCKET
QSM set out to create an electrochemical biosensor and reader that provides diagnostics right in the office, with results available by the next morning or even before your dog leaves the clinic. The instrument is both fast and extremely portable due to the embedded EmStat Pico form factor of 30 mm × 6 mm.


“Having a lab in your pocket means you don't need the regular lab. Instead of waiting a day or more, it will give you a result within two minutes.”Willem van Velzen
CEO, PalmSens
THE NEXT GENERATION OF OTTER EQ
The current generation of Otter eQ detects a single type of bacteria, but the reader has the potential to be used with multiple sensors, which are currently under development. So, there is no need to develop a new reader with every sensor. Soon enough, the Otter eQ will be able to test multiple types of animals for a variety of infections. Future versions may function more like a blood panel, testing for multiple pathogens on a single cartridge.
The latest ADI offerings will enable QSM to scale from B2B markets into B2C territory in the future. Making Otter eQ available to consumers would help lighten the load for overbooked veterinary clinics, either by sparing pet owners unnecessary visits to the vet or by enabling remote appointment follow-ups to ensure prescribed treatments have done their job.
HOW IT WORKS

1. |
Obtain sample, in this case by swabbing the inside of the dog’s affected ear. |

2. |
Insert single-use sensor cartridge, mix sample with pre-measured buffer, and apply to cartridge. |

3. |
Wait for two minutes and read results. Sensor array allows diagnosis of multiple bacteria on one cartridge. |
DOGS, CATS, AND HUMANS: THE QSM VISION
“Starting with a product for the point-of-care market for pets greatly reduces regulatory aspects compared to one with humans,” said van Velzen. “It is also a great stepping-stone to point-of-care applications for humans, for which a bright future awaits.”
QSM technology is already being used to identify herbicides in agricultural water supplies, to monitor drinking water quality, and to check food supplies for pathogens like E. Coli. A cartridge could be calibrated specifically to identify viral particles—or, to monitor other markers that are not infection-related, such as tracking cortisol, cholesterol, or medication use at home.
“COVID made people realize that there hasn’t been enough work done in this space,” said Goluch. “Glucose meters have been around for 70 years, and we haven’t seen other technologies based on it. Now we’re at a point where we can use that module to test for other things. Our cartridges could detect anything. Just change the chemistry and the platform works.”

GETTING LIFESAVING TECH TO MARKET FASTER
Because the EmStat Pico module could be integrated into QSM’s existing cartridge design, proprietary connections and all, Goluch estimates that QSM reduced its product development time by three years compared to developing a custom solution in-house. Additionally, PalmSens provides software development kits that streamlined the process even further; this allowed QSM to develop a product with very little need for technical support from PalmSens.
“The motivation for partnering with PalmSens was to be able to deliver that complete solution—a plug and play measurement module,” said Brian Coffey, ADI. “It’s exciting to hear how it is enabling customers to get to market faster with new lifesaving health diagnostic tools.”

*2017-2018 AVMA Pet Ownership and Demographics Sourcebook