How to Select a Transformer When Designing an Isolated Buck Converter

Feb 7 2022

Abstract

This article explains how an isolated buck converter works and how to select a transformer, a pivotal step in designing an isolated buck converter. It discusses which parameters to consider, the mathematics that should be followed when choosing a transformer, and how these parameters influence the overall circuit.

How Does an Isolated Buck Converter Work?

An isolated buck topology, as shown in Figure 1, is similar to a generic buck converter. By replacing the inductor in a buck circuit using a transformer, we can get an isolated buck converter. The transformer’s secondary side has an independent ground.

Figure 1. An isolated buck topology.
Figure 1. An isolated buck topology.

During on-time, the high-side switch (QHS) is on and the low-side switch (QLS) is off. The transformer’s magnetizing inductance (LPRI) is charged up. The arrows in Figure 2 show the current flow direction. The primary current increases linearly. The current ramping slope depends on (VIN – VPRI) and LPRI. The secondary side diode, D1, is reverse biased during this time interval and loads current flow from COUT to load.

Figure 2. On period equivalent circuit.
Figure 2. On period equivalent circuit.

During off-time, QHS is off and QLS is on. The primary inductor is discharged. The primary current flows from QLS to ground, D1 is forward biased, and the secondary current flows from the second side coil to COUT and to load. COUT is charged up in this time period. (Turning off QHS and turning on QLS cannot change current direction; it can only change the current slope. The positive current decreases until 0 A, then the negative current increases.)

Figure 3. Off period equivalent circuit.
Figure 3. Off period equivalent circuit.

Which Specifications Will Influence the Transformer?

When designing a converter, some specifications should be declared and cleared. It will determine which component will be used especially when choosing a transformer.

  • Input voltage range
  • Output voltage
  • Maximum duty cycle
  • Switch frequency
  • Output voltage ripple
  • Output current
  • Output power

Maximum duty cycle (D) is usually assigned in the range of 0.4 to 0.6. The minimum input voltage (VIN_MIN) and maximum duty cycle will determine the primary output voltage (VPRI). Then, the primary output voltage (VPRI) and secondary output voltage (VOUT) will determine the transformer turns ratio.

Output current (IOUT) and output power (POUT) are key parameters that influence transformer selection. Output current determines the thickness of the copper wire, while output power determines which transformer bobbin should be used. The permeability of the bobbin shows how much energy it can store and how much power it can put out. Generally, the DC output current multiplied by a coefficient is assigned to the inductor’s (transformer’s) ripple current. Duty cycle and switch frequency are used to calculate TON time, while VIN, VPRI, and ripple current determine the primary inductance. The assigned coefficient must not be too large or too small since a large coefficient can lead to a large ripple current. A large ripple current may reach half of the H-bridge current limit and damage the MOSFET. This will lead to a large ripple voltage on the output capacitor due to its ESR and ESL. On the contrary, when an extremely small ripple current is needed, we need to use a high inductance value inductor (transformer). If the coil has many turns, this will require a bulky bobbin. The large inductance will limit loop bandwidth and reduce the dynamic response index.

Choosing a Transformer

Energy is transmitted to secondary coil only in TOFF time. The turns ratio can be determined by Equation 1:

Equation 1

Where VD is the secondary diode forward bias voltage. For VPRI, we usually assign a maximum duty cycle in the range of 0.4 to 0.6. The VPRI can be calculated using Equation 2:

Equation 2

Where D is the maximum duty cycle and VIN_MIN is the minimum input voltage. From Equation 2, we can calculate the turns ratio. In a non-isolated buck converter, the ripple current is the same on both sides of the inductor. Easily, we can calculate the inductance required using Equation 3.

Equation 3

Where f is the switching frequency and ΔI is the ripple current. As discussed previously, ripple current equals the DC output current multiplied by a coefficient:

Equation 4

Where K is the coefficient. But in an isolated buck converter topology, there is a transformer and not an inductor. How do we deal with it when the component is a transformer rather than a inductor? As we know, the current ratio equals the inverse of the turns ratio:

Equation 5

Where IPRITOFF is the secondary current that is converted to a primary current in TOFF time. We should add a transformer’s two-coil current as an equivalent inductor current.

Equation 6

Where ILeq is the equivalent inductor current. If the transformer has three more windings, then

Equation 7

Is this correct? Let’s see a simulation result based on the MAX17682. Figure 4 shows a MAX17682 circuit, which was drawn in EE-Sim® OASIS, powered by SIMetrix/SIMPLIS. Current probes, labeled IPRI and ISEC1, have been placed at both sides of the transformer.

Figure 4.  A MAX17682 typical circuit in EE-Sim OASIS, powered by SIMetrix/SIMPLIS.
Figure 4. A MAX17682 typical circuit in EE-Sim OASIS, powered by SIMetrix/SIMPLIS.

Figure 5 shows a transient simulation result from the two probes. The two current waveforms were added utilizing Equation 6.

Figure 5. A MAX17682 typical circuit simulated current waveform.
Figure 5. A MAX17682 typical circuit simulated current waveform.

The added current results (red) in a triangle wave and behaves just like the inductor in a non-isolated buck converter. So the transformer’s primary ΔI can be easily calculated:

Equation 8

Usually, we assign a load ripple current that is 0.2 times the DC output current. So K can be assigned to 0.2 times NSEC/NPRI. At the same time, the primary peak current should be designed less than the switch current limitation, where IPK is:

Equation 9

Then the transformer’s primary inductance can be easily calculated:

Equation 10

By using the turns ratio, primary inductance, output power, output current, and isolation voltage, we can decide which inductor will be used or designed.

Why a Simplified Equation Can Work

Let’s see how we can better understand and apply the equation shown in the MAX17682 data sheet (see Figure 6).

Figure 6. A screenshot of the MAX17682 data sheet.
Figure 6. A screenshot of the MAX17682 data sheet.

According to the previous discussion, Equation 10 can be rewritten to follow Equation 11 for TOFF time.

Equation 11

Assuming D is 0.6, if and only if ΔI were 0.4 A, the polynomial (1 – D) and ΔI can be reduced. Then Equation 11 and the equation from Figure 6 are the same. The equation in the data sheet already selects the primary ripple current. If we assign D as 0.6, the primary ripple current is 0.4 A. In quantity, TOFF duty cycle equals the primary ripple current.

Equation 12

Conclusion

By using the simplified equation shown in Figure 6, the user ensures a faster design with a primary ripple current that equals the TOFF duty cycle. If you want to modify primary ripple current or use another parameter, you can follow this tutorial.

About the Authors

Yaxian Li
Yaxian Li is an applications engineer in the Training and Technical Services Group at Analog Devices. Yaxian joined Maxim Integrated (now part of Analog Devices) in 2020 after graduating from Hangzhou Dianzi University wit...

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More