Design Note: 227 Sense Milliamps to Kiloamps and Digitize to 12 Bits

Introduction

The LT1787 high side current sense amplifier provides a precision measurement of current into or out of a power source. The part generates an output voltage that is directly proportional to the current flowing through an external current sense resistor. With a miniscule 40μV (typical) input offset voltage, the LT1787 has a better than 12-bit, zero-cross accurate dynamic range at 250mV full-scale input. A hefty 60V maximum supply voltage specification allows the part to be used not only in low voltage battery applications but also in higher voltage telecom and industrial applications. Independent VEE and VBIAS pins make the application of the LT1787 extremely versatile.

The device is self-powered from the supply that it is monitoring and requires only 60μA of supply current. The power supply rejection ratio of the LT1787 is in excess of 120dB. The part has a fixed voltage gain of 8 from input to output.

Additional LT1787 features include provisions for input noise filtering (both differential and common mode) and the ability to operate over a very wide supply range of 2.5V to 60V. A functional diagram of the part and its theory of operation is detailed in the side bar. The part is available in both 8-lead SO and MSOP packages.

Operation with an A/D Converter

Figure 1 shows a detailed schematic of a high resolution (12-bit), bidirectional current-to-bits converter using an LT1787, the LT1783 SOT-23 1.2MHz micropower, rail-to-rail op amp and the LTC1404 SO-8 packaged, 12-bit analog-to-digital converter with shutdown. The circuit, as shown, allows digitization of input current from approximately –3A to approximately 2A with 12-bit resolution.

Figure 1. LT1787 Connected to LTC1404 ADC: Bidirectional Current-to-Bits Converter.

Figure 1. LT1787 Connected to LTC1404 ADC: Bidirectional Current-to-Bits Converter.

The LT1787’s output voltage is buffered by the LT1783, filtered and applied to the LTC1404’s AIN pin. The precision bias voltage applied to the VBIAS pin of the LT1787 is obtained from the LTC1404’s reference output and is typically 2.43V. This bias voltage sets the zero-current output of the LT1787 to 2.43V, or approximately mid-range for the A-to-D converter, allowing measurement of current in both the positive and negative directions. Note that the LTC1404’s internal reference voltage is 4.096V; thus the output of the converter is 1 count per millivolt of input voltage from the LT1787’s output, or 8 counts/mV of input voltage across RSENSE. Zero sense-current translates to 2.43V or 2430 counts from the converter. Full-scale positive current is 4096 counts and full-scale negative current is 0 counts.

Figure 2 shows current versus output code for the complete system. The LTC1404 has a digital interface consisting of the CLK and CONV input and the DOUT serial digital output. The signals provide wide flexibility in allowing the part to be interfaced to most microprocessors and DSPs.

Figure 2. Current vs Output Code.

Figure 2. Current vs Output Code.

The output voltage, VOUT, of the LT1787 is related to the input sense voltage by the following relationships:

VSENSE = ISENSE • RSENSE

VOUT = 8(VSENSE) + VBIAS

Although a –3A to 2A range was selected for this illustration, other current ranges can be accommodated by a simple change in value of the sense resistor. The correct RSENSE value is derived so that the product of the maximum sense current and the sense resistor value is equal to the desired maximum sense voltage(250mV for 12-bit resolution). For instance, the value of the sense resistor to sense a maximum current of 10A is 250mV/10A = 0.025Ω. The smallest measurable current is then 10A/4096 counts = 2.44mA/count. If only10-bit resolution is desired, then the full-scale voltage can be reduced to 60mV and RSENSE reduced to 0.006Ω. Ensure that the power dissipated in the sense resistor, IMAX2 • RSENSE, does not exceed the maximum power rating of the resistor.

Conclusion

The LT1787 high side current sense amplifier provides an easy-to-use method of sensing current with 12-bit resolution for a multiplicity of application areas. The part can operate to 60V, making it ideal for higher voltage systems in telecom or industrial applications. Additionally, the part can fi nd application in battery-powered, handheld equipment and computers, where the need for gauging the amount of current consumed and/or the amount of charge remaining in the battery is critical.

Theory of Operation (See Figure 3)

Inputs VS+ and VS apply the sense voltage to matched resistors RG1 and RG2. The opposite ends of resistors RG1 and RG2 are forced to be at equal potentials by the voltage gain of amplifier A1. The currents through RG1 and RG2 are forced to flow through transistors Q1 and Q2 and are summed at node VOUT by the 1:1 current mirror. The net current from RG1 and RG2 flowing through resistor ROUT gives a voltage gain of eight. Positive sense voltages result in VOUT being positive with respect to pin VBIAS.

Pins VEE, VBIAS and VOUT may be connected in a variety of ways to interface with subsequent circuitry. Split supply and single supply output configurations are easily supported.

Supply current for amplifier A1 is drawn from the VS pin. The user may choose to include this current in the monitored current (through RSENSE) by careful choice of connection polarity.

Figure 3. LT1787 Functional Diagram.

Figure 3. LT1787 Functional Diagram.

Authors

Glen Brisebois

Glen Brisebois

Glen Brisebois is an applications engineer with the Signal Conditioning Group at Analog Devices in Silicon Valley. He attended the University of Alberta in Canada, achieving bachelor’s degrees in both physics and electrical engineering. He attempted monastic life for several years with both the Trappists and the Carthusians, but couldn’t stop thinking about circuits. He is now happily married with several children, and works a lot with circuits, but will sometimes advocate an ADC instead. His article “Signal Conditioning for High Impedance Sensors” at EDN magazine won the Best Article award of 2006.

Generic_Author_image

Richard Markell