Design Note 130: Power Supplies for Subscriber Line Interface Circuits

As the demand for world wide networking grows, so will the need for advanced data transmission products. In particular, ISDN services have become popular because of the recent development of the Internet. ISDN provides higher speed data transmission than standard modems used in PCs. Also, ISDN supports the standard telephone interface (voice and fax), which includes the Subscriber Line Interface Circuit. A Subscriber Line Interface Circuit requires a negative power supply for the interface and the ringer voltages. The power supplies described herein are designed for these applications. Specifically, these designs address the AMD79R79 SLIC device with on-chip ringing.

CIRCUIT DESCRIPTIONS

LT1171 Supplies –23.8V at 50mA and –71.5V at 60mA


Figure 1 shows a current mode flyback power supply using the LT1171CQ device. This current mode device has a wide input voltage range of 3V to 60V, current limit protection and an on-chip 65V, 0.30Ω bipolar switch. The input voltage range for the circuit is 9V to 18V. This circuit is intended for small wall adapters that power ISDN boxes. The output voltages are –23.8V at 50mA and –71.5V at 60mA.

Figure 1.

Figure 1.

The circuit shown in Figure 1 uses the LT1171 in standard flyback topology. The transformer’s turns ratio is 1:1:1:1, where 23.8V appears across each secondary winding and the primary during the switch off time. The remaining secondary windings are stacked in series to develop –47V. The –47V section is then stacked onto the –23.8V section to get –71.5V. This technique provides very good cross regulation, lowers the voltage rating required on the output capacitors and lowers the RMS currents, allowing the use of cheaper output capacitors. Either the –23.8V output or the –71.5V output can be at full load without effecting the other corresponding output. The circuit’s step response is very good; no significant overshoot occurs after either output is shorted and released. Also, the transformer windings are all quadrafilar to lower the leakage inductance and cost.


LT1269 Supplies –23.5V at 60mA and –71.5V at 120mA from 5V Input


Figure 2 shows a current mode flyback power supply using the LT1269CQ device. This current mode device has a wide input voltage range, current limit protection and an onboard 60V, 0.20Ω bipolar switch. The input voltage range for the circuit is 5V to 18V. This design provides a wider input voltage range and greater output power than that of Figure 1. The output voltages are –23.5V at 60mA and –71.5V at 120mA (8.6W). This circuit is designed to power two SLIC devices. The circuit operation is identical to Figure 1, except for a larger switching regulator device (VR1) and a different transformer (T1). These changes allow for 5V operation and higher output power. This circuit is designed for full load on the –71V or –23.5V output. This accommodates the ringing on two SLICs or off hook on two SLICs. R5 and R6 are preload resistors for maintaining an accurate –23.5V output at full load with the –71V output at minimum load.

Figure 2.

Figure 2.

LAYOUT AND THERMAL CONSIDERATIONS

Printed circuit board layout is an important consideration in the design of switching regulator circuits. A good ground plane is required for all ground connections. The path from the input capacitor to the primary winding of the transformer is a high current path, and requires a short, wide copper trace (0.080" to 0.1"). The VSW pin connection also needs a short, wide copper trace. R1 and C2 need to be placed close to VR1. The secondary windings can be connected to their associated components with 0.025" to 0.030" traces. The feedback circuitry needs to be placed close to the FB pin of VR1. Place C5 close to U1 to decouple the op amp power supply. The LT1171CQ and LT1269CQ are surface mount devices that require about a 1" copper pad for heat sink mounting. Heat sinking is most critical for the LT1269CQ because of its high output power. Also, vias from the copper pad to the internal ground layers are highly recommended.

BILL OF MATERIALS

A bill of materials has been provided with each schematic.

Figure 1 Bill of Materials
Reference Designator Quantity Part Number Description Vendor Telephone
C1* 1 ECA-1VFQ331 Capacitor, 330μF, 35V HFQ Panasonic  
C2, C5 1 0805 Capacitor, 0.33μF Ceramic    
C3 1 UPL1V121MPH Capacitor, 120μF, 35V Plastic Nichicon (708) 843-7500
C4 1 UPL1J680MPH Capacitor, 68μF, 63V Plastic Nichicon  
C6 2 0805 Capacitor, 0.01μF    
D1 1 P6KE-43A (MOT), TGL41-43A (GI) Diode, 0.5W Zener Motorola or Equiv  
D2 1 1N5817 Diode, 1A Schottky Motorola or Equiv  
D3, D4 2 MURS120 Diode, Ultrafast Motorola or Equiv  
D5 1 1N4687, MMSZ4V3T1 Diode, Zener Motorola or Equiv  
D6 1 MBRS1100T3 Diode Motorola or Equiv  
R1, R4 2 0805 Resistor, 1k, 5% SMT    
R2 1 0805 Resistor, 71.5k, 1% SMT    
R3 1 0805 Resistor, 1.24k, 1% SMT    
T1* 1 PE-68488 Transformer Pulse Eng  
U1 1 LT1006S8 IC LTC (408) 432-1900
VR1* 1 LT1171CQ IC LTC (408) 432-1900
* Changes and Additions for Figure 2’s Circuit
C1 1 205A100M Capacitor, 100μF, 20V OS-CON Sanyo (619) 661-6835
D5, D7 2 1N4001 Diode    
R5, R6 2   Resistor, 50k 0.25W SMT or Through Hole    
T1 1 HMOO-96553 Transformer BI Technology (714) 447-2656
VR1 1 LT1269CQ IC LTC (408) 432-1900

Author

Eddie Beville

Eddie Beville

Eddie Beville is a power module design manager responsible for the design and development of the μModule® family. Eddie holds a BS in Electronic Engineering Technology from Chapman University, Orange, California. Eddie enjoys mountain biking, Tae Kwon Do and fishing.