How to use Multi-Function GPIs?
Abstract
The MAX77812 is a quad-phase, high-current, step-down (BUCK) converter for high-end gaming consoles, VR/AR headsets, DSLR cameras, drones, network switches and routers, and FPGA systems that use multicore processors. The MAX77812 has two user-programmable general-purpose inputs (GPIs) which can be configured as enable, output voltage selection, and low-power mode control input. This document provides information about using these GPIs.
Introduction
The MAX77812 has two general-purpose inputs (GPI0 and GPI1) which can be configured as the enable function of regulators, output voltage selection, low-power mode control, and ‘no function’. The function of these two inputs is programmable through the I2C/SPI (GPI_FUNC register) on the fly.
Enable Control
When GPIx are configured as the output-enable function, the enable logic of a specific regulator is an ‘OR’ logic of GPIx and the corresponding enable register bit (Mx_EN). For example, the default function of GPI0 is Master 3 Enable (GPI0_FUNC[3:0] = 0011b), so that Master 3 Enable is controlled by GPI0 and the M3_EN bit. If GPI0 is set high earlier than ‘Global Enable (EN)’ input, Master 3 is enabled earlier than other master phases, as shown in Figure 1. The two GPIs can be configured as the same enable function (e.g., M2_EN = GPI0_FUNC[3:0] = GPI1_FUNC[3:0] = 0010b). In this case, those inputs are ORed with the M2_EN bit. The GLB_EN function (GPIx_FUNC[3:0] = 0000b) allows the host processor to enable all the masters in sequence based on the STUP_DLYx registers. Note that M1 through M4 are defined by the PH_CFG0, PH_CFG1, and PH_CFG2 inputs.
Figure 1. Timing diagram with GPI0 and EN in a 2+1+1 phase configuration.
Voltage Selection
The MAX77812 BUCK has two additional output voltage control registers (Mx_VOUT_D[7:0] and Mx_VOUT_S[7:0]), besides Mx_VOUT[7:0]. Those two additional registers are for storing the default output voltage and the system sleep mode output voltage for a specific host processor.
When GPIx are configured as a voltage selection function, the output voltage of a specific regulator is set by Mx_VOUT_D[7:0] and Mx_VOUT_S[7:0] registers based on the GPIx logic level. For example, if the function of GPI0 is programmed as Global Voltage Selection (GPIx_FUNC[3:0] = 0101b), the output voltages of all the master phases are toggled by GPI0 based on the preset values in Mx_VOUT_D[7:0] (GPI0 = HIGH) and Mx_VOUT_S[7:0] (GPI0 = LOW) registers. In case the two GPIs are configured as the same voltage selection function, those inputs are ORed. During the output voltage transition, the ramp-up/down slew rate is controlled by the B_RU_SR[2:0] and B_RD_SR[2:0] registers.
Low-Power Mode
When GPIx are configured as a Low-Power Mode (LPM) enable function, the Low-Power Mode enable logic of a specific master phase is an ‘OR’ logic of GPIx and the corresponding enable register bit (Mx_LPM). For example, if GPI0_FUNC[3:0] = 1011b, the LPM enable of Master 1 is controlled by GPI0 and M1_LPM bit. In case the two GPIs are configured as the same LPM enable function (i.e., GPI0_FUNC[3:0] = GPI1_FUNC[3:0] = 1100b), those inputs are ORed with the M2_LPM bit. The GLB_LPM function (GPIx_FUNC[3:0] = 1010b) allows the host processor to enable Low-Power Mode for all the masters at the same time.
Address 0x0F |
Mode R/W |
Type: O | Reset Value: 0x43 | |||||||||||||||||
Bit | Name | POR | Description | |||||||||||||||||
7:4 | GPI1_FUNC[3:0] | 0100 |
GPI1 Function Selection
|
|||||||||||||||||
3:0 | GPI0_FUNC[3:0] | 0011 |
GPI0 Function Selection
|
GPIx_FUNC[3:0] | Function | Remark |
0000b | GLB_EN | Global Enable (Master 1 thru to Master 4) |
0001b | M1_EN | Master 1 Enable |
0010b | M2_EN | Master 2 Enable |
0011b | M3_EN | Master 3 Enable |
0100b | M4_EN | Master 4 Enable |
0101b | GLB_VSEL | Global Voltage Selection (Master 1 thru Master 4) |
0110b | M1_VSEL | Master 1 Voltage Selection |
0111b | M2_VSEL | Master 2 Voltage Selection |
1000b | M3_VSEL | Master 3 Voltage Selection |
1001b | M4_VSEL | Master 4 Voltage Selection |
1010b | GLB_LPM | Global Low Power Mode Select (Master 1 thru Master 4) |
1011b | M1_LPM | Master 1 Low Power Mode Enable |
1100b | M2_LPM | Master 2 Low Power Mode Enable |
1101b | M3_LPM | Master 3 Low Power Mode Enable |
1110b | M4_LPM | Master 4 Low Power Mode Enable |
1111b | No Function |