AN-1317: Rolling Data Buffer on the ADF7024
Introduction
When the ADF7024 receives a packet, it stores the data in a linear sequence in the packet RAM. Prior to transmission, the data to be transmitted is written to the packet RAM in a linear sequence. This functionality is described in the ADF7024 Reference Manual, UG-698. (The ADF7024 Reference Manual, UG-698, is included in the ADF7024 design resource package, which is available for download on the ADF7024 product page.) The ADF7024 packet RAM is 240 bytes long. If the packet length is greater than 240 bytes, additional measures are required. This application note describes a method for handling longer packet lengths on the ADF7024, up to a maximum length of 65,535 bytes, via a rolling buffer mechanism. This method reuses and renames several registers of the ADF7024.
Tx/Rx Rolling Data Buffer
In rolling buffer mode, packet RAM locations Address 0x020 to Address 0x0FF are available for packet data. Packet RAM memory locations Address 0x000 to Address 0x01F are allocated for use by the ADF7024 and must not be used for packet data. When rolling buffer mode is not enabled, Address 0x000 to Address 0x00F are allocated for use by the ADF7024, and Address 0x010 to Address 0x0FF are available for packet data.
Rolling Buffer Registers
The registers to enable and configure the rolling buffer mode are outlined in Table 1. When the rolling buffer is enabled via the PKT_TESTMODES register (Address 0x139), the RADIO_ PROFILE_18 register to the RADIO_PROFILE_21 register (Address 0x134 to Address 0x137) take on the rolling buffer control mechanism and no longer form part of the radio profile.
Address (Hex) |
Register Name with Rolling Buffer Mode Disabled (Normal Operation) |
Register Name with Rolling Buffer Mode Enabled |
Description |
0x124 | PKT_TX_BASE_ADR | PKT_TX_BASE_ADR | Start address in the packet RAM for the transmit buffer. |
0x125 | PKT_RX_BASE_ADR | PKT_RX_BASE_ADR | Start address in the packet RAM for the receive buffer. |
0x134 |
RADIO_PROFILE_18 | BB_RX_BUFFER_SIGNAL | Location in the packet RAM for the receive buffer nearly full signal. |
0x135 | RADIO_PROFILE_19 | BB_RX_BUFFER_SIZE | Receive buffer size in bytes. |
0x136 | RADIO_PROFILE_20 | BB_TX_BUFFER_SIGNAL | Location in the packet RAM for the transmit buffer nearly full signal. |
0x137 | RADIO_PROFILE_21 | BB_TX_BUFFER_SIZE | Transmit buffer size in bytes. |
0x139 | PKT_TESTMODES | PKT_TESTMODES | Enable/disable the transmit and receive rolling buffer mode. See Table 3. |
Rolling Buffer Interrupts
Use the interrupts defined in Table 2 for rolling buffer operation. The normal operation of the INTERRUPT_SWM_ RSSI_DET interrupt is not available when rolling buffer mode is enabled because this interrupt is replaced with the INTERRUPT_ BUFFER_FULL interrupt. When rolling buffer mode is disabled, the INTERRUPT_SWM_RSSI_DET interrupt is again available and operates as described in the ADF7024 Reference Manual, UG-698. (The ADF7024 Reference Manual, UG-698, is included in the ADF7024 design resource package, which is available for download on the ADF7024 product page.)
Address | Bit | Interrupt Name in Normal Operation |
Interrupt Name with Rolling Buffer Mode Enabled |
Description |
INTERRUPT_MASK_0, Address 0x100 and INTERRUPT_SOURCE_0, Address 0x336 |
6 | INTERRUPT_SWM_RSSI_DET | INTERRUPT_BUFFER_FULL | Asserted in the INTERRUPT_ SOURCE_0 register when the receive or transmit buffer is full. To enable this interrupt source and to mirror the interrupt on the IRQ_GP3 pin, set this bit to Logic 1 in the INTERRUPT_ MASK_0 register. |
5 | Reserved | INTERRUPT_BUFFER_ALMOST_FULL | Asserted in the INTERRUPT_ SOURCE_0 register when the receive or transmit buffer is almost full. To enable this interrupt source and to mirror the interrupt on the IRQ_ GP3 pin, set this bit to Logic 1 in the INTERRUPT_MASK_0 register. |
Bit | Bit Name in Normal Operation |
Bit Name with Rolling Buffer Mode Enabled |
Description |
5 | Reserved | ROLLING_BUFFER_PACKET_RX | 1 is enable receive rolling buffer. 0 is normal operation. |
4 | Reserved | PAYLOAD_ONLY_PACKET_TX | 1 is enable transmit payload only rolling buffer. 0 is normal operation. |
Address (Hex) |
Name in Normal Operation |
Name with Rolling Buffer Mode Enabled |
Description |
0x014 | Available for packet data | TRX_BYTE_LOW | Bits[7:0] of MAX_ROLLING_BUFFER_LEN[15:0], the lower byte of the packet length control register. |
0x015 | Available for packet data | TRX_BYTE_HIGH | Bits[15:8] of MAX_ROLLING_BUFFER_LEN[15:0], the upper byte of the packet length control register. |
Rolling Buffer: Transmit Mode
Set Bit 4 of the PKT_TESTMODES register (Address 0x139) to 1 to enable only the payload rolling buffer in transmit mode. This mode allows the user to transmit a packet of up to 65,535 bytes long using a custom packet structure. The maximum transmit length is programmable up to 0xFFFF by setting the MAX_ ROLLING_BUFFER_LEN[15:0] value as defined in Table 4, which is defined locally in the packet RAM in the rolling buffer mode.
The number and type of preamble, sync, payload, and cyclic redundancy check (CRC) are no longer bounded by the ADF7024; instead, the ADF7024 transmits what is placed in the transmit buffer. In this mode, the data in the transmit buffer is sent over the air until the MAX_ROLLING_BUFFER_LEN[15:0] number of bytes are sent, or a command is issued
In transmit mode, the start of the rolling buffer in the packet RAM is set by the PKT_TX_BASE_ADR register. The size of the buffer is set by the BB_TX_BUFFER_SIZE register. The buffer size must not exceed the available packet RAM.
Set the value in the BB_TX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is generated prior to the transmission of all the data in the buffer. Typically, the BB_TX_BUFFER_SIGNAL register is set so that the interrupt is asserted when half the data in the buffer is transmitted.
When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host processor writes new data to the packet RAM, starting at the address value PKT_TX_BASE_ADR and ending at the address value, PKT_TX_BASE_ADR + BB_TX_ BUFFER_SIGNAL.
When the data in the last byte of the transmit buffer is transmitted, the ADF7024 continues transmitting, starting with the data pointed to by the PKT_TX_BASE_ADR register. If enabled, an INTERRUPT_BUFFER_FULL interrupt is asserted when the last byte in the buffer is transmitted.
When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host processor must write new data to the packet RAM, starting at the address value, PKT_TX_BASE_ADR + BB_TX_ BUFFER_SIGNAL + 1, and finishing at the address value, PKT_TX_BASE_ADR + BB_TX_BUFFER_SIZE.
Transmission of data continues until the MAX_ROLLING_ BUFFER_LEN[15:0] number of bytes are sent (TX_EOF), or the user issues the CMD_PHY_ON command.
Figure 1. Rolling Buffer in Transmit Mode.
Rolling Buffer: Receive Mode
Set Bit 5 of the PKT_TESTMODES register (Address 0x139) to 1 to enable the rolling buffer in receive mode. The ADF7024 can receive packet lengths up to 216 − 1 bytes long (65,535 bytes) via the rolling buffer mechanism. The maximum packet length is programmable up to 0xFFFF by setting the MAX_ROLLING_ BUFFER_LEN[15:0] value as defined in Table 4.
When Bit 5 of the PKT_TESTMODES register (Address 0x139) is set and the sync word is received, the packet handler uses the rolling buffer to capture the remainder of the packet.
In receive mode, the PKT_RX_BASE_ADR register sets the address pointer for the start of the rolling buffer in the packet RAM. Set the size of the buffer using the BB_RX_BUFFER_ SIZE register. The buffer size must not exceed the available packet RAM size. When the value in the BB_RX_BUFFER_ SIZE register is added to the address in the PKT_RX_BASE_ ADR register, it must not exceed 0x0FF.
Set the value in the BB_RX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted prior to the buffer being filled by the received data. Typically, the BB_RX_BUFFER_SIGNAL register is set so the interrupt is asserted when half the buffer is filled with received data.
When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host processor reads the data from the packet RAM, starting at the address value PKT_RX_BASE_ADR and ending at the address value, PKT_RX_BASE_ADR + BB_RX_ BUFFER_SIGNAL.
When the last byte of the receive buffer is filled, the ADF7024 continues to write the received data, starting at the address value PKT_RX_BASE_ADR. If enabled, an INTERRUPT_BUFFER_ FULL interrupt is asserted when the buffer is filled.
When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host processor must read the data from the packet RAM, starting at the address value, PKT_RX_BASE_ADR + BB_RX_ BUFFER_SIGNAL + 1, and ending at the address value, PKT_RX_BASE_ADR + BB_RX_BUFFER_SIZE.
Reception of data continues until the length programmed in the MAX_ROLLING_BUFFER_LEN[15:0] value is achieved (RX_EOF), or the host processor issues the CMD_PHY_ON command.
Note that it is up to the host processor to detect the end of the payload and perform an error checking operation on the data, such as CRC.
Figure 2. Rolling Buffer in Receive Mode.