ADALM2000 Activity: Common Emitter Amplifier

Objective:

The purpose of this activity is to investigate the common emitter configuration of the bipolar junction transistor (BJT).

Background

The common emitter amplifier is one of three basic single-stage amplifier topologies. The BJT version functions as an inverting voltage amplifier. The base terminal of the transistor serves as the input, the collector is the output, and the emitter is common to both input and output (it may be tied to the ground reference or the power supply rail), which gives rise to its common name.

Materials:


  • ADALM2000 active learning module
  • Solderless breadboard
  • Five resistors
  • One 50 kΩ variable resistor, potentiometer
  • One small signal NPN transistor (2N3904)

Directions

The configuration, shown in Figure 1, demonstrates the NPN transistor used as the common emitter amplifier. Output load resistor RL is chosen such that for the desired nominal collector current, IC, approximately one half of the VP (5 V) voltage appears at VCE. Adjustable resistor RPOT, along with RB, sets the nominal bias operating point for the transistor (IB) to set the required IC. Voltage divider R1/R2 is chosen to provide a sufficiently large attenuation of the input stimulus from waveform generator W1. This is done to more easily view the generator W1 signal, given the rather small signal that will appear at the base of the transistor, VBE. The attenuated waveform generator W1 signal is ac-coupled into the base of the transistor by the 4.7 μF capacitor so as not to disturb the dc bias condition.

Figure 1. Common emitter amplifier test configuration.
Figure 1. Common emitter amplifier test configuration.

Hardware Setup

The waveform generator output W1 should be configured for a 1 kHz sine wave with 3 V amplitude peak-to-peak and 0 V offset. The setup should be configured with Scope Channel 1+ connected to display the output W1. Scope Channel 2 (2+) is used to measure alternately the waveform at the base and collector of Q1.

Figure 2. Common emitter amplifier test configuration breadboard connection.
Figure 2. Common emitter amplifier test configuration breadboard connection.

Procedure

Turn on the power supplies connected to the collector (VP = 5 V) of the BJT transistor.

Configure the oscilloscope instrument to capture several periods of the input signal and the output signal.

Plot examples of the simulated circuit using LTspice® are presented in Figure 3 and Figure 4.

Figure 3. Common emitter amplifier test configuration, VIN and VCE.
Figure 3. Common emitter amplifier test configuration, VIN and VCE.
Figure 4. Common emitter amplifier test configuration, VIN and VBE.
Figure 4. Common emitter amplifier test configuration, VIN and VBE.

The voltage gain, A, of the common emitter amplifier can be expressed as the ratio of load resistor RL to the small signal emitter resistance, re. The transconductance, gm, of the transistor is a function of the collector current IC and the so-called thermal voltage, kT/q, which can be approximated by around 25 mV or 26 mV at room temperature.

Equation 1

The small signal emitter resistance is 1/gm and can be viewed as being in series with the emitter. Now with a signal applied to the base , the same current (neglecting base current) flows in re and the collector load RL. Thus, gain A is given by the ratio of RL to re.

Equation 2

An alternative to produce a common emitter amplifier test circuit is shown in Figure 5. All the attributes are basically the same with two slight advantages. One is that the base current bias is no longer dependent on the exponential base voltage (VBE). The second is that the summation of the small ac signal from the attenuated AWG 1 output is independent of the base bias circuit and does not need to be ac-coupled. The small signal ac input is applied to the non-inverting terminal of the operational amplifier (op amp), and thus, due to the negative feedback, also appears at the base of the transistor (inverting op amp input).

Figure 5. Alternate common emitter amplifier test configuration.
Figure 5. Alternate common emitter amplifier test configuration.
Figure 6. Alternate common emitter amplifier test configuration breadboard connection.
Figure 6. Alternate common emitter amplifier test configuration breadboard connection.
Figure 7. Alternate common emitter amplifier test configuration, VIN and VBE.
Figure 7. Alternate common emitter amplifier test configuration, VIN and VBE.
Figure 8. Alternate common emitter amplifier test configuration VBE zoom.
Figure 8. Alternate common emitter amplifier test configuration VBE zoom.

Self-Biased Configuration with Negative Feedback

Objective

The purpose of this section is to investigate the effect of adding negative feedback to stabilize the dc operating point. One of the most frequently used biasing circuits for a transistor circuit is the self-biasing of the emitter-bias circuit where one or more biasing resistors are used to set up the initial dc values for the three transistor currents, IB, IC, and IE.

Figure 9. Self-biased configuration.
Figure 9. Self-biased configuration.

Hardware Setup

The waveform generator output W1 should be configured for a 1 kHz sine wave with 3 V amplitude peak-to-peak and 0 V offset. The setup should be configured with Scope Channel 1+ connected to display the output W1. Scope Channel 2 (2+) is used to alternately measure the waveform at the base and collector of Q1.

Figure 10. Self-biased configuration breadboard connection.
Figure 10. Self-biased configuration breadboard connection.

Procedure

Turn on the power supplies connected to the collector (VP = 5 V) of the BJT transistor.

Configure the oscilloscope instrument to capture several periods of the input signal and the output signal.

Plot examples of the simulated circuit (using LTspice) are presented in Figure 11 and Figure 12.

Figure 11. Self-biased configuration, VIN and VCE.
Figure 11. Self-biased configuration, VIN and VCE.
Figure 12. Self-biased configuration, VIN and VBE.
Figure 12. Self-biased configuration, VIN and VBE.

Adding Emitter Degeneration

Objective

The purpose of this activity is to investigate the effect of the addition of emitter degeneration.

Background

Common emitter amplifiers give the amplifier an inverted output and can have a very high gain and can vary widely from one transistor to another. Additionally, the gain is somehow unpredictable due to temperature and bias current dependence. By introducing a small value feedback resistor in the amplifier stage, the performance of the circuit can be improved.

Additional Materials

One 5 kΩ variable resistor, potentiometer

Directions

Disconnect the emitter of Q1 from ground and insert RE, a 5 kΩ potentiometer, as shown in Figure 13. Adjust RE while noting the output signal seen at the collector of the transistor.

Figure 13. Emitter degeneration added.
Figure 13. Emitter degeneration added.

Hardware Setup

The waveform generator output W1 should be configured for a 1 kHz sine wave with 3 V amplitude peak-to-peak and 0 V offset. The setup should be configured with Scope Channel 1+ connected to display output W1. Scope Channel 2 (2+) is used to alternately measure the waveform at the base and collector of Q1.

Figure 14. Emitter degeneration added breadboard connection.
Figure 14. Emitter degeneration added breadboard connection.

Procedure

Turn on the power supplies connected to the collector (VP = 5 V) of the BJT transistor.

Configure the oscilloscope instrument to capture several periods of the input signal and the output signal.

Plot examples of the simulated circuit (using LTspice) are presented in Figure 15 and Figure 16.

Figure 15. Emitter degeneration added, VIN and VCE.
Figure 15. Emitter degeneration added, VIN and VCE.
Figure 16. Emitter degeneration added, VIN and VBE.
Figure 16. Emitter degeneration added, VIN and VBE

Increasing AC Gain of an Emitter Degenerated Amplifier

Adding the emitter degeneration resistor has improved the stability of the dc operating point at the lower cost amplifier gain. A higher gain for ac signals can be restored to some extent by adding capacitor C2 across the degeneration resistor RE, as shown in Figure 17.

Figure 17. C2 added to increase ac gain.
Figure 17. C2 added to increase ac gain.

Hardware Setup

The waveform generator output W1 should be configured for a 1 kHz sine wave with 3 V amplitude peak-to-peak and 0 V offset. The setup should be configured with Scope Channel 1+ connected to display the output W1. Scope Channel 2 (2+) is used to alternately measure the waveform at the base and collector of Q1.

Figure 18. Breadboard connection with C2 added to increase the ac gain.
Figure 18. Breadboard connection with C2 added to increase the ac gain.

Procedure

Turn on the power supplies connected to the collector (VP = 5 V) of the BJT transistor.

Configure the oscilloscope instrument to capture several periods of the input signal and the output signal.

Plot examples of the simulated circuit (using LTspice ) are presented in Figure 19 and Figure 20.

Figure 19. C2 added to increase the ac gain, VIN and VCE.
Figure 19. C2 added to increase the ac gain, VIN and VCE.
Figure 20. C2 added to increase the ac gain, VIN and VBE.
Figure 20. C2 added to increase the ac gain, VIN and VBE.

Questions

  • For the common emitter amplifier circuit setup, what is the effect on the voltage gain, A, by increasing RL?

You can find the answer at the StudentZone blog.

Authors

Doug Mercer

Doug Mercer

Doug Mercer received his B.S.E.E. degree from Rensselaer Polytechnic Institute (RPI) in 1977. Since joining Analog Devices in 1977, he has contributed directly or indirectly to more than 30 data converter products and holds 13 patents. He was appointed to the position of ADI Fellow in 1995. In 2009, he transitioned from full-time work and has continued consulting at ADI as a fellow emeritus contributing to the Active Learning Program. In 2016, he was named engineer in residence within the ECSE department at RPI.

Antoniu Miclaus

Antoniu Miclaus

Antoniu Miclaus is a software engineer at Analog Devices, where he works on embedded software for Linux and no-OS drivers, as well as ADI academic programs, QA automation, and process management. He started working at ADI in February 2017 in Cluj-Napoca, Romania. He holds an M.Sc. degree in software engineering from the Babes-Bolyai University and a B.Eng. degree in electronics and telecommunications from the Technical University of Cluj-Napoca.