QUESTION:
Is it possible to design a complete RTD module with overvoltage protection?

Answer:
Introduction
RTD (resistance temperature detectors) can provide excellent stability and accuracy, and reduce the impacts of noise and interference. RTD sensors can be made up of either 2-wire, 3-wire, or 4-wire versions, and require an excitation current to produce an output voltage. AD7124-4/AD7124-8 contain two well matched current sources, a PGA, reference buffers, and diagnostic functions, which are ideally suited for high reliability RTD modules.
Incorrect operations, careless connections, and exposed wires usually lead to overvoltage faults in industrial circumstances, which will damage the electronic devices and cause undesirable consequences that may flow from the damage. Overvoltage protection ability is a key specification for an RTD module. Outside of transient overvoltage protection, durable overvoltage protection must be considered during actual production.
This article will focus on hot to provide a total solution for multiwire RTD modules with overvoltage protection function, which is based on AD7124, and overvoltage protection and detection multiplexers and channel protectors. This article can help designers understand this method and choose appropriate devices.
For overvoltage protection functions, here are three optional solutions:
- Using series resistors in front of the pins of an ADC can help protect the AD7124 easily. These pins include analog input and excitation output pins, but the resistors will limit compliance voltage.
- The protection of current source can be realized by discrete components. This solution can achieve higher overvoltage protection and larger voltage compliance. However, the switches and multiplexers are still externally exposed.
- ADI’s overvoltage protection and detection switches, multiplexers, and channel protectors (ADG52xxF and ADG54xxF) can be used for RTD module protection and different wires RTD sensor switching. These parts can provide ±55 V fault voltage protection in both the powered and unpowered mode, and can implement fault detection with latch-up immunity. Their high density package occupies a much smaller PCB area than traditional solutions.
RTD Module Based on AD7124
Ratiometric measurement is widely used in RTD modules, as it can remove the error and drift of the excitation current source. Figure 1 shows the typical diagram for 4-wire RTD measurement based on AD7124-8.

AIN0 provides the excitation current, and the AD7124 integrated reference buffer and PGA, REFIN and AIN are high impedance inputs, so the same current flows through the RTD sensor and reference resistor. The ADC conversion result is the ratio between input voltage (VRTD) and reference voltage (VREF), which is equal to the ratio between RRTD and RREF. If RREF is a known, high precision, and stable reference resistor, RRTD can be calculated by the RREF value and ADC conversion result.
By using a 4-wire RTD configuration, the system can achieve high accuracy and reliability and the error due to lead wire resistance can be removed. Accordingly, the cost is higher than a 3-wire or 2-wire configuration. Figure 2 shows the 3-wire RTD measurement based on AD7124, which is a compromise between performance and cost.

Two integrated, well matched current sources are helpful for 3-wire RTD measurement. VREF and VRTD can be expressed by the following two functions:

AD7124 has two well matched current sources, which means IEXC0 is near or equal to IEXC1 and the lead resistors RL1 and RL2 are very similar. The functions can be expressed as:

Express the conversion code as a composition of these two functions:

According to this function, the RTD resistor value can be calculated by the conversion result and reference resistor value. Please refer to CN-0383 for details.
For a 2-wire RTD, the error due to lead resistance can’t be cancelled, but the cost of these type RTD sensors is lower than the others, and AD7124-8 can be configured as a 2-wire RTD sensor, as seen in Figure 3.

In practice, many industrial customers ask for the same port of an RTD module to many different types of RTD sensors, which is convenient for balancing RTD sensors’ cost and performance. Figure 4 shows a universal interface of an RTD module, which can support different wires RTD sensors.

Due to this requirement, this type of RTD module needs to be configured by firmware for differently wired RTD sensors easily. Figure 5 shows the block diagram for different wire RTD sensors based on one piece of the AD7124-8 and its switches. AD7124-8 can support a 4-channel, 2-wire/3-wire/4-wire RTD measurement.

Using a controller can change the configuration for different sensors easily, and Table 1 shows switches and current source status for different configurations.
S1 | S2 | S3 | IEXT1 | IEXT2 | |
2-wire RTD | Closed | Closed | Open | Enable | Disable |
3-wire RTD | Closed | Open | Closed | Enable | Enable |
4-wire RTF | Open | Open | Open | Enable | Disable |
Choosing appropriate resistor and capacitor value by calculation can optimize the noise performance. The article Analog Front-End Design Considerations for RTD Ratiometric Temperature Measurements can provide guidance. If, in addition to an optimized noise performance, overvoltage protection is needed in the field, the additional requirement will cause a lot of additional trouble.
First, some analog pins of AD7124 are directly exposed to outside environments, and according to the absolute maximum ratings of AD7124 under 25°C, the analog input voltage to AVSS should between −0.3 V to AVDD +0.3 V, which means this module can’t defend high overvoltage occur. Secondly, three switches need to bear high voltage.
Adding Current Limiting Resistors
Adding current limiting resistors on every pin of AD7124 can provide overvoltage protection for AD7124 easily.

Figure 6 shows the AD7124 analog pin architecture. There are two clamping diodes on every analog pin and we can use these diodes to implement protection directly without introducing any other leakage current.
Figure 7 shows the diagram of this method—R1 to R4 are in front of AIN1, AIN2, REF+, and REF– separately. This setup is used for noise elimination. These resistors can be used for current limit at the same time and adding current limiting resistors in front of AIN0 and AIN3 can protect the rest of exposed analog pins of AD7124.

These resistors and the internal clamping diodes can protect against some level of positive and negative overvoltage. When positive or negative overvoltage fault occurs, the current will flow through the resistors and internal clamping diodes to AVDD or AVSS. The current value must be limited to less than 10 mA, according to the absolute specification of AD7124. If RLimit is equal to 3 kΩ, this module can prevent ±30 V durable overvoltage.
However, there would be a voltage drop on RLIMIT when this module works in a normal mode. If the excitation current was 500 μA, the voltage drop on RLIMIT would be 1.5 V, the resistance of sensor and RREF would be limited. Increasing RLIMIT can get better protection, but the resistance range will be smaller. The compliance voltage will decrease along with the increasing overvoltage protection requirement based on this protection method. If the power consumption of RREF and RReturn is taken care of, the fault voltage will directly drop on these two resistors.
Except for AD7124-8 analog pins, the switches are exposed under the high voltage too, so we should choose the parts that can defend ±30 V voltage. In the past few years, photo MOS and relay have been used in these situations, but the high price and large package limit the sphere of application.
Using Discrete Transistors to Protect the Current Source
The biggest weakness of using limit resistors is that the compliance voltage on SOURCE+ is low. Using discrete transistors and diodes can implement overvoltage protection and increase the max allowed voltage on SOURCE+ pin. Figure 8 shows the diagram for this method.

This architecture can keep the excitation current flow to the RTD sensor in a normal situation and defend against high overvoltage damage. The other analog input pins can be protected by current limiting resistors, since analog input pins have no compliance voltage limitation.
If a large positive voltage is applied to this RTD sensor, D1 prevents the current source from positive high voltage. If a large negative voltage is applied to this RTD sensor, the PN junction between Q1’s collector and base is in reverse biased, causing high voltage drops on RB1 and this PN junction, which can prevent damage to AIN0.
In the normal mode, D2 functions as a reverse biased diode, which keeps the current flow through this part very small. There is very little current flow throw Q1’s emitter to base, so the voltage drop on RB1 can be neglectful. This method can keep compliance voltage higher than using current limiting resistors and defend much higher fault voltage.
Using Analog Switches and Multiplexers with Overvoltage Protection Function
The weaknesses of using discrete components to protect this high precision RTD module are obvious—it’s not easy to choose appropriate components; these parts makes the protection circuit complicated; and they occupy a large PCB area.
Even though the leakage current of AD7124 analog input pins is quite small, the large resistor series on these pins, such as R1 and R2, will produce notable error, and the thermal noise of these resistors decrease the resolution. In an actual design, the RTD module may have multiple channels, the current source would switch from one channel to the other, a large resistor value increases the settling time of analog input RC combination, and a RTD module should spend more time on charging the capacitors, such as C1, C2, and C3. It’s hard to balance protection functions and accuracy. And the switches still need to protect against high overvoltage too.
In this case, using analog switches and multiplexers with fault protection can provide switch and overvoltage protection. Figure 9 shows an example.

In Figure 9, there are three SPDT switches using the ADG5243F in front of the AD7124, and two variable resistors using ADG5462F in front of AIN1 and AIN2. These components can be implemented by using ADG5243F and ADG5462F, which have user-defined fault protection and detection functions.
The highlight feature of these parts are:
- The source pins are protected against voltages greater than the secondary supply rails, from –55 V and +55 V.
- The source pins are protected against voltages between –55 V and +55 V in an unpowered state.
- Overvoltage detection with the digital output indicates the operating state of the switches.
- Trench isolation guards against latch-up.
- Optimized for low charge injection and on-capacitance.
- The ADG5243F can be operated from a dual supply of ±5 V to ±22 V or a single power supply of 8 V to 44 V.
Latch-up immunity with low leakage current and industry-leading RON flatness are the advantages of these parts too. Low leakage and low conductive resistance can improve the accuracy and noise performance of this RTD module.
If a positive or negative voltage is applied to the RTD interface, the voltage on the drain pins will be clamped at POSFV + VT or NEGFV – VT. If the POSFV is set to 4.5 V and the NEGFV is set to AGND, the resistor series in the route, which is used for protecting AD7124, is much easier to choose. If the overvoltage occurs during unpowered state, the switches stay in a high impedance state and help prevent damage to the parts.
The detection function of these parts can be used for system diagnostics. The voltages on the source inputs of ADG5243F and ADG5462F are continuously monitored. An active low digital output pin, FF, indicates the state of the switches. The voltage on the FF pin indicates if any of the source input pins are experiencing a fault condition. AD7124 offers many strong diagnostic functions for system safety. The processor can combine the diagnostic functions of these parts to build a much more robust system.
Summary
The functional blocks and diagnostic functions in AD7124 improve the accuracy and robustness. After comparing three overvoltage protection methods in RTD module, using analog switches and multiplexers with overvoltage protection functionality has many advantages:
- Making RTD modules endure higher fault voltage
- Low leakage current, low noise, and short settling time
- Replacing traditional relay and photo MOS, saving PCB area and cost
- Diagnostic functionality enhances system robustness
- Easy to use