The LTC2185 is a 125 MSPS, 16-bit ADC with excellent noise and linearity performance while only consuming 185 mW per channel. It is ideal for demanding, low power applications that require excellent ac performance. A high performance ADC like the LTC2185 requires a high performance amplifier driving it to maintain its excellent performance. The ADA4927-1 delivers the linearity performance required by the LTC2185 while only consuming 215 mW. The well designed package of the ADA4927-1 allows for a simple layout that reduces parasitic capacitance in the feedback path that can erode the phase margin of the amplifier. This combination of ADC and driver allows for excellent performance from 62.5 MHz to 125 MHz a region, where other high speed amplifiers are lacking.
The LTC2185 is a 2-channel, simultaneous sampling parallel ADC that offers a choice of full-rate CMOS or double data rate (DDR) CMOS/LVDS digital outputs. Pin-compatible speed grade options include 25 MSPS, 40 MSPS, 65 MSPS, 80 MSPS, and 105 MSPS with approximate power dissipation of just 1.5 mW/MSPS per channel. It includes popular features such as the digital output randomizer and alternate bit polarity (ABP) mode that minimize digital feedback when using parallel CMOS outputs. Analog full power bandwidth of 550 MHz and ultralow jitter of 0.07 ps rms allow under-sampling of IF frequencies with excellent noise performance. To maintain this level of performance, the LTC2185 needs to be driven with an appropriate amplifier like the ADA4927-1.
The ADA4927 is a high speed, differential current feedback amplifier. Fabricated on Analog Devices’ silicon-germanium process, the ADA4927-1 has excellent distortion and an input voltage noise of only 1.3 nV√Hz. This allows it to drive high speed ADCs like the LTC2185. The gain of the ADA4927-1 is set with external feedback resistors located next to the input pins. By keeping the feedback pins and input pins close on the package, the ADA4927-1 provides a clean layout and minimizes the parasitic capacitance in the feedback network. This makes the ADA4927-1 an ideal choice for driving high performance ADCs, like the LTC2185, from dc to 125 MHz.
Figure 1 shows a schematic of the ADA4927-1 driving the LTC2185. The corresponding layout is shown in Figure 2. The feedback pins on the ADA4927-1 are adjacent to the input pins, which minimizes the parasitic capacitance of the feedback node and improves the phase margin of the amplifier. It also simplifies the layout by making it possible to place feedback resistors directly across the two pins and not having additional trace length in the feedback path. There is a simple filter between the amplifier and ADC that reduces the wideband noise of the amplifier and improves the SNR of the system. This filter also attenuates the sampling glitches from the ADC before they reach the amplifier. This helps keep the output network of the ADA4927 from oscillating in response to these glitches. This filter network can be modified to accommodate a wide range of input bandwidth requirements.


Figure 3 and Figure 4 show the SNR and SFDR of the LTC2185 and ADA4927-1 combination. The SFDR stays above 67 dB out to 125 MHz while the SNR is better than 63 dB to the same frequency. This combination only consumes 250 mW. With a sample rate of 125 MSPS, this combination provides good performance through the entire second Nyquist zone where other amplifiers begin to have poor linearity.


Using the ADA4927-1 to drive the LTC2185 provides excellent linearity while keeping the power consumption low. The fact that the ADA4927-1 stays very linear out to 125 MHz allows this ADC amplifier combination to be used in demanding communication and medical applications that require the use of the second Nyquist zone of the LTC2185. The pin out of the ADA4927-1 and filter design minimize the complexity of the layout while maintaining excellent performance on a low power budget.