iButton and Memory
searchIcon
banner background image

iButton and Memory

iButton® devices provide a unique solution for applications where information needs to travel with a person or an object, even in harsh environments. The silicon chip within the iButton device is laser etched with a unique and unalterable address and is protected by a highly durable stainless steel can. You can drop it, step on it, or scratch it. The lid and base of the can act as the contacts for the silicon chip. iButton devices are wear-tested for 10-year durability. Many iButton devices make use of the 1-Wire® serial protocol.
iButton® devices provide a unique solution for applications where information needs to travel with a person or an object, even in harsh environments. The silicon chip within the iButton device is laser etched with a unique and unalterable address and is protected by a highly durable stainless steel can. You can drop it, step on it, or scratch it. The lid and base of the can act as the contacts for the silicon chip. iButton devices are wear-tested for 10-year durability. Many iButton devices make use of the 1-Wire® serial protocol.

Subcategories

archive icon
iButton® devices are small, durably packaged modules with globally unique digital addresses. An iButton device uses a stainless steel can as an electronic communications interface. The iButton can has a data contact, called the lid, and a ground contact, called the base. Each of the iButton contacts is connected to the silicon chip inside. The iButton base includes a flange to simplify attaching the iButton device to just about anything. Enhanced by our 1-Wire® communications protocol, iButton devices provide the ability to deliver or record data where other products cannot, such as in very harsh environments. An iButton device is ideal for any application where information needs to follow a person or object, such as temperature and humidity data logging, access control, asset tracking, and electronic cash (eCash) transactions.
Arrow image
iButton® devices are small, durably packaged modules with globally unique digital addresses. An iButton device uses a stainless steel can as an electronic communications interface. The iButton can has a data contact, called the lid, and a ground contact, called the base. Each of the iButton contacts is connected to the silicon chip inside. The iButton base includes a flange to simplify attaching the iButton device to just about anything. Enhanced by our 1-Wire® communications protocol, iButton devices provide the ability to deliver or record data where other products cannot, such as in very harsh environments. An iButton device is ideal for any application where information needs to follow a person or object, such as temperature and humidity data logging, access control, asset tracking, and electronic cash (eCash) transactions.

Sub-subcategories

right arrow for link redirect right arrow for link redirect right arrow for link redirect right arrow for link redirect