ADI Multichannel Source Measurement Unit (SMU) Solution
ADI Multichannel Source Measurement Unit (SMU) Solution
A source measure unit (SMU) is widely used in the field of test and measurement. Examples of where it is used include I-V characteristic curve tests for semiconductors, parameter tests for various nonlinear devices or materials, and charge or discharge tests for various types of batteries. SMUs can operate in four quadrants of a V/I coordinate axis and can measure another type of signal while outputting one. The functions that used to be completed by multiple instruments can be now realized by a single SMU. Many well proven SMU products, commonly built with discrete devices, have been put on the market. These SMUs can realize a variety of current /voltage output combinations and accurate measurement, with the disadvantages of a complex structure and high cost. This article introduces an SMU reference design that is composed of an AD5522 master controller plus voltage/current amplifier stage.
Learn more about Analog Devices SMU solutions and main products.
Design Resources
Further Reading
- Application Note AN-1574: Parametric Measurement Unit and Supporting Components for ATE Applications Using the AD5522 PMU and the AD7685 16-Bit ADC
- MT-034 Tutorial: Current Feedback (CFB) Op Amps
- MT-057 Tutorial: High Speed Current Feedback Op Amps
- Design Note DN513: High Voltage CMOS Amplifier Enables High Impedance Sensing with a Single IC
- User Guide UG-1870: Evaluating the AD7606C-18 8-Channel DAS with 18-Bit, 1 MSPS Bipolar Input, Simultaneous Sampling ADC
Design Tool/Forums