Class G
What is a Class G Amplifier?
Definition
Class G amplifiers are similar to class AB amplifiers except they use two or more supply voltages.
When operating at low signal levels, the amplifier uses a lower supply voltage. As the signal level increases, the amplifier automatically picks the appropriate supply voltage.
Class G amplifiers are more efficient than class AB amplifiers since they use the maximum supply voltage only when required, while a class AB amplifier always uses the maximum supply voltage.
Synonyms
rail-switchingFind a term alphabetically: