The MAXREFDES9001 is a complete internet-of-things
(IoT) security reference design featuring a LoRa radio
based, low-power, temperature sensor node secured with
a DS28S60 secure coprocessor, a LoRa gateway, and
a cloud application implemented in AWS infrastructure.
This reference design highlights a robust and easy to
manage end-to-end security scheme with authentication
and confidentiality capabilities independent of the transmission link in use—the LoRaWAN protocol in this case.
The MAXREFDES9001 is designed to easily integrate into
embedded systems enabling confidentiality, authentication, and integrity of information.
The sensor node is motioned by the tiny, low-power,
Cortex-M4-based microcontroller MAX32660 which periodically measures the ambient temperature with the help
of the DS7505, authenticates and encrypts the temperature value using AES-GCM with the DS28S60 secure
coprocessor, and sends it to the AWS infrastructure over
a LoRaWAN network, through a Raspberry Pi-powered
gateway. To prevent rogue nodes from publishing data,
joining the sensor nodes to the network requires a prior
local verification using a convenient NFC-based strong
authentication with the help of the MAX66242 Secure
Authenticator and a dedicated Android application running
on an NFC-enabled Android device.
Once the authentication is successful, proving that the
sensor node is genuine, the Android device communicates
with the cloud application through the Internet to provision
the sensor node; that is, to generate a certificate for the
sensor node and perform an AES-GCM key exchange
between that sensor node and the AWS infrastructure. The
Android device uses the MAX66242 as an NFC bridge to
communicate with the sensor node device’s microcontroller application and store the certificate into the DS28S60
coprocessor, and to have the key exchange done between
the DS28S60 and the cloud application using the Elliptic
Curve Diffie-Hellman (ECDH) protocol. Once the key
exchange is completed, the sensor node is ready to send
its data to the cloud application using the negotiated
AES-GCM key. Further sensor node authentication by
the cloud application is possible using ECDSA since the
sensor node now has a valid certificate with a matching
key pair. Incidentally, the provisioning process also joins
the end device to the LoRaWAN network implemented
using the AWS IoT core, but this is not the main purpose
of the reference design that shows a way to secure data
without relying on the security of the various underlying
communication links.
优势和特点
DS28S60 ChipDNA technology protects private and secret keys against invasive attacks.
DS28S60 provides end-to-end security using hardware-based ECDSA authentication, ECDH key exchange, and AES-GCM authenticated encryption.
Complete low-power sensor node board design
Sample LoRaWAN gateway implementation based on Raspberry Pi
Sample cloud application implemented in AWS infrastructure highlighting end-to-end security with the sensor board’s DS28S60 including ECDH key exchange, and AES-GCM secure communication.
Source code
Peripheral module-compatible sensor expansion port
Raspberry Pi enables portable LoRaWAN gateway deployment.
The reference design includes the following major components: DS28S60, MAX32660, MAX66242, DS7505, and SX1262. The DS28S260 is a cryptographic coprocessor that encrypts temperature measurements using an onboard AES-GCM engine, which is accessible through a SPI interface. The DS7505 is a temperature sensor which uses the I2C interface to provide the environment’s temperature. The MAX66242 enables the NFC communication between the Android mobile device and the node. The MAX32660 is a low-power microcontroller that enables the communication between the different modules. Finally, the SX1262 is used to modulate and transmit the encrypted temperature measurement through LoRa protocol.
This document describes the hardware shown in Figure 1, as well as its supporting software. It provides a detailed, systematic technical guide to set up and understand the MAXREFDES9001 reference design. The system has been built and tested, details of which follow later in this document.
Figure 2. High-Level Block Diagram of the MAXREFDES9001.
The high-level block diagram of the MAXREFDES9001 hardware is shown in Figure 2. This system is composed of three main components: sensor node, LoRaWAN gateway, and Android device.
) Sensor Node
The sensor node incorporates the following major components:
DS28S60 Cryptographic Coprocessor Provides secure authentication and data encryption
DS7505 Temperature Sensor Measures temperature data for transmission
MAX32660 Low-Power Microcontroller: Manages the sensor node operations and data processing
MAX66242 NFC Secure Authenticator: Facilitates secure NFC communication and storage
SX1262 LoRa Transceiver: Enables long-range wireless communication using the LoRa protocol
) LoRaWAN Gateway
The LoRaWAN gateway consists of:
Raspberry Pi: Serves as the main control unit for processing and forwarding data
Dragino PG1301 LoRaWAN Concentrator: Handles the reception and transmission of LoRa packets from multiple sensor nodes
) Android Device
The Android device runs the MAXREFDES9001 app, which provides an interface for provisioning, authenticating, and managing the sensor node. It communicates with
the sensor node through NFC and interacts with the cloud application through WebSocket APIs.
The MAXREFDES9001 software is divided into three
components: sensor device firmware, cloud application,
and Android application.
The reference design sequence is as follows:
Provisioning of Sensor Node
Generation of Device Key Pair
The Android application, using the MAX66242 as a communication bridge, triggers the generation of a key pair for the sensor node.
It then reads the DS28S60 public key, ROM ID, and MANID.
Certificate Request
The Android application sends a request to the cloud application to generate a certificate for the end device, including the device’s unique ID and public key.
Certificate Storage
The cloud application generates the certificate and returns it to the Android application.
The certificate is then stored in the DS28S60 memory.
AWS Public Key Storage
The cloud application supplies its public key, which is stored in the DS28S60 memory.
AES-GCM Key Generation
Using a Diffie-Hellman key exchange, identical AES-GCM keys are generated both in the cloud application and on the DS28S60.
LoRaWan Session Keys Provisioning
The cloud application supplies the necessary session keys to join the LoRaWan network. The keys are stored in the end device.
Authentication of Sensor Node
Certificate and Public Key Retrieval
The Android application requests the stored certificate and public key from the DS28S60.
Challenge Request
The Android application sends the DS28S60’s certificate and public key to the cloud application to request a challenge.
Generate ECDSA Signature
Upon receiving the challenge from the cloud application, the Android application requests the DS28S60 to generate an ECDSA signature using the provided challenge.
Signature Verification
The Android application sends the ECDSA signature to the cloud application for verification.
Data Transmission
Temperature Measurement
The sensor node measures the temperature using the DS7505 sensor.
Encryption
The measured temperature is encrypted using the DS28S60’s AES-GCM engine with the previously exchanged AES key.
Secure Transmission
The secure measurement is transmitted to the cloud application through the LoRaWan gateway.
Authorization
The cloud application retrieves the certificate and public keys to authorize the sensor node.
Packet Reception
The cloud application receives the secure measurement packet.
Key Retrieval
The cloud application retrieves the AES-GCM decryption and verification key associated with the sender end device based on the ID found in the measurement packet.
Data Decryption and Storage
The measurement data is decrypted and stored in Amazon DynamoDB, which is a part of the cloud application.
Data Viewing
The stored data in the database can be viewed through a web browser.
Sensor Node Firmware
The sensor node firmware consists of four major functions:
Provisioning
This process involves the DS28S60 generating a public key and returning its ROMID and MANID. The ECC certificate, LoRaWAN session keys, and AES-GCM
peer public key provided by the server are stored in the DS28S60 memory. This is achieved by writing to and reading from the MAX66242 memory through I2C with the information requested by the application.
Authentication
In this phase, the ECC certificate stored in the DS28S60 memory is provided. A random challenge is received from the server after the ECC certificate’s authenticity is verified. The DS28S60 performs a Read Page Authentication using the received random challenge and returns the ECDSA signature.
Data Encryption
This step involves reading the current temperature using the DS7505 temperature sensor. The DS28S60 generates an AES-GCM encryption key by performing a Diffie-Hellman key exchange with the AES-GCM keys generated by the server. After performing AESGCM encryption using the DS28S60, a ciphertext and an authentication tag are generated.
Data Transmission
This involves sending LoRa packets periodically to the LoRaWAN gateway. The onboard LED flashes to show that the LoRa packets are being transmitted. The LoRa end device joins the LoRaWAN network through Activation by Personalization (ABP) as the LoRaWAN keys are obtained during the provisioning sequence. The LoRa packet is transmitted by the sensor node in JSON format.
Encrypted data packet:
Payload: DS28S60 ROM ID, AES-GCM Keys, AES-GCM Ciphertext (Temperature), AES-GCM Authentication Tag.
Cloud Application Software
The AWS infrastructure hosts the cloud application software, which manages various aspects of the IoT ecosystem involving the sensor nodes. The key components and their roles are as follows:
AWS Lambda Functions
Serverless computing is managed by AWS Lambda functions, which perform tasks such as processing incoming data from the sensor nodes, generating and verifying certificates, decrypting data packets, and interacting with other AWS services.
Amazon DynamoDB
Data storage is managed by Amazon DynamoDB, a NoSQL database service. It stores the sensor nodes information, certificates, public keys, and encrypted measurement data.
AWS IoT Core
This service facilitates the connectivity and management of LoRaWAN devices. It handles the provisioning, authentication, and communication with the LoRaWAN gateway and routes the sensor nodes packet to the AWS Lambda functions for processing.
Amazon API Gateway
The Amazon API gateway is used to create, publish, maintain, monitor, and secure APIs. It serves as an interface for the Android application to interact with the cloud application through a WebSocket API.
AWS Amplify
AWS Amplify hosts the web application that accesses Amazon DynamoDB to display sensor node information in a user-friendly interface. As shown in Figure 3, the web application provides a detailed view of the data collected from the sensor nodes, including:
Time Stamp: Exact date and time when the data was recorded
Node Name: Identifier for each sensor node
Sensor Node Rom ID: Unique ROM ID of each sensor node
Encryption Key: AES-GCM encryption key used for securing the data
Encrypted Data: Data collected by the sensor node, displayed in its encrypted form
Sensor Value: Decrypted temperature measurement from the sensor node
Authorized: Indicates whether the data was authenticated and authorized successfully
The web application allows users to search through the records, navigate between pages, and perform actions such as retrieving or deleting data using buttons like “Get Data” and “Delete Data”.
Android Application Software
The MAXREFDES9001 Android app acts as a communication interface between the MAXREFDES9001 sensor node board and the cloud application used for this reference design. The primary goal of this application is to provide an intuitive interface that demonstrates the features of the DS28S60 cryptographic coprocessor by provisioning and authenticating the sensor node. The Android application commands the DS28S60 to generate the necessary information to register the sensor node with the cloud application.
Main Functions
The purpose of this demo is to showcase the features of the DS28S60 cryptographic coprocessor for which two main functions were developed.
Node Provisioning
During this process, the DS28S60 is asked to generate a public key from the Android application through the NFC interface that gets stored into the MAX66242’s memory, which is also embedded into the node board. The Android App requests the key and transmits it back to the cloud application through a WebSocket client. The cloud application validates this data and generates a certificate that is returned to the Android application. This data is sent back to the MAX66242 though NFC, which will be then collected by the DS28S60 and will in turn store it.
Node Authentication
This function verifies the authenticity of the node board allowing it to transmit sensor data to the cloud application once the device is authenticated, the cloud application data is stored in the DS28S60. By running this command, the Android application request the DS28S60 to return the certificate generated during the provisioning stage and its public key through the MAX66242 NFC Tag. This data is sent to the cloud application which returns a random challenge that is used by the DS28S60 to generate a signature which gets sent to the server again to confirm its authenticity.
For more details about the Android application functionality, refer to the Android Application Details Document. Figure 4 shows what the GUI looks like when running on the Android device. See Table 1 for more details on each functionality. See the Design Resources section to download the software and source code.
Figure 3. Data Received from Sensor Nodes.
Figure 4. Main Display of the MAXREFDES9001 GUI.
Table 1. GUI Controls
Description
Function Number
Details
Command Menu
1
Displays the different command options available
Display Monitor
2
Displays information during the different command processes
Unauthorized Node Mode
3
Enable or disable sending bogus data simulating the behavior of a counterfeit device
NFC Provision
4
Runs the NFC Provision Sequence
Command Options
5
List out all the different command options the user has access to