AN-1285: ADF7021-N Radio Performance for Wireless Meter-Bus (WM-Bus), Mode N
Introduction
This application note describes the radio performance of the ADF7021-N transceiver when configured for operation according to the Wireless Meter-Bus (WM-Bus) standard document EN 13757-4, Mode N. This application note focuses on the key receiver parameters applicable to the 2.4 kbps and 4.8 kbps modes of operation. These parameters are packet error rate (PER) over power, sensitivity over carrier frequency error, blocking, and adjacent channel selectivity. All PER tests are carried out using the WM-Bus development kit available from Analog Devices, Inc. The development kit includes a full WM-Bus stack running on a Renesas RL78 microprocessor. Figure 1 shows a motherboard and daughter card, both of which are included with the development kit.
Wm-bus, Mode N 12.5 Khz Channel Plan
Figure 2 gives an overview of the 12.5 kHz channel plan for the WM-Bus, Mode N. There are six 12.5 kHz channels available. Four of these channels are reserved for 4.8 kbps, and two of these channels are reserved for 2.4 kbps. Channel 1a and Channel 2a are used in this application note for evaluation.
Wm-bus, Mode N Specification
Table 1 shows the key specifications and performance requirements of EN 13757-4. WM-Bus compliant receivers are separated into three classes: HR, MR, and LR, which are the highest, medium, and lowest performance, respectively. Minimum sensitivity is specified as PER <80%.
Parameter | Mode | Notes | |
2.4 kbps | 4.8 kbps | ||
Minimum Sensitivity | −115 dBm | −112 dBm | For a 20 byte frame at 80% PER |
Frequency Error Tolerance | ±2 kHz | ±1.5 kHz | Receiver must be capable of correcting these carrier frequency errors |
Frequency Deviation | 2.4 kHz | 2.4 kHz | Minimum ±1.68 kHz, maximum ±3.12 kHz |
Modulation |
Gaussian Frequency Shift Keying (GFSK) |
GFSK | Gaussian BT = 0.5 |
Data Rate Tolerance | ±100 ppm | ±100 ppm | |
Preamble Length | 16 bits | 16 bits | Data: 0x5555 |
Synchronization Length | 16 bits | 16 bits |
Frame Format A Data: 0xF68D Frame Format B Data: 0xF672 |
Blocking, 2 MHz | 37.5 dB | 37.5 dB | Required for HR class receiver; calculated according to |
Blocking, 10 MHz | 62.5 dB | 62.5 dB | EN 300 220-1, Section 8.4.3, where A = 9 kHz |
Adjacent Channel Rejection | 40 dB | 40 dB | Required for HR class receiver |
Test Setup
The test setup used to obtain the results in this Application Note are as follows:
- All PER tests were carried out using the WM-Bus development kit available from Analog Devices, Inc. The Renesas RL78 microprocessor included with this kit runs a full WM-Bus protocol stack.
- Test methods, where applicable, are consistent with EN 300 220-1.
- Figure 3 shows the packet used for all PER tests. This packet follows the formatting for a packet type of Format A. This packet is 24 bytes long, including the preamble and synchronization word (SWD). EN 13757-4 specifies a 20 byte frame for sensitivity measurements.
- The cyclic redundancy check (CRC) was not used to measure whether or not a packet was correct. A packet was only recorded when received if every bit in the SWD and 20 byte frame was correct. No forward error correction (FEC) was used.
- An automatic frequency control (AFC) algorithm was included on the Renesas RL78 to maximize sensitivity performance when a frequency error is present on the radio frequency (RF) carrier signal. This algorithm includes a preamble detect function that ensures a low false packet detect rate in the presence of noise. The RF frequency error cannot be corrected in the specified number of preamble bits without this algorithm.
- Note that the blocking and selectivity results were obtained using bit error rate (BER) tests. If the PER test method is used, the test results are degraded by 2 dB to 3 dB.
- The EVAL-ADF7021-NDB9Z board was used for the tests. Details of this board are available on the ADF7021-N product page.
- The results listed in this document are typical values measured at room temperature over five daughter cards.
2.4 Kbps Mode Results
The following results apply to Channel 2a and Channel 2b, which correspond to WM-Bus Submode N1c, Submode N2c, Submode N1d, and Submode N2d.
2.4 Kbps Mode Sensitivity
Figure 4 shows the PER results obtained while sweeping the input power from −125 dBm to +10 dBm in 1 dB steps. The PER floor is not clear from the plot. This floor is measured as less than 0.2% for all powers above sensitivity. Table 2 lists spot measurements of the sensitivity level for various PER levels. The results satisfy the minimum sensitivity requirement.
RF Channel (MHz) |
Payload (Bytes) |
PER (%) |
Sensitivity (dBm) |
WM-Bus Limit(dBm) |
169.43125 | 20 |
80 20 1 |
−121.5 −120 −118 |
−115 N/A1 N/A1 |
1 N/A means not applicable.
2.4 Kbps Mode Sensitivity Vs. Rf Frequency Error
Figure 5 shows the variation in sensitivity as the RF frequency error increases to the ±2 kHz limit levels specified in the EN 13757-4. The sensitivity level is 80% PER.
2.4 Kbps Mode Blocking
Figure 6 shows the blocking performance of the receiver over ±30 MHz. The device was tested according to the method outlined in the EN 300 220-1, Section 8.4.2, using the BER conducted measurement method. Table 3 contains spot measurements at the offsets referred to in the EN 13757-4. The results satisfy the HR class receiver requirements.
RF Channel (MHz) |
Interferer Offset (MHz) |
Blocking (dB) |
HR Class Receiver Limit (dB) |
169.43125 |
+2 −2 +10 −10 |
84 83.5 84 83 |
37.5 37.5 62.5 62.5 |
2.4 Kbps Mode Adjacent Channel Selectivity
Figure 7 shows the blocking performance of the receiver over ±100 kHz with fine interferer resolution steps. Other than the interferer step size, the test setup was identical to the 2.4 kbps Mode Blocking section. Table 4 lists spot measurements at the adjacent channels. The results satisfy the HR class receiver requirements.
RF Channel (MHz) |
Interferer Offset (kHz) |
Blocking (dB) |
HR Class Receiver Limit (dB) |
169.43125 |
+12.5 −12.5 |
42 42 |
40 N/A1 |
4.8 Kbps Mode Results
The following results apply to Channels 1a, Channel 1b, Channel 3a, and Channel 3b, which correspond to WM-Bus Submode N1a, Submode N2a, Submode N1b, Submode N2b, Submode N1e, Submode N2e, Submode N1f, Submode N2f.
4.8 Kbps Mode Sensitivity
Figure 8 shows the PER results obtained while sweeping the input power from −125 dBm to +10 dBm in 1 dB steps. The PER floor is not clear from the plot. This floor was measured as less than 0.1% for all powers above sensitivity. Table 5 lists spot measurements of the sensitivity level for various PER levels. The results satisfy the minimum sensitivity requirement.
RF Channel (MHz) |
Payload (Bytes) |
PER(%) | Sensitivity (dBm) |
WM-Bus Limit (dBm) |
169.40625 | 20 |
80 20 1 |
−121 −119 −117 |
−112 N/A1 N/A1 |
1 N/A means not applicable.
4.8 Kbps Mode Sensitivity Vs. Rf Frequency Error
Figure 9 shows the variation in sensitivity as the RF frequency error was increased to the ±1.5 kHz limit levels specified in the EN 13757-4. The sensitivity level is 80% PER.
4.8 Kbps Mode Blocking
Figure 10 shows the blocking performance of the receiver over ±30 MHz. The device is tested according to the method outlined in the EN 300 220-1, Section 8.4.2, using the BER conducted measurement method. Table 6 contains spot measurements at the offsets referred to in the EN 13757-4. The results satisfy the HR class receiver requirements.
RF Channel (MHz) |
Interferer Offset (MHz) |
Blocking (dB) |
HR Class Receiver Limit (dB) |
169.40625 |
+2 −2 +10 −10 |
83 82 84 83 |
37.5 37.5 62.5 62.5 |
4.8 Kbps Mode Adjacent Channel Selectivity
Figure 11 shows the blocking performance of the receiver over ±100 kHz with fine interferer resolution steps. Other than the interferer step size, the test setup was identical to the 4.8 kbps Mode Blocking section. Table 7 lists spot measurements at the adjacent channels. The results satisfy the HR class receiver requirements.
RF Channel (MHz) |
Interferer Offset (kHz) |
Blocking (dB) |
HR Class Receiver Limit (dB) |
169.40625 |
+12.5 −12.5 |
42 41 |
40 N/A1 |
1 N/A means not applicable.
Conclusion
The ADF7021-N has excellent sensitivity when configured for WM-Bus, Mode N, providing a significant margin to the required minimum sensitivity specification.
The AFC algorithm running on the Renesas RL78 ensures that excellent sensitivity is maintained when a frequency error is present on the RF carrier. The algorithm includes a preamble detect function, which provides a low false packet detect rate in the presence of noise.
Blocking performance provides significant margin for the HR class receiver requirements.
Adjacent channel selectivity satisfies the HR class receiver requirements with a small margin.
The WM-Bus development kit provides a fully operational stack, reference code, and a graphic user interface (GUI) for evaluation. For additional information about purchasing a WM-Bus development kit, contact your local Analog Devices sales representative.
参考电路
EN 13757-4:2013. “Communication systems for meters and remote reading of meters — Part 4: Wireless meter readout (Radio meter reading for operation in SRD bands)” (European Normal standard, 2013).
ETSI EN 300 220-1,V2.4.1 (2012-1), “Electromagnetic compatibility and Radio spectrum Matters (ERM); Short Range Devices (SRD); Radio equipment to be used in the 25 MHz to 1 000 MHz frequency range with power levels ranging up to 500 mW” (European Telecommunications Standards Institute (ETSI) standard, 2012).