AN-1283: Receiving the 4:2:0 Stream with the ADV7619

Introduction

This application note outlines the usage of the ADV7619 HDMI® video receiver for the 4:2:0 HDMI stream 4k × 2k at 60 Hz.

The ADV7619 can receive 4:2:0 video streams in a way similar to how t it receives 4:4:4 data in 4k × 2k modes. To enable this, set OP_FORMAT_SEL to the value of 0x54 and set all other I2C writes in the same way as for 4k × 2k 4:4:4 video mode. Because the ADV7619 works only as a bypass for 4k × 2k modes, it outputs samples as they are received without providing color space conversion (CSC). The receiver bypasses CP core and thus neither CSC nor upconversion/down-conversion of video standard is available.

The 4k × 2k at 60 Hz HDMI 4:2:0 8-bit data stream has a TMDS clock frequency of 297 MHz. It is the same as 4k × 2k at 30 Hz HDMI 4:4:4 8-bit data stream. The main difference between the 4:2:0 and 4:4:4 enabling 60 Hz refresh rate is the content of the stream.

The 4:2:0 stream sends two luma (Y) samples in the same period of time as the 4:4:4 stream sends one luma sample. This allows for a shortening period of line length, thus shortening the period of frame by half allowing for 60 Hz transmission. This increase of luma bandwidth in 4:2:0 is done at the cost of bandwidth reduction of chroma (Cb and Cr) samples.


Pixel Bus Output for 4:2:0 Transmission


The 4:2:0 4k × 2k at 60 Hz stream consists of two luma samples per dot clock and one chroma sample. The chroma sample contains blue (Cb) or red (Cr) components depending on the line being transmitted. Even lines (0, 2, 4, and so on) contain Cb samples whereas odd lines (1, 3, 5, and so on) contain Cr samples as shown in Figure 1 and Figure 2, respectively.

Figure 1. Pixel Lines Assignment of the 4:2:0 Stream (Even Line) in ADV7619.

Figure 1. Pixel Lines Assignment of the 4:2:0 Stream (Even Line) in ADV7619.

Figure 2. Pixel Lines Assignment of the 4:2:0 Stream (Odd Line) in ADV7619.

Figure 2. Pixel Lines Assignment of the 4:2:0 Stream (Odd Line) in ADV7619.

In 2 × SDR 4:4:4 interleaved mode, the pixel bus outputs two 2 × 24 bit data onto two 24-bit wide sub-buses (upper pixel output 47 to 24) and lower pixel output 23 to 0). Note that this mode is detailed in the Special SDR 4:2:2 and 4:4:4 Output Modes for Video with Pixel Clock Frequencies Above 170 MHz table in the ADV7619 data sheet.

This parallel output allows for dividing the clock frequency by half to 148.5 MHz from the original 297 MHz for 4k × 2k at 60 Hz 4:2:0.

The detailed pixel bus assignment is shown in Table 1.

Conversion 4:2:0 To 4:4:4

The ADV7619 does not provide a color space converter that could handle a conversion between 4:2:0 and 4:4:4. The conversion can be performed in an external FPGA. The upscaling of 4:2:0 to 4:4:4 increases bandwidth by 2.

To convert 4:4:4 to 4:2:0, it is necessary to use line buffers that allow for collection of Cb and Cr data from consecutive video lines. Figure 3 shows the concept of upscaling 4:2:0 to 4:4:4 stream.

Figure 3. Concept of 4:2:0 to 4:4:4 Conversion.

Figure 3. Concept of 4:2:0 to 4:4:4 Conversion.

Table 1. Pixel Bus Output for 4:2:0 Mode with OP_FORMAT_SEL = 0x54
Pin Even Lines = 0, 2, 4, 6, … Odd Lines = 1, 3, 5, 7, …
2 × 24-Bit Mode 0 2 × 24-Bit Mode 0
P47 Y7-0 Y7-0
P46 Y6-0 Y6-0
P45 Y5-0 Y5-0
P44 Y4-0 Y4-0
P43 Y3-0 Y3-0
P42 Y2-0 Y2-0
P41 Y1-0 Y1-0
P40 Y0-0 Y0-0
P38 Cb6-0 Cr6-0
P37 Cb5-0 Cr5-0
P36 Cb4-0 Cr4-0
P35 Cb3-0 Cr3-0
P34 Cb2-0 Cr2-0
P33 Cb1-0 Cr1-0
P32 Cb0-0 Cr0-0
P31 Y7-1 Y7-1
P30 Y6-1 Y6-1
P29 Y5-1 Y5-1
P28 Y4-1 Y4-1
P27 Y3-1 Y3-1
P26 Y2-1 Y2-1
P25 Y1-1 Y1-1
P24 Y0-1 Y0-1
P23 Y7-2 Y7-2
P22 Y6-2 Y6-2
P21 Y5-2 Y5-2
P20 Y4-2 Y4-2
P19 Y3-2 Y3-2
P18 Y2-2 Y2-2
P17 Y1-2 Y1-2
P16 Y0-2 Y0-2
P15 Cb7-2 Cr7-2
P14 Cb6-2 Cr6-2
P13 Cb5-2 Cr5-2
P12 Cb4-2 Cr4-2
P11 Cb3-2 Cr3-2
P10 Cb2-2 Cr2-2
P9 Cb1-2 Cr1-2
P8 Cb0-2 Cr0-2
P7 Y7-3 Y7-3
P6 Y6-3 Y6-3
P5 Y5-3 Y5-3
P4 Y4-3 Y4-3
P3 Y3-3 Y3-3
P2 Y2-3 Y2-3
P1 Y1-3 Y1-3
P0 Y0-3 Y0-3

作者

Witold Kaczurba

Witold Kaczurba

Witold Kaczurba 是ADI公司高级电视部(爱尔兰利默里克)资深应用工程师,负责支持解码器和HDMI产品。2007年从波兰弗罗茨瓦夫理工大学毕业并获得电气工程硕士学位后,他加入ADI公司。学生期间,他曾为小型电子和IT公司工作,后来作为工读生加入ADI公司(爱尔兰),随后成为应用工程师。