As an applications engineer, I am frequently asked about operating regulators with no load. Most modern LDOs and switching regulators are stable with no load, so why do people repeatedly ask? Some older power devices require a minimum load to guarantee stability, as one of the poles that must be compensated is affected by the effective load resistance, as discussed in “Low-Dropout Regulators (Ask the Applications Engineer—37).” For example, Figure A shows that the LM1117 requires a 1.7-mA minimum load current (up to 5 mA).

Most newer devices are designed to operate with no load, and exceptions to this rule are very limited. The same design techniques that allow LDOs to be stable with any output capacitor, especially low ESR caps, are used to guarantee stability at no load. For those few modern devices that require a load, the limitation is usually a result of leakage current through the pass element, not the stability. So, how can you tell? Read the data sheet. If the device requires a minimum load, the data sheet would surely say something.
The ADP1740 and other low-voltage, high-current LDOs fall into this category. The worst-case leakage current from the integrated power switch is about 100 µA at 85°C and 500 µA at 125°C. Without a load, the leakage current would charge the output capacitor until the switch VDS was low enough to reduce the leakage current to a negligible level, raising the no-load output voltage. The data sheet says that a 500 µA minimum load is required, so a dummy load is advisable if the device will operate at high temperature. This load is small compared to the device’s 2-A rating. Figure B shows the minimum load current specification from the ADP1740 data sheet.

What if the data sheet doesn’t explicitly specify a minimum load? In most cases, a minimum load is not required. It may not sound very convincing, but if a minimum load was required, the data sheet would certainly say so. The confusion often comes into play because data sheets will often include graphs showing the specifications over some operating range. Most of these graphs are logarithmic, allowing them to show multiple decades of load ranges, but a log scale cannot go to zero. Figure C shows the ADM7160 output voltage and ground current vs. load current over the 10-µA to 200-mA range. Other graphs, such as ground current vs. input voltage, show measurements at multiple load currents, but don’t show data at zero current. In addition, parameters such as PSRR, line regulation, load regulation, and noise specify a certain load current range that does not include zero, as shown in Figure D. None of this means that a minimum load is required, though.



Users of switching regulators with power-saving mode (PSM) are often worried about operation at light loads because PSM reduces the operating frequency, skips pulses, provides a burst of pulses, or some combination of these. PSM reduces power consumption and increases efficiency at light loads. Its disadvantage is a noticeable increase in output ripple, but the device remains stable and can easily operate with no load.
As shown in Figure E, the ADP2370 high-voltage, low-quiescent-current buck regulator produces increased ripple due to PSM operation when the load switches between 800 mA and 1 mA. The fact that the test was done at 1 mA does not indicate that 1 mA is the minimum load.

Figure F shows the ripple voltage changing with load current. In this case the graph goes all the way to zero, indicating both that the load can be zero and that the noise at no load may not be any worse than the noise at 1 mA or 10 mA.

Conclusion
Most modern regulators are stable with zero load current, but when in doubt, consult the data sheet. Be careful, though. Logarithmic graphs don’t go to zero, and tests aren’t always done with zero load current, so you shouldn’t infer that the regulator won’t work with no load even though no-load data isn’t shown. With switching regulators, ripple in power-saving mode is normal, not a sign of instability.
参考电路
Patoux, Jerome. “Low-Dropout Regulators (Ask the Applications Engineer—37),” Analog Dialogue, Volume 41, Number 2, 2007.