Installing DC1223                                                                                                                                          01/28/16

 

Requirements

  1. DC1223A-A or DC1223A-B (if DC1223A-A is used, the SMBus monitor will be disabled)
  2. Windows XP or later
  3. 20Mb disk space
  4. DC1223A-B.msi installation file

 

Steps for GUI installation

  1. Do not plug DC1223 to the PC yet.
  2. Double click DC1223A-Bv102.msi to install DC1223A-B.msi.

 

step1

 

  1. The above screen will appear. Click Next.

 

step2

 

  1. Confirm the installation folder.

 

step3

 

  1. Installation in progress.

 

step4

 

  1. Software installation completes.

 

Steps for Hardware driver installation

 

 

  1. Without connecting to the USB port yet, check that the jumper JP4 on DC1223 is on the ‘Direct’ position.

 

  1. Download QuikEval from the Linear Technology website: http://ltspice.linear.com/software/ltcqev.exe

 

  1. Follow the installation instructions from the DC1223A-B Demo Manual: http://www.linear.com/docs/38012