Using a Differential I/O Amplifier in Single-Ended Applications

2009年12月01日

Introduction

Recent advances in low voltage silicon germanium and BiCMOS processes have allowed the design and production of very high speed amplifiers. Because the processes are low voltage, most of the amplifier designs have incorporated differential inputs and outputs to regain and maximize total output signal swing. Since many low voltage applications are single-ended, the questions arise, “How can I use a differential I/O amplifier in a single-ended application?” and “What are the implications of such use?” This article addresses some of the practical implications and demonstrates specific single-ended applications using the 3GHz gain-bandwidth LTC6406 differential I/O amplifier.

Background

A conventional op amp has two differential inputs and an output. The gain is nominally infinite, but control is maintained by virtue of feedback from the output to the negative “inverting” input. The output does not go to infinity, but rather the differential input is kept to zero (divided by infinity, as it were). The utility, variety and beauty of conventional op amp applications are well documented, yet still appear inexhaustible. Fully differential op amps have been less well explored.

Figure 1 shows a differential op amp with four feedback resistors. In this case the differential gain is still nominally infinite, and the inputs kept together by feedback, but this is not adequate to dictate the output voltages. The reason is that the common mode output voltage can be anywhere and still result in a “zero” differential input voltage because the feedback is symmetric. Therefore, for any fully differential I/O amplifier, there is always another control voltage to dictate the output common mode voltage. This is the purpose of the VOCM pin, and explains why fully differential amplifiers are at least 5-pin devices (not including supply pins) rather than 4-pin devices. The differential gain equation is VOUT(DM) = VIN(DM) • R2/R1. The common mode output voltage is forced internally to the voltage applied at VOCM. One final observation is that there is no longer a single inverting input: both inputs are inverting and noninverting depending on which output is considered. For the purposes of circuit analysis, the inputs are labeled with “+” and “–” in the conventional manner and one output receives a dot, denoting it as the inverted output for the “+” input.

Figure 1. Fully differential I/O amplifier showing two outputs and an additional VOCM pin

Anybody familiar with conventional op amps knows that noninverting applications have inherently high input impedance at the noninverting input, approaching GΩ or even TΩ. But in the case of the fully differential op amp in Figure 1, there is feedback to both inputs, so there is no high impedance node. Fortunately this difficulty can be overcome.

Simple Single-Ended Connection of a Fully Differential Op amp

Figure 2 shows the LTC6406 connected as a single-ended op amp. Only one of the outputs has been fed back and only one of the inputs receives feedback. The other input is now high impedance.

Figure 2. Feedback is single-ended only. This circuit is stable, with a Hi-Z input like the conventional op amp. the closed loop output (VOUT+ in this case) is low noise. Output is best taken single-ended from the closed loop output, Providing a 3dB bandwidth Of 1.2GHz. The Open Loop Output (VOUT–) has a noise gain of two from VOCM, but is well behaved to about 300MHz, above which it has significant passband ripple.

The LTC6406 works fine in this circuit and still provides a differential output. However, a simple thought experiment reveals one of the downsides of this configuration. Imagine that all of the inputs and outputs are sitting at 1.2V, including VOCM. Now imagine that the VOCM pin is driven an additional 0.1V higher. The only output that can move is VOUT – because VOUT+ must remain equal to VIN, so in order to move the common mode output higher by 100mV the amplifier has to move the VOUT – output a total of 200mV higher. That’s a 200mV differential output shift due to a 100mV VOCM shift. This illustrates the fact that single-ended feedback around a fully differential amplifier introduces a noise gain of two from the VOCM pin to the “open” output. In order to avoid this noise, simply do not use that output, resulting in a fully single-ended application. Or, you can take the slight noise penalty and use both outputs.

A Single-Ended Transimpedance Amplifier

Figure 3 shows the LTC6406 connected as a single-ended transimpedance amplifier with 20kΩ of transimpedance gain. The BF862 JFET buffers the LTC6406 input, drastically reducing the effects of its bipolar input transistor current noise. The VGS of the JFET is now included as an offset, but this is typically 0.6V so the circuit still functions well on a 3V single supply and the offset can be dialed out with the 10k potentiometer. The time domain response is shown in Figure 4. Total output noise on 20MHz bandwidth measurements shows 0.8mVRMS on VOUT+ and 1.1mVRMS on VOUT–. Taken differentially, the transimpedance gain is 40kΩ.

Figure 3. Transimpedance amplifier. Ultralow noise JFET buffers the current noise of the bipolar LTC6406 input trim the pot for 0V differential output under no-light conditions.

Figure 4. Time domain response of circuit of Figure 3, showing both outputs each with 20kΩ of TIA gain. Rise time is 16ns, indicating a 20MHz bandwidth.

Conclusion

New families of fully differential op amps like the LTC6406 offer unprecedented bandwidths. Fortunately, these op amps can also function well in single-ended and 100% feedback applications.

著者について

Glen Brisebois
Glen Briseboisは、アナログ・デバイセズのシグナル・コンディショニング・グループ(シリコン・バレー)に所属するアプリケーション・エンジニアです。カナダのアルバータ大学で物理学と電気工学の学士号を取得しています。同大学を卒業後、トラピスト修道院とカルトゥジオ修道院で数年間、修道生活を送ろうとしました。しかし、その間も「回路」のことが頭から離れませんでした。現在は結婚し、子どもたちと一緒に幸せに暮らしています。業務の大半は回路に関連...
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して

最新メディア 21

Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成