Overview
設計リソース
説明
The Riverside design (MAXREFDES8#) uses an H-bridge transformer driver (MAX256) and a low dropout (LDO) linear regulator (MAX1659) to create a 12V (15V) output isolated power supply from a 3.3V voltage input (Figure 1). This general-purpose power solution can be used in many different types of isolated power applications, but is mainly targeted for industrial sensors, industrial automation, process control, and medical applications.
Figure 1. The Riverside subsystem design block diagram.
機能と利点
Features
- Isolated power
- 12V (15V) output
- Small printed circuit board (PCB) area
- Pmod™-compatible form factor
Applications
- Industrial sensors
- Process control
- Industrial automation
- Medical
使用されている製品
Details Section
The Riverside subsystem reference design operates from a 3.3V DC power source. The MAX256 H-bridge transformer driver switches at approximately 475kHz and drives the primary side of the 1:2.6 turns ratio, with the use of a TGM-H281NF transformer from Halo® Electronics. The transformer secondary side is connected to a voltage doubler that rectifies the AC output into DC output. The MAX1659 LDO regulates the voltage to 12V. The Zener diode D3 protects the LDO by keeping its input voltage below 16.1V.
The input power can be from the J1 Pmod-compatible connector or from an external power supply connected to the EXT_+3.3V and DGND connectors. To change the output voltage of this reference design, simply change the feedback resistors (R2, R3) of the LDO.
The output voltage of the MAX1659 LDO is set by the following equation:
VOUT = VSET × (1 + R2/R3)
Where VSET = 1.21V.
For example, for the 15V output application, change R2 to 187kΩ and change R3 to 16.2kΩ. In applications sensitive to output voltage ripple, a lowpass LC pi-filter can be added in front of the LDO input.
The isolation transformer in this design has an isolation voltage of 1500VRMS. It is recognized by UL 60950 and EN 60950 and falls into the "functional" insulation class.
Required equipment:
- Riverside (MAXREFDES8#) board
- 3.3V 1A power supply
- One digital voltmeter
Procedure
The Riverside board is fully assembled and tested. Follow the steps below to verify board operation.
- Place the shunt on jumper JU1 to the 1–2 position.
- Connect the positive terminal of the power supply to the EXT_+3.3V connector.
- Connect the negative terminal of the power supply to the DGND connector.
- Connect the positive terminal of the voltmeter to the +12V connector.
- Connect the negative terminal of the voltmeter to the GND connector.
- Turn on the power supply.
- Use the voltmeter to measure the output voltage.
The Riverside design was tested for two output voltage rails: 12V and 15V. Other voltage rails can be achieved by modifying the resistor values of R2 and R3.
When set for 12V output, the circuit can deliver a maximum load current of approximately 165mA. When set for 15V output, the circuit can deliver a maximum load current of approximately 60mA.
To achieve a larger maximum load, the user can either increase the input power supply voltage or increase the transformer turns ratio properly. Refer to the MAX256 data sheet for details. The power efficiencies are illustrated in Figure 2 and Figure 3.
Figure 2. Power efficiency vs. current load for 12V output.
Figure 3. Power efficiency vs. current load for 15V output.
The output noise is well below 0.5% of the output voltage. The noise is mainly due to the switching pulses of the MAX256. Figure 4 and Figure 5 display the noise at no load for 12V and 15V outputs, respectively. Figure 6 and Figure 7 display the noise at the maximum loads for 12V and 15V outputs, respectively.
Figure 4. Noise at VOUT = 12V, IOUT = 0mA.
Figure 5. Noise at VOUT = 15V, IOUT = 0mA.
Figure 6. Noise at VOUT = 12V, IOUT = 165mA.
Figure 7. Noise at VOUT = 15V, IOUT = 60mA.
Halo is a registered trademark of Halo Electronics, Inc.
Pmod is a trademark of Digilent Inc.
Documentation & Resources
-
MAXREFDES8 Design Files2021/03/10ZIP485 K
Support & Training
Search our knowledge base for answers to your technical questions. Our dedicated team of Applications Engineers are also available to answer your technical questions.