CN0531:20ビットの分解能でプログラム可能な高精度のDC電圧源
2022年01月25日
非常に要件の厳しいテスト/計測分野では、極めて性能の高いアプリケーションを構築する必要があります。例えば、数ppmの温度ドリフト性能、1ppm未満の直線性、予測可能な低ノイズ性能が求められるといった具合です。「CN0531」は、20ビットの分解能でプログラムすることが可能なバイポーラ電圧源のリファレンス設計です。精度、直線性、安定性に優れる±5VのDC電圧を生成することができます。
CN0531:20ビットの分解能でプログラム可能な高精度のDC電圧源
2022年01月25日
非常に要件の厳しいテスト/計測分野では、極めて性能の高いアプリケーションを構築する必要があります。例えば、数ppmの温度ドリフト性能、1ppm未満の直線性、予測可能な低ノイズ性能が求められるといった具合です。「CN0531」は、20ビットの分解能でプログラムすることが可能なバイポーラ電圧源のリファレンス設計です。精度、直線性、安定性に優れる±5VのDC電圧を生成することができます。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}