faqs
よくある質問(FAQ)
Why are the safeload registers five bytes long, while I'm loading four-byte parameters into the RAM using these registers?
The safeload registers are also used to load the slew RAM data, which is five bytes long. For parameter RAM writes using safeload, the first byte of the safeload register can be set to 0x00.