faqs
よくある質問(FAQ)
What does the J2KPROG encode parameter mean?
Every tile contains packets that make up the coded tile. These packets contain information about a specific layer, component, resolution level and a specific position. The J2KPROG encode parameter allows the user to program the order in which packets are arranged in the codestream.
More detailed information on Progression Order can be found in the ISO/IEC15444-1 standard, Annex B.12.