AN-1339: ADF7023-J AD_15d4g Firmware Download Module

Introduction

This application note describes the AD_15d4g firmware download module for the ADF7023-J transceiver IC. The AD_15d4g firmware download module adds the following features to the ADF7023-J:

  • IEEE 802.15.4g physical layer (PHY) header formatting
  • IEEE 802.15.4g data whitening
  • Tx/Rx rolling data buffer
  • 1 byte to 1000 byte Tx preamble
  • ARIB STD T108 clear channel assessment (CCA)
  • Rx antenna diversity

Figure 1 shows a block diagram of the ADF7023-J low power, 902 MHz to 958 MHz transceiver IC. The transceiver contains a custom microcontroller (MCU) core with a mask ROM, which implements packet handling functions and translates radio commands into internal control sequences. An additional 2 kB of program RAM (PRAM) is available and serves as program code memory. PRAM enables the addition of radio controller commands to provide modified or extended functionality. The AD_15d4g firmware download module described in this application note is based on program code downloaded into this PRAM.

Figure 1. ADF7023-J block diagram.
Figure 1. ADF7023-J block diagram.

The PRAM block is volatile memory and must be reloaded each time the transceiver wakes up from sleep state. The PRAM locations can be accessed sequentially through the serial peripheral interface (SPI) interface. The details of the code download mechanism are explained in the Code Download Sequence section.

The firmware download binary is rom_ram_7023_2_2_AD_ 15d4g_R4p3.dat and is available from Analog Devices, Inc., at ftp://ftp.analog.com/pub/RFL/FirmwareModules.

The AD_15d4g firmware download module remaps several of the ADF7023-J registers and commands and extends the data sheet state diagram. See the Register Remapping section for more information.

Note that throughout this application note, multifunction pins, such as the ADCIN_ATB3 pin, are referred to either by the entire pin name or by a single function of the pin, for example, ATB3, when only that function is relevant.

Register Remapping

The firmware extends the ADF7023-J data sheet state diagram to include the 15d4g state, as outlined in Figure 2, and extends the firmware states, as defined in Table 3.

When the firmware module is downloaded and the 15d4g state is entered, some of the battery backup random access memory (BBRAM) registers take on new meaning, and some are rendered redundant. The remapped BBRAM registers are defined in Table 1. The command list is expanded, as defined in Table 2. The INTERRUPT_MASK_0 register and the INTERRUPT_ SOURCE_0 register are also remapped while in the 15d4g state, as defined in Table 29 and Table 30.

Packet RAM locations 0x20 to 0xFF are available for packet data in the 15d4g state. Bytes 0x00 to 0x1F are allocated for use by the on-chip processor and must not be used for packet data.

When 15d4g state is exited, all normal data sheet functionality is restored. Note, however, that the reused settings must be reprogrammed appropriately according to the data sheet.

Table 1. BBRAM Reuse During 15d4g State
Address (Hex) Normal Operation Operation in 15d4g State Comment
0x100 INTERRUPT_MASK_0 INTERRUPT_MASK_0 Interrupts remapped in 15d4g state
0x101 INTERRUPT_MASK_1 INTERRUPT_MASK_1
0x102 NUMBER_OF_WAKEUPS_0 Reserved Do not overwrite in 15d4g state
0x103 NUMBER_OF_WAKEUPS_1 BB_CCA_CFG_0
0x104 NUMBER_OF_WAKEUPS_IRQ_THRESHOLD_0 BB_CCA_CFG_1
0x105 NUMBER_OF_WAKEUPS_IRQ_THRESHOLD_1 BB_CCA_THRESHOLD
0x106 RX_DWELL_TIME Reserved Do not overwrite in 15d4g state
0x107 PARMTIME_DIVIDER PARMTIME_DIVIDER Not used in 15d4g state
0x108 SWM_RSSI_THRESH SWM_RSSI_THRESH Not used in 15d4g state
0x109 CHANNEL_FREQ_0 CHANNEL_FREQ_0
0x10A CHANNEL_FREQ_1 CHANNEL_FREQ_1
0x10B CHANNEL_FREQ_2 CHANNEL_FREQ_2
0x10C RADIO_CFG_0 RADIO_CFG_0
0x10D RADIO_CFG_1 RADIO_CFG_1
0x10E RADIO_CFG_2 RADIO_CFG_2
0x10F RADIO_CFG_3 RADIO_CFG_3
0x110 RADIO_CFG_4 RADIO_CFG_4
0x111 RADIO_CFG_5 RADIO_CFG_5
0x112 RADIO_CFG_6 RADIO_CFG_6
0x113 RADIO_CFG_7 RADIO_CFG_7
0x114 RADIO_CFG_8 RADIO_CFG_8
0x115 RADIO_CFG_9 RADIO_CFG_9
0x116 RADIO_CFG_10 RADIO_CFG_10
0x117 RADIO_CFG_11 RADIO_CFG_11
0x118 IMAGE_REJECT_CAL_PHASE IMAGE_REJECT_CAL_PHASE
0x119 IMAGE_REJECT_CAL_AMPLITUDE IMAGE_REJECT_CAL_AMPLITUDE
0x11A MODE_CONTROL MODE_CONTROL
0x11B PREAMBLE_MATCH PREAMBLE_MATCH
0x11C SYMBOL_MODE SYMBOL_MODE
0x11D PREAMBLE_LEN PREAMBLE_LEN
0x11E CRC_POLY_0 CRC_POLY_0
0x11F CRC_POLY_1 CRC_POLY_1
0x120 SYNC_CONTROL SYNC_CONTROL
0x121 SYNC_BYTE_0 SYNC_BYTE_0
0x122 SYNC_BYTE_1 SYNC_BYTE_1
0x123 SYNC_BYTE_2 SYNC_BYTE_2
0x124 TX_BASE_ADR TX_BASE_ADR
0x125 RX_BASE_ADR RX_BASE_ADR
0x126 PACKET_LENGTH_CONTROL PACKET_LENGTH_CONTROL
0x127 PACKET_LENGTH_MAX PACKET_LENGTH_MAX
0x128 STATIC_REG_FIX RESERVED Set to 0 for 15d4g state
0x129 ADDRESS_MATCH_OFFSET BB_RX_ANTENNA_DIVERSITY_CFG
0x12A ADDRESS_LENGTH BB_TX_ANTENNA_CFG
0x12B Address matching BB_ANTENNA0_RSSI
0x12C Address matching BB_ANTENNA1_RSSI
0x12D Address matching BB_THRESHOLD_DIFF_RSSI
0x12E Address matching BB_NB_PREAMBLE_BYTES_LOW
0x12F Address matching BB_NB_PREAMBLE_BYTES_HIGH
0x130 Address matching BB_SFD_LOW
0x131 Address matching BB_SFD_HIGH
0x132 Address matching BB_PHR_LOW Controlled by firmware in 15d4g state
0x133 Address matching BB_PHR_HIGH Controlled by firmware in 15d4g state
0x134 Address matching BB_RX_BUFFER_SIGNAL
0x135 Address matching BB_RX_BUFFER_SIZE
0x136 Address matching BB_TX_BUFFER_SIGNAL
0x137 Address matching BB_TX_BUFFER_SIZE
0x138 RSSI_WAIT_TIME Reserved Set to 0x00 for 15d4g state
0x139 TESTMODES BB_TESTMODES
0x13A TRANSITION_CLOCK_DIV Reserved Set to 0x01 for 15d4g state
0x13B Reserved BB_VCO_BAND_READBACK
0x13C Reserved BB_VCO_AMP_READBACK
0x13D Reserved Reserved
0x13E RX_SYNTH_LOCK_TIME RX_SYNTH_LOCK_TIME
0x13F TX_SYNTH_LOCK_TIME TX_SYNTH_LOCK_TIME
0x01F Packet data PHY_RX_STATUS Packet RAM used in 15d4g state
 
Figure 2. 15d4g state diagram.
Figure 2. 15d4g state diagram.
 Table 2. Commands and States Included in the Firmware Download
Command/Bit Command Code Present State Next State
CMD_ENTER_15d4_MODE 0xC1 PHY_ON PHY_ON_15d4
CMD_EXIT_15d4_MODE 0xB1 PHY_ON_15d4 PHY_ON
CMD_PHY_RX_CCA_15d4 0xB2 PHY_ON_15d4, PHY_TX_15d4, PHY_RX_CCA_15d4 PHY_RX_CCA_15d4
CMD_PHY_TX_15d4 0xB5 PHY_ON_15d4, PHY_RX_CCA_15d4 PHY_TX_15d4
CMD_PHY_ON_15d4 0xB1 PHY_RX_CCA_15d4, PHY_TX_15d4 PHY_ON_15d4
CMD_SYNTH_CAL_15d4 0xEE PHY_ON_15d4 PHY_ON_15d4
CMD_CCA_START 0xB7 PHY_RX_CCA_15d4 PHY_RX_CCA_15d4
CMD_CCA_STOP 0xB8 PHY_RX_CCA_15d4 PHY_RX_CCA_15d4
CMD_CCA_FILTER 0xB9 PHY_RX_CCA_15d4 PHY_RX_CCA_15d4
CMD_CONFIG_DEV 0xBB PHY_ON_15d4 PHY_ON_15d4
Table 3. FW_STATE Description
Value State Description
0x18 PHY_ON_15d4 The device is ready to operate in 15d4 mode, and PHY_RX_CCA_15d4 and PHY_TX_15d4 states can be entered.
0x1A PHY_RX_CCA_15d4 The device is in 15d4 receive mode where valid 15d4 packets can be received, CCA and antenna diversity can be enabled. After reception of a valid packet, the device can return to the PHY_ON_15d4 state, can remain in the PHY_RX_CCA_15d4 state, or can transition to the PHY_TX_15d4 state depending on the user settings.
0x1C PHY_TX_15d4 The device is in 15d4 transmit mode, where it automatically transmits the transmit packet stored in packet RAM. After transmission of the packet, the device can return to the PHY_ON_15d4 state, can remain in the PHY_TX_15d4 state, or can transition to the PHY_RX_CCA_15d4 state depending on the user settings.

Register Map Extension

Table 4. Registers for Use with AD_15d4g Firmware Download
Address (Hex) Register Description
0x103 BB_CCA_CFG_0 CCA Configuration Word 0
0x104 BB_CCA_CFG_1 CCA Configuration Word 1
0x105 BB_CCA_THRESHOLD CCA threshold
0x129 BB_RX_ANTENNA_DIVERSITY_CFG Rx antenna diversity configuration register
0x12A BB_TX_ANTENNA_CFG Tx antenna configuration register
0x12B BB_ANTENNA0_RSSI If antenna diversity is enabled, this stores the receive signal strength indicator (RSSI) value from Antenna 0
0x12C BB_ANTENNA1_RSSI If antenna diversity is enabled, this stores the RSSI value from Antenna 1
0x12D BB_THRESHOLD_DIFF_RSSI Stores the difference between the CCA threshold and the measured RSSI
0x12E BB_NB_PREAMBLE_BYTES_LOW Lower byte of the number of preamble bytes
0x12F BB_NB_PREAMBLE_BYTES_HIGH Upper byte of the number of preamble bytes
0x130 BB_SFD_LOW Lower byte of start of frame delimiter (SFD) word
0x131 BB_SFD_HIGH Upper byte of SFD word
0x132 BB_PHR_LOW Lower byte of PHY header (PHR) word
0x133 BB_PHR_HIGH Upper byte of PHR word
0x134 BB_RX_BUFFER_SIGNAL Rx buffer nearly full
0x135 BB_RX_BUFFER_SIZE Rx buffer full
0x136 BB_TX_BUFFER_SIGNAL Tx buffer nearly full
0x137 BB_TX_BUFFER_SIZE Tx buffer full
0x138 Reserved Set to 0
0x139 BB_TESTMODES Controls test modes
0x13A Reserved Set to 0x01
0x13B BB_VCO_BAND_READBACK Voltage controlled oscillator (VCO) band select calibration value
0x13C BB_VCO_AMP_READBACK VCO amplitude level calibration value
0x01F PHY_RX_STATUS Indicates preamble and SFD states in Rx

Register Descriptions

Table 5. Address 0x103: BB_CCA_CFG_0
Bits Name Access Description
7 CCA_STATUS R/W Indicates if channel is clear (0) or busy (1).
[6:5] CCA_FILTER_BW R/W CCA_FILTER_BW sets the intermediate frequency (IF) filter bandwidth for CCA RSSI.
00: 100 kHz.
01: 150 kHz.
10: 200 kHz.
11: 300 kHz.
4 CCA_AUTO_TX R/W 1: remain in the PHY_RX_CCA_15d4 state (manual Tx) on CCA. This is for use with CCA infinity mode.
0: automatic Tx on CCA. This is for use with CCA timer mode.
[3:1] CCA_TIMER R/W CCA_TIMER selects one of eight timer options.
000: 160 µs.
001: 320 µs.
010: 640 µs.
011: 1280 µs.
100: 1920 µs.
101: 2560 µs.
110: 9960 µs.
111: infinity mode.
0 CCA_BYPASS_UPDATE R/W Debug mode only. For normal use, set to 0.
0: CCA data is updated every byte (normal use).
1: CCA data is not updated every byte (debug mode only, causes the CCA_STATUS bit to be frozen).
Table 6. Address 0x104: BB_CCA_CFG_1
Bits Name Access Description
7 CCA_LIVE_STATUS R/W Live indication if channel is clear (0) or busy (1).
6 ENABLE_IFBW_SWITCH_ON_PREAMBLE R/W 1: changes bandwidth when preamble is detected.
0: keep bandwidth when preamble is detected.
5 ENABLE_IFBW_AUTO_SWITCH R/W 1: changes bandwidth when CMD_CCA_START is issued.
0: keep default bandwidth when CMD_CCA_START is issued.
4 WAIT_FOR_HOST_EOCCA R/W Debug mode only. For normal use, set to 0.
1: wait for host at end of CCA timer after CCA trigger (debug mode only).
0: continue to update CCA registers on CCA timer timeout (normal use).
[3:0] Reserved R/W Set to 0.
Table 7. Address 0x105: BB_CCA_THRESHOLD
Bits Name Access Description
[7:0] CCA_THRESHOLD R/W This is an 8-bit number representing the CCA RSSI threshold in dBm. CCA_THRESHOLD = RSSI (dBm) + 107
Table 8. Address 0x129: BB_RX_ANTENNA_DIVERSITY_CFG
Bits Name Access Description
[7:6] RX_ANTENNA_DIVERSITY_CFG_PATH_ANT_0 R/W Maps the Rx Antenna 0 path to the ATB pins
Bit 7 = ATB1/ATB3, 0 = low, 1 = high
Bit 6 = ATB2/ATB4, 0 = low, 1 = high
[5:4] RX_ANTENNA_DIVERSITY_CFG_PATH_ANT_1 R/W Maps the Rx Antenna 1 path to the ATB pins
Bit 5 = ATB1/ATB3, 0 = low, 1 = high
Bit 4 = ATB2/ATB4, 0 = low, 1 = high
3 RX_ATB_LEVEL R/W 1: select to use 1.8 V drivers (ATB3 and ATB4)
0: select to use VDD drivers (ATB1 and ATB2)
2 Reserved R/W Set to 0
1 ANTENNA_SELECTED R/W If the ANTENNA_DIVERSITY_ENABLE bit = 1, this bit reports the antenna selected by the diversity algorithm:
0 = Antenna 0
1 = Antenna 1
If the ANTENNA_DIVERSITY_ENABLE bit = 0, this bit selects the receive antenna:
0 = Antenna 0 (using the RX_ANTENNA_DIVERSITY_CFG_PATH_ANT_0 bit mapping)
1 = Antenna 1 (using the RX_ANTENNA_DIVERSITY_CFG_PATH_ANT_1 bit mapping)
0 ANTENNA_DIVERSITY_ENABLE R/W 1 = enable antenna diversity algorithm (and autoselect the Rx antenna)
0 = disable antenna diversity algorithm (and manually select the Rx antenna)
Table 9. Address 0x12A: BB_TX_ANTENNA_CFG
Bits Name Access Description
[7:6] TX_ANTENNA_CFG_PATH_ANT_0 R/W Maps the Tx Antenna 0 path to the ATB bits
Bit 7 = ATB1/ATB3, 0 = low, 1 = high
Bit 6 = ATB2/ATB4, 0 = low, 1 = high
[5:4] TX_ANTENNA_CFG_PATH_ANT_1 R/W Maps the Tx Antenna 1 path to ATB bits
Bit 5 = ATB1/ATB3, 0 = low, 1 = high
Bit 4 = ATB2/ATB4, 0 = low, 1 = high
3 TX_ATB_LEVEL R/W 1: selects to use 1.8 V drivers (ATB3 and ATB4)
0: selects to use VDD drivers (ATB1 and ATB2)
2 Reserved R/W Set to 0
1 TX_ANTENNA R/W This bit selects the transmit antenna
0 = Antenna 0 (using the TX_ANTENNA_DIVERSITY_CFG_PATH_ANT_0 bit mapping)
1= Antenna 1 (using the TX_ANTENNA_DIVERSITY_CFG_PATH_ANT_1 bit mapping)
0 Reserved R/W Set to 0
Table 10. Address 0x12B: BB_ANTENNA0_RSSI
Bits Name Access Description
[7:0] ANTENNA0_RSSI_READBACK R/W This register contains the RSSI value measured on Antenna 0:
RSSI (dBm) = ANTENNA0_RSSI_READBACK − 107
Table 11. Address 0x12C: BB_ANTENNA1_RSSI
Bits Name Access Description
[7:0] ANTENNA1_RSSI_READBACK R/W This register contains the RSSI value measured on Antenna 1:
RSSI (dBm) = ANTENNA1_RSSI_READBACK − 107
Table 12. Address 0x12D: BB_THRESHOLD_DIFF_RSSI
Bits Name Access Description
[7:0] THRESHOLD_DIFF_RSSI R/W Difference between the CCA_THRESHOLD and the most recent RSSI value evaluated
Table 13. Address 0x12E: BB_NB_PREAMBLE_BYTES_LOW
Bits Name Access Description
[7:0] NB_PREAMBLE_BYTES_LOW R/W Bits[7:0]of the NB_PREAMBLE_BYTES word
Table 14. Address 0x12F: BB_NB_PREAMBLE_BYTES_HIGH
Bits Name Access Description
[7:0] NB_PREAMBLE_BYTES_HIGH R/W Bits[15:8] of the NB_PREAMBLE_BYTES word. Note that valid values are within the range, 4 ≤ the NB_PREAMBLE_BYTES word ≤ 1000
Table 15. Address 0x130: BB_SFD_LOW
Bits Name Access Description
[7:0] BB_SFD_LOW R/W Bits[7:0] of the SFD word (see Table 34)
Table 16. Address 0x131: BB_SFD_HIGH
Bits Name Access Description
[7:0] BB_SFD_HIGH R/W Bits[15:8] of the SFD word. For supported SFD values, see Table 34

The values in Address 0x132 (the BB_PHR_LOW register) are read only. In receive mode, the values are copied in by the AD_15d4g firmware download module from a received packet. In transmit mode, the required PHR value for a transmit must be written to the TX_BASE_ADR register and the firmware reflects those values back in Address 0x132.

Table 17. Address 0x132: BB_PHR_LOW
Bits Name Access Description
7 MODE_SWITCH R Indicates if the packet is a mode switch packet.
[6:5] Reserved R Set to 0.
4 FCS R 0 = 32-bit frame check sequence (FCS); 1 = 16-bit FCS. Note that only a 16-bit FCS is automatically handled by the ADF7023-J. A 32-bit FCS must be calculated by the user. For a 32-bit FCS Tx, the user must calculate the FCS and add to the end of the payload. For a 32-bit FCS Rx, the user must calculate the cyclic redundancy check (CRC) and compare with the last four bytes received into the packet RAM. In a 32-bit FCS Rx, a CRC correct interrupt is never generated. The INTERRUPT_RX_EOF interrupt signifies the end of packet reception.
3 Whitening R 1 = PHY service data unit (PSDU) whitened.
[2:0] PSDU_LENGTH_HI R Bits[10:8] of the PSDU_LENGTH[10:0] word.

The values in Address 0x133 (the BB_PHR_HIGH register) are read only. In receive mode, the values are copied in by the AD_15d4g firmware download module from a received packet. In transmit mode, the required PHR value for a transmit must be written to the TX_BASE_ADR register and the firmware reflects those values back in Address 0x133

Table 18. Address 0x133: BB_PHR_HIGH
Bits Name Access Description
[7:0] PSDU_LENGTH_LO R Bits[7:0] of the PSDU_LENGTH[10:0] word. Note that valid values are within the range, 2 < the PSDU_LENGTH[10:0] word < 2048
Table 19. Address 0x134: BB_RX_BUFFER_SIGNAL
Bits Name Access Description
[7:0] RX_BUFFER_SIGNAL R/W The rolling buffer fills from the RX_BASE_ADR register with data. When the buffer reaches location, RX_BASE_ADR + RX_BUFFER_SIGNAL, the INTERRUPT_BUFFER_ALMOST_FULL interruptis generated. Note that the contents of RX_BUFFER_SIGNAL must be greater than 2.
Table 19. Address 0x134: BB_RX_BUFFER_SIGNAL
Bits Name Access Description
[7:0] RX_BUFFER_SIGNAL R/W The rolling buffer fills from the RX_BASE_ADR register with data. When the buffer reaches location, RX_BASE_ADR + RX_BUFFER_SIGNAL, the INTERRUPT_BUFFER_ALMOST_FULL interruptis generated. Note that the contents of RX_BUFFER_SIGNAL must be greater than 2.
Table 20. Address 0x135: BB_RX_BUFFER_SIZE
Bits Name Access Description
[7:0] RX_BUFFER_SIZE R/W This is the maximum size of the Rx buffer. When the location, RX_BASE_ADR + RX_BUFFER_SIZE, is filled with data, an INTERRUPT_BUFFER_FULL interruptis generated, and the buffer loops back to location RX_BASE_ADR and continues to fill from there. Note that RX_BUFFER_SIZE must have a value greater than 2 and that, for a 16-bit FCS case, a 2-byte overflow area is required after the RX_BUFFER_SIZE register.
Table 21. Address 0x136: BB_TX_BUFFER_SIGNAL
Bits Name Access Description
[7:0] TX_BUFFER_SIGNAL R/W The rolling buffer sends from the TX_BASE_ADR register with data. When the buffer reaches and sends from location, TX_BASE_ADR + TX_BUFFER_SIGNAL, an INTERRUPT_BUFFER_ALMOST_FULL interrupt is generated. Note that TX_BUFFER_SIGNAL must have a value greater than 2.
Table 22. Address 0x137: BB_TX_BUFFER_SIZE
Bits Name Access Description
[7:0] TX_BUFFER_SIZE R/W This is the maximum size of the Tx buffer.When the data from location, TX_BASE_ADR + TX_BUFFER_SIZE, is sent, an INTERRUPT_BUFFER_FULL interrupt is generated, and the buffer loops back to location TX_BASE_ADR and continues to send from there. Note that TX_BUFFER_SIZE must have a value greater than 2.
Table 23. Address 0x138: Reserved
Bits Name Access Description
[7:0] Reserved R/W Set to 0
Table 24. Address 0x139: BB_TESTMODES
Bits Name Access Description
[7:2] Reserved R/W Set to 0
1 BIT_CONTINUOUS_TX R/W 1: device remains in the PHY_TX_15d4 state after packet transmission
0: device returns to the PHY_ON_15d4 state after packet transmission
0 BIT_CONTINUOUS_RX R/W 1: device remains in the PHY_RX_CCA_15d4 state after packet reception
0: device returns to the PHY_ON_15d4 state after packet reception
Table 25. Address 0x13A: Reserved
Bits Name Access Description
[7:1] Reserved R/W Set to 0
0 Reserved R/W Set to 1
Table 26. Address 0x13B: BB_VCO_BAND_READBACK
Bits Name Access Description
[7:0] VCO_BAND_READBACK R/W Stores the VCO band calibration results after synthesizer calibration, for fast Tx/Rx transitions
Table 27. Address 0x13C: BB_VCO_AMPL_READBACK
Bits Name Access Description
[7:0] VCO_AMPL_READBACK R/W Stores the VCO amplitude calibration results after synthesizer calibration, for fast Tx/Rx transitions
Table 28. Address 0x01F: PHY_RX_STATUS
Bits Name Access Description
[7:2] Reserved R Reserved
1 SFD_RX_STATUS R 1: SFD detected
0: SFD not detected
0 PREAMBLE_RX_STATUS R 1: preamble detected
0: preamble not detected

Interrupt Mask and Source Configurations

Table 29. Address 0x100: INTERRUPT_MASK_0
Bits Name Access Description
7 INTERRUPT_CCA R/W In timer mode, interrupt after CCA period has expired. (The CCA_STATUS flag indicates if the channel is busy or clear.) In infinity mode, interrupt when the channel is clear.
1: interrupt enabled; 0: interrupt disabled.
6 INTERRUPT_BUFFER_FULL R/W Interrupt when the Rx or Tx buffer is full.
1: interrupt enabled; 0: interrupt disabled.
5 INTERRUPT_BUFFER_ALMOST_FULL R/W Interrupt when the Rx or Tx buffer is almost full.
1: interrupt enabled; 0: interrupt disabled.
4 INTERRUPT_RX_EOF R/W Interrupt when a packet has finished receiving.
1: interrupt enabled; 0: interrupt disabled.
3 INTERRUPT_TX_EOF R/W Interrupt when a packet has finished transmitting.
1: interrupt enabled; 0: interrupt disabled.
2 INTERRUPT_CRC_CORRECT R/W Interrupt when a received packet has the correct CRC.
1: interrupt enabled; 0: interrupt disabled.
1 INTERRUPT_PHR_DETECT R/W Interrupt when PHR has been detected in the received packet. The interrupt is generated when SFD is detected, but is delayed and issued at the end of PHR reception.
1: interrupt enabled; 0: interrupt disabled.
0 INTERRUPT_PREAMBLE_DETECT R/W Interrupt when a qualified preamble is in the received packet.
1: interrupt enabled; 0: interrupt disabled.
Table 30. Address 0x336: INTERRUPT_SOURCE_0
Bits Name Access Reset Description
7 INTERRUPT_CCA R/W 0 In timer mode, after CCA period has expired, a CCA interrupt is asserted.
In infinity mode, the INTERRUPT_CCA interrupt is asserted only when the channel is clear.
6 INTERRUPT_BUFFER_FULL R/W 0 Asserted when the Rx or Tx buffer is full (Rx or Tx buffer size is reached).
5 INTERRUPT_BUFFER_ALMOST_FULL R/W 0 Asserted when the Rx or Tx buffer is almost full (Rx or Tx buffer signal is reached).
4 INTERRUPT_RX_EOF R/W 0 Asserted when a packet has finished receiving.
3 INTERRUPT_TX_EOF R/W 0 Asserted when a packet has finished transmitting.
2 INTERRUPT_CRC_CORRECT R/W 0 Asserted when a received packet has the correct CRC.
1 INTERRUPT_PHR_DETECT R/W 0 Asserted when PHR is detected in the received packet.
0 INTERRUPT_PREAMBLE_DETECT R/W 0 Asserted when a qualified preamble is detected in the received packet.

Antenna Signal Path Control

The ATB1, ATB2, ATB3, and ATB4 pins on the ADF7023-J are used to control the radio frequency (RF) antenna diversity switches. This section provides configuration details for these four pins in receive and transmit modes.


Receive Mode


In PHY_RX_CCA_15d4 state, the mapping of the control bits to configure the antenna signal paths is automatically controlled by Bits[7:6] and Bits[5:4] of the BB_RX_ANTENNA_DIVERSITY_ CFG register (Address 0x129). Bits[7:6] control the signal path for Antenna 0, as shown in Table 31, and Bits[5:4] control the signal path for Antenna 1, as shown in Table 32.

With antenna diversity enabled (Address 0x129, Bit 0 = 1), the ADF7023-J automatically toggles between the two antennas.

With antenna diversity disabled (Address 0x129, Bit 0 = 0), the device uses the value programmed into Address 0x129, Bit 1 (the ANTENNA_SLECTED bit) to select which antenna and antenna path to use.

These control bits appear at the ATB1 and ATB2 pins as VDD control bits, or at the ATB3 and ATB4 pins as 1.8 V control bits. The selection between VDD or 1.8 V controls is made using the RX_ATB_LEVEL bit, Bit 3 of the BB_RX_ANTENNA_DIVERSITY_CFG register.

Table 31. Antenna 0 Path Rx/Tx Configuration
Address 0x129 for Rx,
Address 0x12A for Tx
ATB States
Path (Bits[7:6]) ATB Level, (Bit 3) ATB11 ATB21 ATB32 ATB42
0 0 0 Low Low High-Z High-Z
0 1 0 Low High High-Z High-Z
1 0 0 High Low High-Z High-Z
1 1 0 High High High-Z High-Z
0 0 1 High-Z High-Z Low Low
0 1 1 High-Z High-Z Low High
1 0 1 High-Z High-Z High Low
1 1 1 High-Z High-Z High High
1 ATB1 and ATB2 are VDD drivers: high = VDD, low = 0 V, high-Z = tristate.
2 ATB3 and ATB4 are 1.8 V drivers: high =1.8 V, low = 0 V, high-Z = tristate.
Table 32. Antenna 1 Path Rx/Tx Configuration
Address 0x129 for Rx,
Address 0x12A for Tx
ATB States
Path (Bits[5:4]) ATB Level, (Bit 3) ATB11 ATB21 ATB32 ATB42
0 0 0 Low Low High-Z High-Z
0 1 0 Low High High-Z High-Z
1 0 0 High Low High-Z High-Z
1 1 0 High High High-Z High-Z
0 0 1 High-Z High-Z Low Low
0 1 1 High-Z High-Z Low High
1 0 1 High-Z High-Z High Low
1 1 1 High-Z High-Z High High
1 ATB1 and ATB2 are VDD drivers: high = VDD, low = 0 V, high-Z = tristate.
2 ATB3 and ATB4 are 1.8 V drivers: high =1.8 V, low = 0 V, high-Z = tristate.

Transmit Mode


For transmit mode, the transmit path is automatically controlled by Bits[7:6] and Bits[5:4] of the BB_TX_ANTENNA_CFG register (Address 0x12A). Bits[7:6] control the signal path for Antenna 0, as shown in Table 31, and Bits[5:4] control the signal path for Antenna 1, as shown in Table 32.

The selection of which antenna to use for Tx is controlled by the TX_ANTENNA bit (Bit 1 of Address 0x12A). Setting the TX_ANTENNA bit to 0 selects Antenna Path 0 for Tx, and setting it to 1 selects Antenna Path 1 for Tx.

These control bits appear at the ATB1 and ATB2 pins as VDD control bits, or at the ATB3 and ATB4 pins as 1.8 V control bits. The selection between VDD or 1.8 V controls is made using the TX_ATB_LEVEL bit, Bit 3 of the BB_TX_ANTENNA_ CFG register.

Fast Tx/Rx Transitions

The AD_15d4g firmware download module supports fast transitions from the PHY_ON_15d4 state to the PHY_TX_ 15d4 state and the PHY_RX_CCA_15d4 state. The fast transitions are achieved by the following sequence:

  1. Issue the CMD_SYNTH_CAL_15d4 command (Command 0xEE) while in the PHY_ON_15d4 state. A synthesizer calibration is performed at the programmed channel frequency, and the results are stored in the BB_VCO_BAND_READBACK register (Address 0x13B) and the BB_VCO_AMP_READBACK register (Address 0x13C).
  2. Enable synthesizer calibration overwrite by setting VCO_OVRW_EN (Address 0x3CD) to 0x3.

The CMD_PHY_RX_CCA_15d4 command and the CMD_ PHY_TX_15d4 command complete in a shorter time after this sequence, because a synthesizer calibration is no longer performed.

Note that it is good practice to periodically perform a full synthesizer calibration. A full synthesizer calibration maintains optimum RF performance across fluctuations in operating temperature or battery voltage.

Antenna Diversity

In addition to propagation loss, channel impairments, such as multipath and signal fading, can degrade the performance and robustness of a wireless communication link.

The propagation of an electromagnetic wave is subject to impairments such as reflections, refractions, and scattering along its path, as illustrated in Figure 3. At the input to a receiver, multiple copies of the transmitted signal can arrive at slightly different times and have varying amplitudes. These multipath signals superimpose and result in constructive or destructive interference in the composite signal seen at the input to the receiver.

Figure 3. Multipath propagation.
Figure 3. Multipath propagation.

To combat this issue, antenna diversity techniques can be used to improve the performance of the radio link. By measuring the signal quality from two antennas that are physically separate, the antenna with the highest quality signal can be directed to the input of the receiver. By physically separating the antennas, the probability that both antennas suffer the same fading characteristics at the same time is significantly reduced.

The technique employed by the ADF7023-J firmware download is a switched diversity technique. In receive mode, an external RF switch (for example, a double pole, double throw (DPDT) switch) is used to select a signal from one of two antennas, as shown in Figure 4. The ATB1 and ATB2 pins provide logic control of the RF diversity switch from the ADF7023-J. The ADF7023-J also offers the flexibility to assign any combination of logic states (00, 01, 10, 11) to the switch control pins, ATB1 and ATB2. This configurable polarity scheme supports control of a wide range of RF switch topologies. The maximum logic output level from the ATB1 and ATB2 pins is VDD. If 1.8 V logic levels are required, use the ATB3 and ATB4 pins. See the Antenna Signal Path Control section for more details on the configuration of these pins.

The ADF7023-J evaluates the quality of the received signal from either antenna by the use of a dual qualification process: by qualifying the existence of a valid preamble sequence (101010…) and by measuring the power level (RSSI). This two-level qualification process ensures high quality signal integrity at the input to the receiver and ensures sufficient signal-to-noise ratio (SNR) for packet reception.

After a packet is received, if continuous Rx is enabled (Address 0x139, Bit 0 = 1), the ADF7023-J remains in receive mode with the algorithm continuing to evaluate signal quality from both paths. If continuous Rx is not enabled, the ADF7023-J returns to the PHY_ON_15d4 state after packet reception.

Figure 4. Typical antenna diversity hardware.
Figure 4. Typical antenna diversity hardware.

The diversity algorithm is most effective at input power levels close to the sensitivity level of the receiver. In such conditions, if antenna diversity is not used, the packet error rate (PER) performance of the receiver can be significantly degraded due to multipath and signal fading loss. With diversity enabled, the likelihood of fading occurring on both antennas at the same time is significantly diminished and the ADF7023-J firmware automatically selects an antenna with the highest SNR.


Antenna Diversity Algorithm


Antenna diversity is enabled by setting Bit 0 of the BB_RX_ ANTENNA_DIVERSITY_CFG register (Address 0x129) to 1.

Upon entering the PHY_RX_CCA_15d4 state with antenna diversity enabled, the signal on each antenna is evaluated, switching between antennas with a fixed search timer period.

The algorithm operates as follows:

  • The ADF7023-J performs both preamble qualification and RSSI measurement on both antennas. During preamble qualification, the received bit stream is correlated against a fixed number of 10 preamble bit pairs in the ADF7023-J.
  • RSSI measurement is also performed during this search period.
  • After the antenna search period has expired, the same preamble qualification and RSSI measurement is performed on the second antenna.
  • When a valid preamble sequence is detected on both antennas, the antenna with the largest RSSI reading is used for reception.
  • When a valid preamble sequence is detected only on one antenna, this antenna is selected for reception of the packet.
  • If the preamble sequence is not qualified on either antenna, the algorithm continues to switch between both antennas at the search period rate.

After completing packet reception, if the BIT_CONTINUOUS_ RX bit, Bit 0 of the BB_TESTMODES register (Address 0x139), = 1, the device returns to the PHY_RX_CCA_15d4 antenna search state and the diversity algorithm continues to evaluate both antennas. Note that as the device transitions back to the PHY_ RX_CCA_15d4 state, the interrupts are not automatically cleared (see Figure 5).

If the BIT_CONTINUOUS_RX bit = 0, the device returns to the PHY_ON_15d4 state at the end of packet reception, and the identification of the antenna selected can be read back from the value in Bit 1 of the BB_RX_ANTENNA_DIVERSITY_CFG register.

The Antenna RSSI values can be read back from Address 0x12B (Antenna 0) and Address 0x12C (Antenna 1) (see Figure 6).

The mapping of the control bits to configure the antenna paths is programmable in Bits[7:6] and Bits[5:4] of the BB_RX_ ANTENNA_DIVERSITY_CFG register (Address 0x129).

These control bits appear at the ATB1 and ATB2 pins as VDD logic levels, or at the ATB3 and ATB4 pins as 1.8 V logic levels. Select between VDD or 1.8 V levels using the RX_ATB_LEVEL bit, Bit 3 of the BB_RX_ANTENNA_DIVERSITY_CFG register (Address 0x129).

See the Antenna Signal Path Control section for more details.

Figure 5. Antenna diversity timing with continuous Rx.
Figure 5. Antenna diversity timing with continuous Rx.
Figure 6. Antenna diversity timing, the BIT_CONTINUOUS_RX Bit = 0.
Figure 6. Antenna diversity timing, the BIT_CONTINUOUS_RX Bit = 0.

Performance in a Fading Environment


The performance of this algorithm was measured under the following conditions:

  • Preamble length = 10 bytes
  • Payload length = 12 bytes
  • Data rate = 100 kbps
  • Modulation index = 1
  • Rayleigh fading
  • Fading pitch = 4 Hz
  • Correlation between antennas: 0% and 100% (100% correlation is equivalent to the single antenna case in a fading environment)

Under these conditions, a diversity gain of >9 dB was achieved at the 1% PER point (see Figure 7).

Figure 7. Performance results: antenna diversity gain in a fading environment.
Figure 7. Performance results: antenna diversity gain in a fading environment.

Clear Channel Assessment

For clear channel assessment, the CCA threshold is programmed into the BB_CCA_THRESHOLD register (Address 0x105). If the measured RSSI is above this threshold, the channel is busy. If the measured RSSI is below this threshold, the channel is clear.

Evaluation of CCA and RSSI is automatically activated upon entering the PHY_RX_CCA_15d4 state. Multiple times per byte, the RSSI value is evaluated, and the CCA_LIVE_STATUS flag is updated to busy or clear. Thus, after entering the PHY_RX_CCA_ 15d4 state, the RSSI value and a live CCA status are always updated unless updates are turned off with the CCA_BYPASS_UPDATE bit (Bit 0 of Address 0x103).

Note that there is a time lag until the first RSSI value is updated upon first entering the PHY_RX_CCA_15d4 state. Until the first RSSI value is updated, the previously measured RSSI value is retained. To clear the previously measured RSSI value, the BB_ANTENNA0_RSSI and BB_ANTENNA1_RSSI registers can be zeroed before entering the PHY_RX_CCA_15d4 state.

The ADF7023-J firmware download module can support CCA and antenna diversity at the same time.

When antenna diversity is enabled, the RSSI value on the current antenna is evaluated multiple times every byte, while the value on the alternate antenna is held at its last measured value. When the antenna switches, the RSSI on the deselected antenna is held, and the RSSI on the currently selected antenna is updated. The CCA_LIVE_STATUS bit is updated continuously to signify if the measured RSSI is above or below the CCA threshold. Any excursion above the CCA threshold sets the CCA_STATUS bit to busy.

When antenna diversity is not enabled, only the RSSI on the current antenna is evaluated and compared with the CCA threshold to determine if the channel is busy or clear, and update the CCA_STATUS flag accordingly.

There are two distinct modes of operation: timer mode and infinity mode. These modes are discussed in the CCA Timer Mode section and the CCA Infinity Mode section.


CCA Timer Mode


CCA timer mode is used with automatic Tx (the BB_CCA_ CFG_0 register, Bit 4 = 0), and is initiated by the CMD_CCA_ START command.

In timer mode, the CCA evaluation period is programmable in CCA_TIMER in the BB_CCA_CFG_0 register. This is a timer in µs, as defined in Table 33.

In timer mode, the timer is initiated and the evaluation period is started by the CMD_CCA_START command. When the timer times out, or the timer is interrupted by an incoming packet, the CCA interrupt is generated (if it is enabled). Note that there is an internal overhead on the timer mode, which means the CCA evaluation period is somewhat less than the CCA timer value. In particular, for the 160 µs timer, under certain conditions, the CCA evaluation time is less than 128 µs. Therefore, it is recommended that, if Timer 000 is used, users perform their own characterization tests to ensure performance, per TELEC requirements.

Table 33. CCA Timer Mode Times
Timer Option Evaluation Period Time (µs)
000 160
001 320
010 640
011 1280
100 1920
101 2560
110 9960

The CCA_STATUS bit is automatically cleared at the beginning of every evaluation period (channel free). If the CCA_LIVE_ STATUS bit goes high (becomes busy) at any stage during the evaluation period, the CCA_STATUS flag is automatically updated to busy.

CCA timer mode is used with automatic Tx (the BB_CCA_ CFG_0 register, Bit 4 = 0) only. If the channel is clear, and automatic Tx is enabled, the device transitions automatically to the PHY_TX_15d4 state (see Figure 8).

Figure 8. CCA timer mode, channel clear, automatic Tx.
Figure 8. CCA timer mode, channel clear, automatic Tx.

If the channel is busy and the timer times out, a CCA interrupt is generated, and the device remains in the PHY_RX_CCA_ 15d4 state, with the CCA_STATUS bit set to busy (see Figure 9).

Figure 9. CCA timer mode, antenna diversity enabled, channel busy.
Figure 9. CCA timer mode, antenna diversity enabled, channel busy.

It is important to note that the RSSI value is continuously updated and evaluated during each byte period. Therefore, in antenna diversity mode, to ensure that both antennas are evaluated before making a CCA judgment, the CCA timer must be ≥4 bytes.

During CCA timer mode, incoming packets can be received.

If an SFD is detected on the best antenna, any running CCA timer is terminated and the CCA interrupt is asserted after SFD detection. The CCA_STATUS bit is set to busy. The packet continues to be received normally (see Figure 10).

Figure 10. Packet reception during CCA timer mode.
Figure 10. Packet reception during CCA timer mode.

If the CCA timer times out during the preamble or SFD of an incoming packet, that packet is lost and the CCA interrupt is generated (see Figure 11).

Figure 11. CCA timer timeout during packet reception.
Figure 11. CCA timer timeout during packet reception.

Issuing Commands During Packet Reception

Take care when issuing the CMD_CCA_START command because there are certain conditions under which issuing the command, coincident with the start of preamble on an incoming packet, causes that packet to be lost. Minimizing this risk is discussed in the Potential Packet Loss When Issuing Commands section.

Dynamic IF Filter Bandwidth Setting During CCA Timer Mode

The functionality of the intermediate frequency (IF) filter bandwidth for Rx during CCA timer mode is discussed in this section.

Upon entering the PHY_RX_CCA_15d4 state, the receiver baseband filter bandwidth is selected from the BBRAM (Bits[7:6] of Address 0x115).

In CCA timer mode, the receiver baseband filter can be automatically changed for CCA RSSI by setting the ENABLE_ IFBW_AUTO_SWITCH bit (Bit 5 of the CCA_CFG_1 register, Address 0x104) to 1. Then, the filter bandwidth automatically switches to the CCA_FILTER_BW bit setting (Bits[6:5] of the BB_CCA_CFG_0 register, Address 0x103) when the CMD_ CCA_START command (Command 0xB7) is issued.

Note that the IF of the receiver can toggle between 200 kHz and 300 kHz depending on the selected filter bandwidth.

The IF filter bandwidth of the receiver is switched back to its original BBRAM setting (Bits[7:6] of Address 0x115) on the occurrence of one of the following events:

  • If the CCA timer times out
  • Upon issuing the CMD_CCA_STOP command
  • Upon issuing the CMD_PHY_RX_CCA_15d4 command
  • Upon an incoming packet preamble detection if the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit = 1

Upon an incoming packet preamble detection, if the ENABLE_ IFBW_SWITCH_ON_PREAMBLE bit = 1, the receiver baseband filter switches back to its original value for packet reception (see Figure 12).

Figure 12. IF bandwidth automatic switching.
Figure 12. IF bandwidth automatic switching.

Upon an incoming packet preamble detection, if the ENABLE_ IFBW_SWITCH_ON_PREAMBLE bit = 0, the receiver baseband filter bandwidth is retained at its current value for the duration of the packet reception, and switches back at the end of packet reception.

False Preamble Detection During CCA Timer Mode

If a false preamble is detected while in CCA timer mode and the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit = 1, the receiver switches back to its original value for packet reception (as specified in the IFBW bits (Bits[7:6] of Address 0x115)).

If SFD is subsequently not detected, this is a false preamble detection, and the firmware takes the following action:

  • If the ENABLE_IFBW_AUTO_SWITCH bit = 1, the ADF7023-J sets the IF filter bandwidth to the CCA_FILTER_BW bit setting (Bits[6:5] of the BB_CCA_CFG_0 register, Address 0x103) as soon as SFD is not detected.
  • If the ENABLE_IFBW_AUTO_SWITCH bit = 0, the ADF7023-J sets the IF filter bandwidth to the original IFBW bit setting for packet reception, as specified in the IFBW bits (Bits[7:6] of Address 0x115) as soon as SFD is not detected.

If a false preamble is detected while in CCA timer mode, and the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit = 0, the receiver does not switch back during preamble.

If SFD is subsequently not detected, this is a false preamble detection, and the firmware takes the following action:

  • If the ENABLE_IFBW_AUTO_SWITCH bit = 1, the ADF7023-J sets the IF filter bandwidth to the CCA_ FILTER_BW bit setting (Bits[6:5] of Address 0x103) as soon as SFD is not detected.
  • If the ENABLE_IFBW_AUTO_SWITCH bit = 0, the ADF7023-J sets the IF filter bandwidth to the original IFBW value for packet reception, as specified in the IFBW bit (Bits[7:6] of Address 0x115) as soon as SFD is not detected.

CCA Infinity Mode


CCA infinity mode is used with manual Tx (the BB_CCA_ CFG_0 register, Bit 4 = 1).

Setting CCA_TIMER to 7 (binary code 111), initiates infinity mode. To select a wider IF filter for CCA during infinity mode, the CMD_CCA_FILTER command must be issued before setting CCA_TIMER to 7. Therefore, when transitioning from the PHY_ON_15d4 state, set the timer value to a value other than infinity. Upon entering Rx, the CMD_CCA_FILTER command can be issued, followed by setting the timer value to infinity. The operation of the IF bandwidth switching for infinity mode is discussed in the Dynamic IF Filter Bandwidth Setting During CCA Infinity Mode section.

As soon as infinity mode is initiated, the ADF7023-J continues to evaluate the channel until the channel is clear (see Figure 13 and Figure 14).

Figure 13. CCA infinity mode, channel clear on entering.
Figure 13. CCA infinity mode, channel clear on entering.
Figure 14. CCA infinity mode, channel becomes clear.
Figure 14. CCA infinity mode, channel becomes clear.

In infinity mode, the ADF7023-J only generates a CCA interrupt when the channel is clear for a minimum of 128 µs. If the channel is clear, the device generates an INTERRUPT_CCA interrupt, stays in the PHY_RX_CCA_15d4 state, and reverts the IF filter back to its default value while still evaluating CCA RSSI and updating the CCA_LIVE_STATUS flag.

Note that if the channel remains clear, and the CCA interrupt is cleared, it is reasserted after another 128 µs evaluation period. To avoid reasserting the channels, the CCA interrupt can be masked, or infinity mode can be exited, by setting CCA_TIMER to a value other than 7 before clearing the interrupt.

Infinity mode is used with manual Tx, so automatic Tx must be disabled for infinity mode.

If infinity mode is used with antenna diversity enabled, both antennas must be clear before the channel is considered clear and the interrupt is generated. In this case, the CCA time increases to a minimum of 250 µs (see Figure 15).

Figure 15. CCA infinity mode with antenna diversity.
Figure 15. CCA infinity mode with antenna diversity.

During CCA infinity mode, any incoming packet can be received. If continuous Rx is enabled, the device returns to the PHY_RX_CCA_15d4 state with infinity mode still enabled. However, if the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit is enabled (1), the CCA filter bandwidth reverts to its default Rx value on preamble detection. If continuous Rx is enabled, the filter bandwidth is reverted to the CCA filter bandwidth by reissuing the CMD_CCA_FILTER command.

If continuous Rx is not enabled, the device returns to the PHY_ON_15d4 state upon packet reception.

Dynamic IF Filter Bandwidth Setting During CCA Infinity Mode

Upon entering the PHY_RX_CCA_15d4 state, the receiver baseband filter bandwidth is selected from the BBRAM (Bits[7:6] of Address 0x115).

Setting CCA_TIMER to 7 (binary code 111), initiates infinity mode. To select a wider IF filter for CCA during infinity mode, the CMD_CCA_FILTER command (Command 0xB9) must be issued before setting CCA_TIMER to 7.

After the user issues the CMD_CCA_FILTER command (Command 0xB9), the bandwidth is automatically adjusted to the desired setting in Bits[6:5] of BBRAM Address 0x103 and Rx is restarted to allow synchronization of the antenna search period with the new setting (Figure 16).

Figure 16. Dynamic CCA filter bandwidth with Rx, and CCA infinity mode.
Figure 16. Dynamic CCA filter bandwidth with Rx, and CCA infinity mode.

Take care when issuing the CMD_CCA_FILTER command because there are certain conditions under which issuing the command, coincident with the start of preamble on an incoming packet, causes that packet to be lost. To minimize this risk, see the Potential Packet Loss When Issuing Commands section for more information.

Note that the IF of the receiver can toggle between 200 kHz and 300 kHz depending on selected filter bandwidth.

The IF filter bandwidth of the receiver is reverted back to its original BBRAM setting (Bits[7:6] Address 0x115) under of the following conditions:

  • Upon issuing the CMD_CCA_STOP command (Command 0xB8)
  • Upon issuing the CMD_PHY_RX_CCA_15d4 command (Command 0xB2)
  • Upon an incoming packet preamble detection if the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit = 1

Upon an incoming packet preamble detection, if the ENABLE_ IFBW_SWITCH_ON_PREAMBLE bit = 1, the receiver baseband filter switches back to its original value for Rx.

If the ENABLE_IFBW_SWITCH_ON_PREAMBLE bit = 0 , the receiver baseband filter bandwidth is retained at its current CCA value for the duration of the packet reception.

False Preamble Detection During CCA Infinity Mode

Note that a false preamble detection reverts the filter back to its default Rx value. By enabling the preamble detect interrupt, this condition can be alerted to the user. The filter returnsto the desired CCA filter value by reissuing the CMD_CCA_FILTER command.

Alternatively, Bit 0 in the PHY_RX_STATUS register (Address 0x01F) can be monitored to alert when a preamble has been detected and revert the filter to its previous CCA value if no SFD interrupt is received.

Command Access During the PHY_RX_CCA_15d4 STATE

The ADF7023-J is controlled through commands, and command access is described in the ADF7023-J data sheet. The ADF7023-J data sheet also describes the use of the status word to ensure the communications processor is ready to accept a new command.


Potential Packet Loss when Issuing Commands


Take care when issuing commands in the PHY_RX_CCA_15d4 state while waiting for an incoming packet because of the asynchronous timing of the incoming packets.

There are certain conditions under which issuing a command, coincident with the start of preamble on an incoming packet, causes that packet to be lost. Commands involved are the following:

  • CMD_PHY_RX_CCA_15d4
  • CMD_PHY_TX_15d4
  • CMD_PHY_ON_15d4
  • CMD_CCA_START
  • CMD_CCA_FILTER

To minimize this risk of losing an incoming packet, a PHY_ RX_STATUS byte (Address 0x01F) is offered (see Figure 17). Bit 0 of this byte highlights when a preamble is detected, and Bit 1 indicates when the SFD is detected.

Figure 17. PHY_RX_STATUS register.
Figure 17. PHY_RX_STATUS register.

Upon entering the PHY_RX_CCA_15d4 state, Bit 0 and Bit 1 of the PHY_RX_STATUS register (Address 0x01F), are set to 0. Upon preamble detection, Bit 0 is set to 1. Upon SFD detection, Bit 1 is set to 1. At the end of packet reception, both bits are set back to 0 (see Figure 18). If a false preamble is detected (for example, a qualified preamble without a subsequent SFD), these bits are set to 0 and the search for a preamble continues.

Figure 18. PHY_RX_STATUS Register update on packet reception.
Figure 18. PHY_RX_STATUS Register update on packet reception.

Packet loss can be minimized by monitoring the PHY_RX_ STATUS register and issuing commands only when the PHY_RX_STATUS register = 0.

However, monitoring the PHY_RX_STATUS register method, there is still a condition under which packet loss is possible where a preamble may have started in the air, but is not yet detected by the device.

The two extremes of this condition are outlined in Figure 19 and Figure 20. The worst case scenario occurs at the latest possible preamble qualification time during antenna diversity, which is 8 bytes into the 10-byte preamble (see Figure 19). In this scenario, if a command (for example, the CMD_CCA_START command) occurs during the first eight bytes of preamble, it disrupts the preamble acquisition and may cause packet loss. The best case scenario occurs at the earliest possible preamble qualification time, which is three bytes into preamble (see Figure 20). In this case, if the CMD_CCA_START command occurs during the first three bytes of preamble, there may be packet loss.

Figure 19. Packet loss due to issuing the CMD_CCA_START command during preamble (worst case).
Figure 19. Packet loss due to issuing the CMD_CCA_START command during preamble (worst case).
Figure 20. Packet loss due to issuing the CMD_CCA_START command during preamble (best case).
Figure 20. Packet loss due to issuing the CMD_CCA_START command during preamble (best case).

Packet Structure in 15d4 Mode

The ADF7023-J AD_15d4g firmware download module supports the MR_FSK PPDU header format without mode switching.

The packet structure is displayed in Figure 21.

Figure 21. PPDU format example.
Figure 21. PPDU format example.

In transmit mode, the ADF7023-J firmware download module adds the requested number of preamble bytes, and then inserts the requested SFD and PHR. If whitening is enabled, the PSDU is whitened. If a 16-bit FCS is enabled, the 16-bit CRC is automatically calculated and appended to the transmit payload.

In receive mode, the preamble optionally generates a preamble detect interrupt, and is not stored to the packet RAM. The SFD is used for byte level synchronization, optionally generates an interrupt synchronous with PHR reception, and is not stored to the packet RAM. PHR is received next, and, depending on its contents, dictates the receive packet length, whether dewhitening is to be applied or not, and whether or not FCS bytes are validated (the 16-bit FCS case is handled). Dewhitening is required in Rx if whitening is applied in Tx.


Preamble


Preamble is a 1010 sequence added to the start of the packet during transmission, and removed after receiving the packet. Preamble length is defined in bytes, with a programmable range of 4 bytes to 1000 bytes. It is configured by writing to the BB_NB_ PREAMBLE_BYTES_HIGH register (Address 0x12F) and the BB_NB_PREAMBLE_BYTES_LOW register (Address 0x12E).


SFD


SFD is a 2-byte word that is controlled by writing to the BB_SFD_ HIGH register (Address 0x131) and the BB_SFD_LOW register (Address 0x130). The SFD takes on one of four valid options selected from Table 34. Note that the SFD is transmitted starting from Bit 0.

Table 34. SFD Values
phyMRFSKSFD SFD Value for Coded PHR and PSDU (Bit 0 to Bit 15) SFD Value for Uncoded PHR and PSDU (Bit 0 to Bit 15)
0 0110 1111 0100 1110 1001 0000 0100 1110
1 0110 0011 0010 1101 0111 1010 0000 1110

PHR


PHR is a 2-byte word, as defined in the PHR section in Figure 21. This word is controlled by writing the low byte to the TX_BASE_ ADR register, and the high byte to the address value, TX_BASE_ ADR + 1, because these form the first two bytes of the transmit packet. After issuing the CMD_PHY_TX_15d4 command, the contents of these two bytes are copied into the BB_PHR_LOW (Address 0x132) and BB_PHR_HIGH (Address 0x133)registers, respectively. Likewise, upon successful packet reception, the packet header bytes are copied into the BB_PHR_LOW register and the BB_PHR_HIGH register.

The following sections detail the PHR bit definitions: mode switch, reserved, FCS, whitening, and length.

Mode Switch

Bit 7 of the BB_PHR_LOW register is the MODE_SWITCH bit. The MODE_SWITCH bit is set to 0, indicating there is no data rate or modulation scheme change during the packet transmission. If the ADF7023-J receives a packet with mode switch the MODE_ SWITCH bitset to 1, it does not generate a PHR interrupt, but does generate an INTERRUPT_CRC_CORRECT interrupt and INTERRUPT_RX_EOF interrupt (if they are enabled).

Reserved

The BB_PHR_LOW register, Bits[6:5], are reserved. The reserved bits are set to 0 for the ADF7023-J firmware for transmit mode, and are ignored by the ADF7023-J firmware download module in receive mode.

FCS

Bit 4 of the BB_PHR_LOW register is the FCS bit.

FCS = 0 indicates a 32-bit FCS. This case is not handled automatically by the ADF7023-J firmware download module. For transmit, the user must calculate the 32-bit CRC and add it to the PSDU. In receive mode, the 32-bit CRC is received as part of the PSDU and stored in the packet RAM, CRC is not validated, and the CRC interrupt is not asserted. The INTERRUPT_RX_EOF interrupt indicates when the packet is received.

FCS = 1 indicates a 16-bit CRC. This case is handled automatically by the firmware. In transmit mode, the 16-bit CRC is calculated and appended to the transmit PSDU. In receive mode, the 16-bit CRC is calculated from the incoming payload and, if the CRC is correct, the CRC interrupt is asserted (if enabled).

Whitening

Bit 3 of the BB_PHR_LOW register is the whitening bit. If the whitening bit = 0, the PSDU is not whitened, and if the whitening bit = 1, the PSDU is whitened on transmission. Only the PSDU is whitened, not the SFD or PHR.

In receive mode, if the whitening bit is set to 1 in the received packet header, the ADF7023-J firmware download module automatically dewhitens the received PSDU.

Length

Bits[2:0] of the BB_PHR_LOW register define Bits[10:8] of the PSDU_LENGTH[10:0] word, and Bits[7:0] of the BB_PHR_ HIGH register define Bits[7:0] of the PSDU_LENGTH[10:0] word.

The PSDU_LENGTH[10:0] word can be set to values in the range of 3 to 2047.

Tx/Rx Rolling Data Buffer

In packet mode, when the ADF7023-J receives a packet, the data is stored in a linear sequence in the packet RAM. Prior to transmission, the data to be transmitted is written to the packet RAM in a linear sequence. This functionality is described in the ADF7023-J data sheet.

If the AD_15d4g firmware download module is used, it is possible to receive or transmit packets that are longer than the available packet RAM, which is accomplished via a rolling buffer. The registers applicable to the operation of the rolling buffer are given in Table 35.

Packet RAM locations 0x20 to 0xFF are available for packet data. Bytes 0x00 to 0x1F are allocated for use by the on-chip processor and must not be used for packet data.

Table 35. Registers for Use with Tx/Rx Rolling Data Buffer
Address (Hex) Register Description
0x124 TX_BASE_ADR Start location in packet RAM of Tx buffer
0x125 RX_BASE_ADR Start location in packet RAM of Rx buffer
0x134 BB_RX_BUFFER_SIGNAL Rx buffer nearly full
0x135 BB_RX_BUFFER_SIZE Rx buffer full
0x136 BB_TX_BUFFER_SIGNAL Tx buffer nearly full
0x137 BB_TX_BUFFER_SIZE Tx buffer full

Rolling Buffer in Transmit Mode


In transmit mode, the TX_BASE_ADR registersets the start of the rolling buffer in packet RAM. The BB_TX_BUFFER_SIZE register sets the size of the buffer. Do not allow the buffer size to exceed the available packet RAM. When the value in the BB_TX_BUFFER_ SIZE register is added to the value in the TX_BASE_ADR register, do not exceed Address 0x0FF.

Set the value in the BB_TX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is generated prior to transmission of all the data in the buffer. Typically, the BB_TX_BUFFER_SIGNAL register is set so the interrupt is asserted when half of the data in the buffer has been transmitted.

When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host microprocessor writes new data to the locations from address value TX_BASE_ADR to address value, TX_BASE_ADR + BB_TX_BUFFER_SIGNAL.

When the data in the last byte of the Tx buffer has been transmitted, the ADF7023-J continues transmitting, starting with the data at the address value TX_BASE_ADR. If enabled, an INTERRUPT_BUFFER_FULL interrupt is asserted when the last byte in the buffer is transmitted.

When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host microprocessor writes new data to the locations from address value, TX_BASE_ADR + BB_TX_BUFFER_SIGNAL + 1, to address value, TX_BASE_ADDRESS + BB_TX_BUFFER_SIZE.

Transmission of data continues until PSDU_LENGTH[10:0] bytes are sent, the INTERRUPT_TX_EOF interrupt goes high if enabled, or the user issues the CMD_PHY_ON_15d4 command.

Figure 22. Rolling buffer in transmit mode.
Figure 22. Rolling buffer in transmit mode.

Rolling Buffer in Receive Mode


In receive mode, the RX_BASE_ADDRESS register sets the start of the rolling buffer in packet RAM. The BB_RX_BUFFER_ SIZE register sets the size of the buffer. Do not allow the buffer size to exceed the available packet RAM. When the value in the BB_RX_BUFFER_SIZE register is added to the value in the RX_BASE_ADR register, do not exceed 0x0FF. If the 16-bit FCS checking on the ADF7023-J is enabled, 0x0FD is not exceeded.

Set the value in the BB_RX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted prior to the buffer being filled by received data. Typically, the BB_RX_BUFFER_SIGNAL register is set so the interrupt is asserted when half the buffer has been filled with received data.

When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host microprocessor reads in the data in the locations from address value RX_BASE_ADDRESS to address value, RX_BASE_ADR + BB_RX_BUFFER_SIGNAL.

When the last byte of the Rx buffer has been filled, the ADF7023-J continues writing the received data starting at the RX_BASE_ADR register. If enabled, an INTERRUPT_BUFFER_ FULL interrupt is asserted when the buffer has been filled.

When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host microprocessor reads in the data in the locations from address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIGNAL + 1, to address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIZE.

Reception of data continues until the number of bytes defined in the PSDU_LENGTH[10:0] word has been received and INTERRUPT_RX_EOF and/or INTERRUPT_CRC_CORRECT are asserted (if enabled), or the host microprocessor issues the CMD_PHY_ON_15d4 command.

Note that if a 16-bit CRC is enabled (16-bit FCS), the FCS bytes are placed into the packet RAM as two bytes after the payload, outside of the rolling buffer control. What this means is that if the payload fills up to address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIZE, when the 16-bit FCS is calculated and checked vs. the incoming FCS, the received FCS bytes are placed in the next two memory locations (beyond the address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIZE). If another buffer is defined to start in the memory location immediately following an address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIZE, in this instance the first two bytes are overwritten.

To avoid this situation arising for any length and buffer size, leave an overflow area of two bytes vacant immediately after the Rx buffer. If the Rx buffer is assigned to the upper part of the packet memory, set it to not exceed memory location 0xFD.

If the Rx buffer is placed lower down in packet memory, and is immediately followed in packet memory by a Tx buffer, set the TX_BASE_ADR register to be three bytes greater than address value, RX_BASE_ADDRESS + BB_RX_BUFFER_SIZE. This procedure ensures that if the payload length places the packet end at the BB_RX_BUFFER_SIZE boundary, the overflow of the FCS bytes does not cause overwriting of the first two bytes of the following Tx buffer. The FCS bytes are written into the overflow bytes, instead.

This overwriting issue does not arise in 32-bit CRC mode. In 32-bit CRC mode, the ADF7023-J does not calculate the CRC itself, so the incoming four bytes of FCS are considered the same as the payload, and are loaded into the receive buffer under rolling buffer control.

Figure 23. Rolling buffer in receive mode.
Figure 23. Rolling buffer in receive mode.

Recommended Register Settings

Recommended Automatic Gain Control (AGC) Settings


To optimize the receiver for robust PER performance over the full input power range, overwrite the default AGC clock divide setting in the modem configuration random access memory (MCR). It is recommended to set the AGC_CLOCK_DIVIDE register (Address 0x32F) to 0x12.


Tx Lookup Table (LUT) Settings


The optimized phase-locked loop (PLL) bandwidth settings for T108 operation are built into the AD_15d4g firmware download. Therefore, it is unnecessary to write a custom transmit LUT. Set Bits[5:4] of the RADIO_CFG_7 register (Address 0x113) to 0 when using the PHY_TX_15d4 state.


Reused BBRAM Settings


The ADF7023-J AD_15d4g firmware download reuses the BBRAM registers, and, thus, some default functions are no longer available when in 15d4 mode (see Table 1).

Smart wake mode is not available with the AD_15d4g firmware download because BBRAM Address 0x103, Address 0x104, and Address 0x105 are reused for CCA functionality in the firmware download.

Address matching and static register fix are not available with the AD_15d4g download because BBRAM Address 0x129 to Address 0x137 are reused by the firmware to control the antenna diversity and packet structure.

Transmit test modes are not available within the PHY_TX_ 15d4 state. To use the transmit test modes, it is necessary to revert to the PHY_ON state to get to the PHY_TX state.

To use the optimized PLL settings for T108 operation in PHY_TX state, the sequence outlined in the ADF7023-J data sheet must be followed.

Therefore, the full sequence from the PHY_ON_15d4 state to transmit test mode with optimized T108 PLL settings is as follows:

  1. Issue Command 0xB1 to exit 15d4 mode.
  2. Use the custom transmit LUT. Write 0x2 to Bits[5:4] of the RADIO_CFG_7 register (Address 0x113).
  3. Issue the CMD_CONFIG_DEV command.
  4. Write the custom LUT, as defined in Table 36.
  5. Select the transmit test mode desired (see the test modes information in the ADF7023-J data sheet).
  6. Enter the PHY_TX state.
Table 36. T108 Custom Transmit LUT
Register Data Rate = 50 kbps or 100 kbps (Closed Loop Bandwidth (CLBW) = 130 kHz) Data Rate = 200 kbps (CLBW = 223 kHz)
0x010 0x10 0x20
0x011 0x10 0x20
0x012 0x0F 0x0F
0x013 0x0F 0x0F
0x014 0x1F 0x1F
0x015 0x0F 0x05
0x016 0x1F 0x1F
0x017 0x33 0x33
0x018 0x22 0x22

Example Receiver Settings for 100 kbps and 200 kbps Operation, Automatic Frequency Control (AFC) Enabled

Table 37. Example Rx Settings, AFC Enabled
Parameter 100 kbps, fDEV = 50 kHz 200 kbps, fDEV = 100 kHz
Data Rate 0x3E8 0x7D0
Deviation 0x1F4 0x3E8
IF Filter Bandwidth (BW) 150 kHz 200 kHz
Discriminator Bandwidth 0x20 0x10
Post Demodulated Bandwidth 0x26 0x4B
AGC Thresholds Default Default
AGC Clock Divide 0x12 0x12

Specifications

All specifications are for 100 kbps, 50 kHz deviation only unless otherwise indicated.

Table 38. Application to the IEEE 802.15.4g Standard
Parameter Typical Specification Test Conditions/Comments
PPDU Format
Preamble 4 bytes to 1000 bytes
SFD 2 bytes
PHR 2 bytes
PSDU 3 bytes to 2047 bytes
CRC 16-bit x16 + x12 + x5 + 1
Data Whitening PN9 As defined in the IEEE 802.15.4g standard
Bit Sequence LSB first
Turnaround Time
Rx (CCA) to Tx (Data) 216 µs The CCA_AUTO_TX bit = 0, fast Rx/Tx transitions enabled
Rx (CCA) to Tx (Data) 270 µs The CCA_AUTO_TX bit = 0, fast Rx/Tx transitions disabled
Rx (Data) to Tx (Acknowledge) 210 µs The RX_TO_TX_AUTO_TURNAROUND bit enabled, fast Rx/Tx transitions enabled
Rx (Data) to Tx (Acknowledge) 350 µs The RX_TO_TX_AUTO_TURNAROUND bit enabled, fast Rx/Tx transitions disabled
Tx (Data) to Rx 125 µs The TX_TO_RX_AUTO_TURNAROUND bit enabled, fast Rx/Tx transitions enabled
Tx (Data) to Rx 281 µs The TX_TO_RX_AUTO_TURNAROUND bit enabled, fast Rx/Tx transitions disabled

Test Conditions

Table 39.
Parameter Typical Specification Test Conditions/Comments
Antenna Diversity
Minimum Preamble 10 bytes Antenna diversity enabled, 100 kbps, 50 kHz deviation, AGC on, AFC on
20 bytes Antenna diversity enabled, 200 kbps, 100 kHz deviation, AGC on, AFC on
Sensitivity −103.0 dBm Antenna diversity enabled, delta between antennas = 0 dB, 100 kbps, 50 kHz deviation, PER = 1%, AGC on, AFC on, IF BW = 150 kHz, PSDU length = 12 bytes
−101.5 dBm Antenna diversity enabled, delta between antenna = 20 dB, 100 kbps, 50 kHz deviation, PER = 1%, AGC on, AFC on, IF BW = 150 kHz, PSDU length = 12 bytes
Sensitivity Including IFBW Switching −101.5 dBm Antenna diversity enabled, CCA enabled, 200 kHz to 150 kHz, PER = 1%, delta between antennas = 20 dB, 100 kbps, 50 kHz deviation, AGC on, AFC on, IF BW = 150 kHz, PSDU length = 12 bytes
Processing Gain of Antenna Diversity 9 dB PER = 1%, PSDU length = 12 bytes, 100 kbps, 50 kHz deviation, Rayleigh/static fading: fD = 4 Hz pitch, correlation factor of 0, 1

Code Download Sequence

The AD_15d4g firmware download module must be stored in the PRAM starting from Address 0x0000.

The program RAM can be written to only by using the memory block write. Set the SPI_MEM_WR command to 0x1E.

The sequence to write a firmware module to program RAM is as follows:

  1. Ensure that the ADF7023-J is in the PHY_OFF state.
  2. Issue the CMD_RAM_LOAD_INIT command.
  3. Write the module to PRAM using an SPI memory block write.
  4. Issue the CMD_RAM_LOAD_DONE command.

The firmware module is now stored on program RAM.

著者

Generic_Author_image

Liam O'Hora