AN-045: TRINAMIC Technology Access Package

The TMC2208 is an advanced 1-axis stepper driver, which supports stealthChopand 256 microsteps. This appnote shows how to setup the TMC2208 as a replacement of the A4988 (legacy mode).

Pin Comparison

The TMC2208 in comparison with other motor drivers comes with additional features: 256 microsteps.

An automatic current reduction reduces power dissipation and cooling requirements. Per default, the stand still current reduction is enabled by pulling PDN UART input to GND.

The UART single wire interface allows control of the TMC2208 with any microcontroller UART. This gives the possibilty to program the TMC2208 and add additional features such as full 256 Microsteps control (not only interpolation). UART is not available in legacy mode.

An active DIAG output shows that the driver cannot work normally.

The INDEX output signals the microstep counter zero position, which occurs once per electrical revolution/- four fullsteps. In combination with a mechanical home switch, a more precise homing is enabled.

The TMC2208 is able to control the motor with 256 microsteps per fullstep. In legacy mode the TMC2208 will interpolate received step signals to 256 microsteps.

For optimized performance in legacy mode it is recommended to consider the hints as shown in the comparison below:

Table 1. I/O pin comparison.
Pin A4988
Number
TMC2208
Number
Hints for series using TMC in legacy mode
1 OUT2B OB2 -
2 ENABLE ENN -
3 GND GND -
4 CP1 CP0 -
5 CP2 CPI Tie to CPO using 22nF (not 100nF)
6 VCP VCP -
7 - - -
8 VREG 5VOUT -
9 MS1 MS1 (a)
10 MS2 MS2 (a)
11 MS3 DIAG Diagnostics output. High level upon driver error. Reset by ENN = high. (b)
12 RESET IndexX Configurable index output. Provides index pulse. (c)
13 ROSC CLK CLK input. Tie to GND using short wire for internal clock or supply external clock.
14 SLEEP PDN UART Power down not control input (low=automatic standstill current reduction). Optional UART Input/Output. Power down function can be disabled in UART mode.
15 VDD VCC IO -
16 STEP STEP -
17 REF VREF (d)
18 GND GND -
19 DIR DIR -
20 - - -
21 OUT1B OA2 -
22 VBB1 VS -
23 SENSE1 BRA -
24 OUT1A OA1 -
25 - - -
26 OUT2A OB1 -
27 SENSE2 BRB -
28 VBB2 VS -

I/O Config: Using 2,4,16 microsteps won’t require any change. See table 2 below. Different microstep configurations are marked bold:

Table 2. Configuration of microsteps with I/Os.
TMC2208/A4988
MS1

TMC2208/A4988
MS2

A4988
MS3
A4988
Microsteps
TMC2208
Microsteps
low low low 1 8
high low low 2 2
low high low 4 4
high high high 16 16

With default settings the TMC2208 will interpolate the microsteps set by the I/O configuration pins to 256 microsteps.

TMC2208 doesn’t use third config pin for external microstep configuration, instead this pin offers optional diagnostic function. This is an output pin and should be set as input in the MCU, leave open if unused.

INDEX pin is an output pin and should be set as input in the MCU, leave open if unused.

Analog reference voltage for current scaling or reference current for use of internal sense resistors (optional mode). A voltage between 0V and 2.5V linearly scales the current between 0 and the current scaling defined by the sense resistor setting. Adjust sense resistors to motor current IRMS:

Application Example

Figure 1a. Stepstick schematic.

Figure 1a. Stepstick schematic.

Figure 1b. Stepstick schematic.

Figure 1b. Stepstick schematic.

As an application example a schematic of an StepStick is depicted at the top (subfigure 1a). The TMC2208 is inserted and used in legacy mode (subfigure 1b). Recommended changed parts are marked blue. The Pins PDN/UART, INDEX, DIAG, MS2, MS1 feature additional or slightly changed functions as discussed in table 1.

The sense resistor should be chosen according to the motor current of the application. Table 3 shows the relation between sense rensistor and current for VREF = 2.5A after equation 1. For the application example RSENSE is set to 0.18Ω which allows to control motor currents up to 1.2A.

Table 3. Choice of RSENSE and resulting max. motor current.
RSENSE RMS current[A], VREF = 2.5V or open Fitting motor type (examples)
1.00 0.22 300mA motor
0.82 0.27
0.75 0.29
0.68 0.32 400mA motor
0.5 0.43 500mA motor
0.47 0.46
0.39 0.55 600mA motor
0.33 0.64 700mA motor
0.27 0.77 800mA motor
0.22 0.92 1 A motor
0.18 1.09 1.2A motor
0.15 1.28 1.5A motor
0.12 1.53*
0.10 1.77*
* Value exceeds upper current rating, scaling down required, e.g. by reduced VREF.

著者

Joshua_Pham_Xuan_blue

Joshua Pham Xuan

Joshua Pham Xuan is Staff Engineer for Product Applications at Analog Devices Trinamic Motion Control team based in Hamburg, Germany. Joshua joined the team in 2016 and is an expert in the motion and motor control field.