ADI Logo

Combining the Best of Both Worlds: True Time Delays and Phase Shifters

This article details performance measurements vs. predictions of a 16-channel S-band direct sampling receiver design. The design is based on recently released direct sampling analog-to-digital converters (ADCs) clocked at 4 GSPS and sampling in the second Nyquist zone of the converter. The design configuration is first described with pointers to online references that provide further description. Next, the receiver is shown for both the RF components and the configuration of the embedded digital signal processing (DSP) that is now integrated into modern data converters. Calculations for single-channel performance predictions are presented and compared against measurements. With the single-channel performance understood, a set of measurements combining data from 16 channels evaluates the dynamic range improvements for noise density, spurious signals, and inter[1]modulation products. The article concludes with a set of observations for the multichannel performance trends that can be used for extrapolation to models of large phased arrays implemented with many distributed receivers.

Combining the Best of Both Worlds: True Time Delays and Phase Shifters Cover
ご案内に関する同意
© 1995 - 2025 Analog Devices, Inc. All Rights Reserved

アナログ・デバイセズについて

アナログ・デバイセズ(NASDAQ: ADI)は、物理的世界とデジタル世界の架け橋となり、インテリジェント・エッジでのブレークスルーを実現する、グローバルな半導体企業です。ADIは、アナログ、デジタル、そしてソフトウェアの技術を組み合わせて、工場のデジタル化、モビリティ、デジタル・ヘルスケアの進歩に寄与し、気候変動に取り組み、高い信頼で人と世界とを接続するソリューションを実現しています。