Search You searched for “AD9214BRS-105” Filters Filters Product Categories A/D Converters (ADC) 1 Show More Resources Data Sheet 1 Show More Industry Solutions Aerospace and Defense Systems 1 Show More Tools and Models Technology Solutions Show More Site Section Resource Library1 Result Type Blog Post17Docs & FAQs350Forum Reply5,061Forum Thread1,590Media1Webinar1Show More Groups, Forums & Libraries Audio120Blackfin Processors58Clock and Timing83CrossCore Embedded Studio and Add-ins54Design Support AD9361/AD9363/AD9364339Design Support AD9371/AD9375143Design Support ADRV9008-1/ADRV9008-2/ADRV9009144Differential Amplifiers and ADC Drivers74Show More Author ADIApproved862AdrianC27CatherineR30DaveD82DaveThib63DragosB63EZAdministrator60Fil42Show More Tag RF Integrated Transceivers219Wideband Transceiver IC217HDMI/DVI Devices120ad9361106High Speed A/D Converters >10 MSPS105Audio Signal Processors91Step-Down (Buck) Regulators91amplifiers87Show More Results on Analog.com 2 Results on EngineerZone 7,020 Results on Analog.com 2 Relevance Relevance Oldest First Newest First Sort by AD9214ProductionProductStandard High Speed A/D Converters10-Bit, 65 MSPS/80 MSPS/105 MSPS 3 V Analog-to-Digital Converter PDFDatasheetDocumentationAsk the CommunitySample & BuySample & BuyAD9215: 10-Bit, 65/80/105 MSPS, 3 V A/D Converter Data SheetData SheetPDFAD9215: 10-Bit, 65/80/105 MSPS, 3 V A/D Converter Data Sheet1416 kB <<<1>>> Results on EngineerZone 7,020 Regarding the external clock selection in ADRV9361-Z7035 Board (GPIO Offset : 105)Forum ThreadAnswered Microcontroller no-OS Drivers03 August, 2023Hello support team, ADRV9361-Z7035 board has external clock selection . I have found that K11 is the pin assignment for the selection of external clock( when apply logic low to this pin). In order to select external clock instead of internal clock, which modifications needs to be done in main … adrv9361-z7035hardwaremain.c modificationssystem_topexternal clockWideband Transceiver ICRegarding the use of LT6100 for Current Sensing & Application Note 105 December 2005 Page Number 60,61 [ Requirement is for Low Current Sensing]Forum ThreadAnswered Specialty Amplifiers18 February, 2022… it. I have to sense current of few nA and I have to sense it towards the ground side. In the application note [Application Note 105, December 2005] [Page No : 60,61] the current range is in pico Ampere. So can we use it or not. As per the datasheet … analog circuitcurrent measureadcamplifiersprecision dacsanalog cmos icSpecialty Amplifiersac to dc conversionCurrent Sensing with Low input voltageresearchQuestions about using AD9172-FMC-EBZ and Xilinx's KCU-105 board (MicroSD Image)Forum ThreadAnswered High-Speed DACs19 June, 2020My client wants to test with AD9172-FMC-EBZ and Xilinx KCU-105 board. My customer says that the necessary components are ready, but there is no MicroSD listed below. (wiki.analog.com/.../ad917x-fmc-ebz Setup -MicroSD card with preprogrammed FPGA image to be used with DPGDownloader software Can … KCU-105MicroSD cardAD9172-FMC-EBZWhat is the AD-HSDACFX3-EBZ? And How to configure AD9173-FMC-EBZ & Xilinx KCU 105 boardForum ThreadAnswered High-Speed DACs15 June, 2020… wiki.analog.com/resources/eval/dpg/ad917x-fmc-ebz?s[]=kcu&s[]=105 As above link, additional boards seem to be required for using KCU 105 board as the Data Packet Generatordetailed informatio. But I can't find exact information about these additional boards and configue KCU 105 boards. Would … dpgxilinxStandard High Speed D/A ConvertersMicroSD cardad9173ad-hsdacfx3-ebzkcu105FPGA image fileHigh Speed D/A Converters =30MSPSAD9173-FMC-EBZAD9172-FMC-EBZ with KCU-105Forum ThreadAnswered High-Speed DACs25 September, 2019Hi, I am trying to use AD9172-FMC-EBZ eval board with KCU-105. I have seen that there should be a Micro SD card containing FPGA image to be used with the KCU-105. Is the FPGA image available for downloading? Standard High Speed D/A Converterskcu105High Speed D/A Converters =30MSPSfpga reference designad9172AD6645ASVZ-105 Digital Output Current & driver conditionForum ThreadAnswered High-Speed ADCs20 December, 2018Hi all, In the AD6645 Rev. E datasheet, Absolute Maximum Ratings @ page 7, Digital Output Current : 4 mA We think this is continuous currents. Is it rating of total pin or each pin ? Is it true ? Digital Outputs @ page 18, 10 mA (10 pF × 1 V ÷ 1 ns) 140 mA … digital outputad6645logic outputHigh Speed A/D Converters >10 MSPSStandard High Speed A/D ConvertersAD9633-105 Single-input configuration.Forum ThreadAnswered High-Speed ADCs31 October, 2014Hi, Can the AD96633-105, 12 bit ADC be used with a Single-input configuration? because want to fit a volt of 1.2Vp-p to the ADC in the single-input configuration. Need help with a reference circuit for the AD96633-105 single-input configuration. Kind regards, high_speed_adcad9633High Speed A/D Converters >10 MSPSStandard High Speed A/D ConvertersBF518 Junction Temperature Limit of 105CForum ThreadAnswered Blackfin Processors27 February, 2013… rated @ TAMBIENT = –40°C to +85°C; running at 240MHz clock with 1.37V internal supply.The module this chip is designed into sees an ambient of 105C. Internal to external temp rise within this module has been measured at 5C meaning the BF518 device sees an ambient temperature of 105+5 … junction_temperaturebf518blackfinAN-105Forum ThreadAnswered Precision ADCs08 August, 2024Figure 38 shows SDO and SCL connected to an exclusive-or gate, which would appear to create a Manchester coded data-stream. Do you have a recommended circuit to return the signal to SDO and SCL? Single Channel A/D ConvertersDatasheet/SpecsLTC2433-1Precision A/D Converters5V 80W 105 Degrees Power SolutionForum ThreadAnswered Power Management13 June, 2024Hi, I'm trying to design a regulator solution to meet these requirements: Input V: 12V ±10% Output V: 5V ±2% Output V Ripple: <50mVpp Output I: 16A (80W) Ambient Temperature: 105°C I'm struggling to find a solution to meet the ambient temperature and looking for recommendations on what … µModule Buck Regulatorshardware0µModule RegulatorsStep-Down (Buck) RegulatorsMultiple Output Buck Regulators <<<1234567>>>