Search

Filters
Filters
Tools and Models
- 1
Site Section
- 42
- 26
Results on Analog.com
Newest First
Sort by
- Site_section:Resource Library
- Product_categories.lvl0:RF and Microwave > RF Switches
- Application NoteThis application note answers frequently asked questions about the ADG9xx CMOS wideband switches that are designed primarily to meet the requirements of devices transmitting at industrial, scientific, and medical (ISM) band frequencies (≥900 MHz).
- Analog DialogueThis article presents an effective solution for the post-PA phase shifting block using two Analog Devices ADRF5347 SP4T switches, enabling the reduction of total system cost, while meeting the requirements of the mMIMO system.
- Application NoteThis application note emphasizes the impacts of the arbitrary load conditions on insertion loss, isolation, and power handling using a load pull-based approach.
- Design NoteMassive multiple input, multiple output (M-MIMO) radios have seen their popularity surge in the late stage deployment of 4G LTE cellular base stations, particularly in dense urban areas where small cells effectively filled the cellular coverage voids while boosting higher data speed services.
- Technical ArticlesJun 9, 2023In this paper we summarize measured receive antenna performance for a commercially available 32-element phased array demonstrator.
- Analog DialogueThis article explains the technology advancements enabling this age of wideband software defined radio expected to transform EW and multi-band Radar architectures.
- Design NoteMultiple input, multiple output (MIMO) transceiver architectures are widely used in the design of high power RF wireless communications systems.
- Evaluation Board & KitThe X-Band Development Platform contains one MxFE® software defined, direct RF sampling transceivers, X-Band to C-Band Up/Down Converter, and a X/Ku Band analog phased array proto-typing platform. The target application is phased array radars, electronic warfare, and ground-based SATCOM, specifically a X Band 32 transmit/32 receive channel hybrid beamforming phased array radar. The X-Band Development Platform highlights a complete system solution. It is intended as …
- Evaluation Board & KitADRF5046-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material. For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to V1 and V2 test points to select the switch states; RFC to RF1 …