Search

Filters
Filters
Site Section
- 10
Results on Analog.com
Relevance
Sort by
- Site_section:Resource Library
- Product_categories.lvl0:RF and Microwave > RF Switches
- Resource_types.lvl0:Evaluation Board
- Evaluation Board & KitADRF5046-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material. For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to V1 and V2 test points to select the switch states; RFC to RF1 …
- Evaluation Board & KitThe ADRF5547 is a dual-channel integrated radio frequency (RF) front end ideally suited for time division duplexing (TDD) wireless infrastructure applications. The ADRF5547 is a multichip device that consists of a high power switch and a dual stage low noise amplifier on each channel. This user guide describes the ADRF5547 evaluation board designed to easily evaluate the features and performance of the ADRF5547. A photograph of the evaluation board is shown in Figure 1 …
- Evaluation Board & KitGenerate the evaluation PCB with proper RF circuit design techniques. Signal lines at the RF port must have a 50 Ω impedance, and the package ground leads and backside ground slug must connect directly to the ground plane. The evaluation board available from Analog Devices, Inc. upon request.
- Evaluation Board & KitThe ADRF5043-EVALZ (see Figure 1) is designed to evaluate the features and performance of the ADRF5043 9 kHz to 44 GHz, nonreflective, SP4T switch manufactured in the silicon on insulator (SOI) process. Note that the ADRF5043-EVALZ board is labeled ADRF5042-EVALZ. The same printed circuit board (PCB) is used for both the ADRF5042 and the ADRF5043.For full details on the ADRF5043, see the ADRF5043 data sheet, which must be consulted in conjunction …
- Evaluation Board & KitThe ADRF5545A is a dual-channel integrated radio frequency (RF) front end ideally suited for time division duplexing (TDD) wireless infrastructure applications. The ADRF5545A is a multichip device that consists of a high power switch and a dual stage low noise amplifier on each channel. This user guide describes the ADRF5545A-EVALZ evaluation board designed to easily evaluate the features and performance of the ADRF5545A. A photograph of the evaluation board is shown in Figure …
- Evaluation Board & KitADRF5047-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material. For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to V1 and V2 test points to select the switch states; RFC to RF1 …
- Evaluation Board & KitThe ADRF5042-EVALZ (see Figure 1) is designed to evaluate the features and performance of the ADRF5042 100 MHz to 44 GHz, nonreflective, SP4T switch manufactured in the silicon on insulator (SOI) process. For full details on the ADRF5042, see the ADRF5042 data sheet, which must be consulted in conjunction with this user guide when using the ADRF5042-EVALZ.
- Evaluation Board & KitADRF5026-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material. For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to EN and CTRL test points to select the switch state between RFC-RF1 …
- Evaluation Board & KitADRF5027-EVALZ is a fully populated, connectorized evaluation board using 4-layer, 62 mil thick, RO4003 PCB material. For normal operation, two supply voltages +3.3V and -3.3V should be applied to the VDD and VSS test points respectively, while their ground voltages are connected to the GND test point. Two control input voltages, 0/+3.3V, should be applied to EN and CTRL test points to select the switch state between RFC-RF1 …
- Evaluation Board & KitThe X-Band Development Platform contains one MxFE® software defined, direct RF sampling transceivers, X-Band to C-Band Up/Down Converter, and a X/Ku Band analog phased array proto-typing platform. The target application is phased array radars, electronic warfare, and ground-based SATCOM, specifically a X Band 32 transmit/32 receive channel hybrid beamforming phased array radar. The X-Band Development Platform highlights a complete system solution. It is intended as …
- <<
- <
- 1
- >
- >>