Search

Filters
Filters
Tools and Models
- 1
Site Section
- 279
- 100
- 4
Results on Analog.com
Newest First
Sort by
- Site_section:Resource Library
- Product_categories.lvl0:Processors and Microcontrollers > Microcontrollers
- Application NoteFigure 1. AD7794 current source application (see AD7794 data sheet for more details). Introduction Many applications require current sources to excite various devices for sensor drive, accurate measurement, and other applications. This application note discusses several options that are available to designers when designing current sources using ICs from Analog Devices, Inc. It shows examples of current sources from the microampere range which are integrated in specific devices and also medium to high power discrete …
- Application NoteUsing a keypad input in a MicroConverter application is sometimes required for specific operations.
- Application NoteThis application note introduces the main features of the ADSP-CM408F analog-to-digital converter controller (ADCC) blocks.
- Application NoteIntroduction A key feature of the Analog Devices, Inc., Cortex-M3-based device family is the ability of the devices to download code to their on-chip Flash/electronically erasable (EE) program memory while in circuit. An in circuit code download is conducted over the device universal asynchronous receiver transmitter (UART) serial port, and is thus commonly referred to as a serial download. The serial download capability allows developers to reprogram the device while it …
- Application NoteThis application note introduces the main features of the sinc filters of the ADSP-CM402F/ADSP-CM403F/ADSP-CM407F/ ADSP-CM408F microprocessors, with a focus on high performance motor control applications.
- Application NoteThis application note describes this parallel programming protocol.
- Application NoteWein bridge oscillators have the advantage of requiring only one op amp.
- Application NoteThis application note describes the library functions available in the LINBWSD.dll library.
- Application NoteThis application note describes assembly language techniques for the MAX6951/50 LED drivers using the MAXQ2000’s SPI peripheral.
- Application NoteThis application note describes many of the operational modes and clock options for these devices and details the power savings for each configuration.