Home
Search
left arrow Back to Home
Magnifying Glass Icon close icon

Filters

Filter Icon

Filters

Expand or Collapse Filter Icon
Expand or Collapse Filter Icon
Product Categories
  • A/D Converters (ADC) 737
  • Amplifiers 526
  • Analog Functions 300
  • Audio Products 784
    • Audio Amplifiers 36
  • Clock and Timing 308
Expand or Collapse Filter Icon
Resources
  • Application Note 1
  • Education 2
  • Evaluation Board 1
  • Evaluation Documentation 21
  • Glossary 7
Expand or Collapse Filter Icon
Industry Solutions
  • Automotive Solutions 2
  • Consumer Technology Solutions 3
  • Energy Solutions 1
  • Healthcare Solutions 3
  • Industrial Automation 1
Expand or Collapse Filter Icon
Tools and Models
Expand or Collapse Filter Icon
Technology Solutions
Expand or Collapse Filter Icon
Site Section
  • 36
  • 20
  • 1
Expand or Collapse Filter Icon
Result Type
  • 26
  • 5,341
  • 84,129
  • 222,978
  • 455,895
  • 1,145
Expand or Collapse Filter Icon
Groups, Forums & Libraries
  • 11,832
  • 10,781
  • 13,299
  • 13,219
  • 10,110
  • 19,404
  • 7,327
  • 17,422
Expand or Collapse Filter Icon
Author
  • 28,868
  • 3,160
  • 3,617
  • 1,828
  • 1,996
  • 5,267
  • 2,200
  • 1,512
Expand or Collapse Filter Icon
Tag
  • 46,612
  • 46,098
  • 44,367
  • 33,033
  • 27,343
  • 23,453
  • 23,148
  • 20,524
Analog Devices Inc. logo Results on Analog.com
36
engineer-zone-play-icon Results on EngineerZone
769,517

Results on Analog.com

36
Newest First
Relevance
Oldest First
Newest First

Sort by

  • Site_section:Resource Library
  • Product_categories.lvl0:Audio Products > Audio Amplifiers
Clear All Filters Icon
External Link Icon Right Arrow Icon External Link Icon External Link Icon Tag pst-icon
  1. ADI’s Medical Ultrasound Solutions
    Application Note
    By transmitting acoustic energy into the body and receiving and processing the returning reflections, ultrasound systems can generate images of internal organs and structures, map blood flow and tissue motion, and provide highly accurate blood velocity information.
  2. Spread Spectrum
    Glossary
    Spread-Spectrum is a technology that modulates a signal over many carrier frequencies at once. This method can be used to make transmissions more secure, reduce interference, and improve bandwidth-sharing. Spread-spectrum techniques can also be used to reduce electromagnetic interference by dithering the clock frequency so emissions are no longer concentrated at one frequency.
  3. Class A
    Glossary
    The simplest type of amplifier, class A amplifiers are those in which the output transistors conduct (i.e. do not fully turn off) irrespective of the output signal waveform. This type of amplifier is typically associated with high linearity but low efficiency.
  4. Class G
    Glossary
    Class G amplifiers are similar to class AB amplifiers except they use two or more supply voltages. When operating at low signal levels, the amplifier uses a lower supply voltage. As the signal level increases, the amplifier automatically picks the appropriate supply voltage. Class G amplifiers are more efficient than class AB amplifiers since they use the maximum supply voltage only when required, while a class AB amplifier always uses the maximum supply voltage.
  5. Class D
    Glossary
    Class D amplifiers are those that output a switching waveform, at a frequency far higher than the highest audio signal that needs to be reproduced. The low-pass filtered, average value of this waveform corresponds to the actual required audio waveform. Class D amplifiers are highly efficient (often up to 90% or higher) since the output transistors are either fully turned on or off during operation. This completely eliminates the use of the linear region …
  6. Class AB
    Glossary
    Class AB amplifiers combine Class A and Class B to achieve an amplifier with more efficiency than Class A but with lower distortion than class B. This is achieved by biasing both transistors so they conduct when the signal is close to zero (the point where class B amplifiers introduce non-linearities). The transistors transition to class B operation for large excursions. So, for small signals both transistors are active, acting like a class A …
  7. Class B
    Glossary
    Class B amplifiers are those in which the output transistors only conduct during half (180 degrees) of the signal waveform. To amplify the entire signal, two transistors are used: one conducting for positive output signals and the other conducting for negative outputs. Class B amplifiers are much more efficient than class A amplifiers, but have high distortion due to the crossover point when the two transistors transition from on to off.
  8. Class H
    Glossary
    Class H amplifiers modulate the supply voltage to the amplifier output devices so that it is never higher than necessary to support the signal swing. This reduces dissipation across the output devices connected to that supply and allows the amplifier to operate with an optimized class AB efficiency regardless of output power level. Class H amplifiers are generally more complex than other designs, with extra control circuitry required to predict and control the supply voltage.
  9. Enhance Your Augmented/Virtual Reality Experience with Nearfield Surround Sound
    Technical Articles
    Jun 4, 2021
    Discover the features of a tiny Class D audio amplifier that makes nearfield surround sound in a wearable head mount a reality.
  10. EVAL-SSM3525
    Evaluation Board & Kit
    The EVAL-SSM3525Z is an evaluation board for the SSM3525, which is an integrated mono 30 W, high efficiency, stereo Class-D audio amplifier with digital input. The application circuit requires a few external components and can operate from a single 4.5 V to 17 V supply. It is capable of delivering 15.3 W of continuous output power into a 4 Ω load from a 12 V power supply, with <1% total harmonic …
    EVAL-SSM3525

    Documentation

  • <<
  • <
  • 1
  • 2
  • 3
  • 4
  • >
  • >>

Results on EngineerZone

769,517
    Clear All Filters Icon
    1. Supply (Vs) current consumption

      Forum Thread
      Answered
      Clock and Timing
      28 May, 2025
      Hello, What is the typical and maximum current consumption of the supply pin (Vs) in AD9516-1? I couldn't find it in the datasheet (Rev C) in the TPC or the figures. Best regards~
      Clock Generation DevicesDatasheet/SpecsClock Generation and DistributionClock Distribution Devicesclock and timingad9516-1

    2. There are three 24-Bit registers in the ADE9103 which are broken into three separate 8-bit registers. Is there any way to make sure you get the correct data when you read all three registers?

      Forum Thread
      Answered
      Energy Monitoring and Metering
      27 May, 2025
      There are three 24-Bit registers in the ADE9103 which are broken into three separate 8-bit registers (see page 53 of the data sheet). https://www.analog.com/media/en/technical-documentation/data-sheets/ade9103-ade9112-ade9113.pdf#page=37&zoom=100,0,105 I_WAV_HI, I_WAV …
      Datasheet/SpecsADE9103

    3. Question about disabling CRC in the ADE9103 and basic CRC operation

      Forum Thread
      Answered
      Energy Monitoring and Metering
      27 May, 2025
      Page 49 of the data sheet for the ADE9103 indicates that you can enable or disable CRC Checking in the Device by setting CONFIG0 Register BIT #1 (CRC_EN_SPI_WRITE) to 1 to enable CRC or 0 to disable CRC checking. The description for the Bit indicates, &ldquo;Enables CRC …
      Datasheet/SpecsADE9103

    4. Need alternative for AD698AP

      Forum Thread
      Answered
      Specialty Amplifiers
      27 May, 2025
      Hi everyone, My company has developed a board for LVDT signal measurement based on the Analog Devices AD698AP. However, since this chip is now obsolete, and we plan to keep this product in production for the next 10 to 15 years, we are looking for a suitable alternative. I noticed …
      hardwareLVDT Sensor Amplifiersad698Specialty AmplifiersAD698AP

    5. Need help running the simulation

      Forum Thread
      Answered
      Operational Amplifiers
      27 May, 2025
      i received the schematics, from colleague, but can't run the simulation, the log file is not so easy to understand.
      Operational Amplifiers (Op Amps)simulationhardwarePrecision Op Amps (Vos &le;1mV &amp; TCVos &le;2uV/C)High Output Current Op Amps = 100mALow Noise Op Amps (= 10nV/vHz)

    6. ADAR1000-EVALZ Not Respondin

      Forum Thread
      Answered
      RF and Microwave
      27 May, 2025
      I have the ADAR1000-EVALZ and i am trying to control it using the SDP-S but the gain and phase of the Eval. Board are not controlled through GUI and only respond when writing the manual registers through the "Manual Register Write" menu. I tried to adjust the gains …
      Phase Shifterssoftwareadar1000Beamformersrf and microwaveAnalog Devices ADAR1000 Evaluation Softwareand Vector ModulatorsRF Integrated Transceivers

    7. Not output clock

      Forum Thread
      Answered
      Clock and Timing
      27 May, 2025
      We are currently evaluating the hardware.We are having trouble with ANALOGDEVICES AD9246(DPLL) not outputting. We are using the ACE tool to set the register settings, but it does not output.Could you please tell me how to check the cause of the no output.
      Clock Generation and Distributionhardwaread9545Clock SynchronizationHigh Speed A/D Converters &gt;10 MSPSad9246Standard High Speed A/D Converters

    8. SPI sequence Register For Fixed Out

      Forum Thread
      Answered
      Direct Digital Synthesis (DDS)
      27 May, 2025
      I want to set a fixed output frequency on the AD9910 via register configuration. I haven't succeeded yet. What is the correct sequence of register settings to configure a fixed output frequency?
      Datasheet/Specsclock and timingDirect Digital Synthesis (DDS)ad9910

    9. How to properly use DC Input Entry

      Forum Thread
      Answered
      SigmaDSP Processors & SigmaStudio Dev. Tool
      26 May, 2025
      Hi, I want to use DC Input Entry to index ISF. So, if I'm using 1467 - 32bit, according to AD Wiki I need to use integer value for ISF: 32.0 But before that I wanted to debug input value with a Readback, but it reads the wrong value …
      Audio Signal ProcessorsSigma Studio (Rev. 4.7)softwareDSP Readbackadau1467SigmaDSP Audio ProcessorsDC Input Entry

    10. Output not following the Input signal.

      Forum Thread
      Answered
      Operational Amplifiers
      26 May, 2025
      Hello I have designed a photodiode circuit to convert current to voltage using the ADA4817-1 IC. The output voltage is change between 0.7V to 4V depend of the light source. I expected the output signal will follow the input signal but that is not what happened. In fact …
      Operational Amplifiers (Op Amps)hardwareLow Input Bias Current Op Amps (&le;100 pA)ada4817-1

    • <<
    • <
    • 1
    • 2
    • 3
    • 4
    • 5
    • 6
    • 7
    • >
    • >>
  • Who We Are
  • Careers
  • Newsroom
  • What We Do (Signals+)
  • Investor Relations
  • Quality & Reliability
  • Sales and Distribution
  • What's New on Analog.com
  • Contact Us
  • Support
  • EngineerZone
  • Resources
  • Wiki
  • Analog Dialogue
  • ADI Developer Portal
  • Legal and Risk
  • Accessibility
  • Privacy Policy
  • Privacy Settings
  • Cookie Settings
  • EZ
  • Linkedin
  • Instagram
  • Youtube
  • Facebook
  • Twitter