Search

Filters
Filters
Site Section
- 38
- 20
- 1
Results on Analog.com
Relevance
Sort by
- Site_section:Resource Library
- Product_categories.lvl0:Amplifiers
- Industry_solutions.lvl0:Wireless Communication Solutions
- Technical ArticlesOct 1, 2019Industries can often benefit from technology created for a different industry’s application. The microwave oven is generally credited to an engineer working on radars who noticed his lunch was melting during testing.
- Technical Articles
- Technical ArticlesMay 1, 2021This article presents experimental results utilizing a 16-channel transmit and 16-channel receive subarray in which all transmit and receive channels are calibrated using hardened DSP blocks within the digitizer integrated circuit (IC).
- Application NoteAN-2547 discusses selecting a driver amplifier to provide the first stage of gain at the output of an IQ modulator, specifically using the ADL5375 IQ modulator and the ADL5320 driver amplifier.
- Technical ArticlesSep 20, 2023This article will focus on GaN PA pulse droop as a nonideality of real-world radar performance and will discuss what can be done to mitigate its negative impact on radar range.
- Technical ArticlesMar 1, 2016Radio system design is becoming ever more complex, with increasing demands on performance, cost, and power consumption. With many different frequency bands in use around the world, and commercial systems now extending up into the millimeter wave frequencies above 50 GHz, today’s RF system designer is facing significant challenges. Wideband amplifiers are addressing this challenge of multiple bands and complex radio front ends. Instead of a separate chain of components for each band, the …
- Evaluation Board & KitThe evaluation board is powered by a single 5 V supply. The power supply is decoupled by 10 µF and 0.1 µF capacitors. On board regulators provide a 2.5 V common mode voltage and 3 V logic supply voltage to enable/disable the power-down feature. Several termination options are also provided to allow the user to terminate unused inputs/outputs of the amplifier for single-ended applications.
- Application NoteThis application note looks at some basic filter key specifications concepts.