Abstract
This application note presents various voltage-controlled oscillator (VCO) designs for popular IF frequencies of 85MHz, 190MHz, and 210MHz. These designs reduce the number of iterations required for optimized results. Analysis can be accomplished with a simple spreadsheet program.
Additional Information:
- Quick View Data Sheet for the MAX2306/MAX2308/MAX2309
- Quick View Data Sheet for the MAX2310/MAX2312/MAX2314/MAX2316
Introduction
This application note presents various voltage-controlled oscillator (VCO) designs for popular IF frequencies of 85MHz, 190MHz, and 210MHz. These designs reduce the number of iterations required for optimized results. Analysis can be accomplished with a simple spreadsheet program.
VCO Design
Figure 2 shows the differential tank circuit used for the MAX2310 IF VCO. For analysis purposes, the tank circuit must be reduced to an equivalent simplified model. Figure 1 depicts the basic VCO model. The frequency of oscillation can be characterized by EQN1:
fosc = frequency of oscillation
L = inductance of the coil in the tank circuit
Cint = internal capacitance of the MAX2310 tank port
Ct = total equivalent capacitance of the tank circuit
Figure 1. Basic VCO model.
Rn = equivalent negative resistance of the MAX2310 tank port
Cint = internal capacitance of the MAX2310 tank port
Ct = total equivalent capacitance of the tank circuit
L = inductance of the coil in the tank circuit
Figure 2. The MAX2310 tank circuit.
Inductor L resonates with the total equivalent capacitance of the tank and the internal capacitance of the oscillator (Ct+Cint) (see Figure 1). Ccoup provides DC block and couples the variable capacitance of the varactor diodes to the tank circuit. Ccent is used to center the tank's oscillation frequency to a nominal value. It is not required but adds a degree of freedom by allowing one to fine-tune resonance between inductor values. Resistors (R) provide reverse-bias voltage to the varactor diodes via the tune voltage line (Vtune). Their value should be chosen large enough so as not to affect loaded-tank Q but small enough so that 4kTBR noise is negligible. The resistors' noise voltage gets modulated by KVCO, producing phase noise. Capacitance Cv is the variable tuning component in the tank. The capacitance of varactor diode (Cv) is a function of reverse-bias voltage (see Appendix A for the varactor model). Vtune is the tuning voltage from a phase-locked loop (PLL).
Figure 3 shows the lumped Cstray VCO model. Parasitic capacitance and inductance plague every RF circuit. In order to predict the frequency of oscillation, the parasitic elements must be taken into account. The circuit in Figure 3 lumps the parasitic elements in one capacitor called Cstray. The frequency of oscillation can be characterized by EQN2:
L = inductance of the coil in the tank circuit
Cint = internal capacitance of the MAX2310 tank port
Ccent = tank capacitor used to center oscillation frequency
Cstray = lumped stray capacitance
Ccoup = tank capacitor used to couple the varactor to the tank
Cv = net variable capacitance of the varactor diode (including series
inductance)
Cvp = varactor-pad capacitance
Figure 3. Lumped Cstray model.
Figure 4 depicts the detailed VCO model. It takes into account the capacitance of the pads but does not include the effects of series inductance for simplicity. Cstray is defined as:
CL = capacitance of the inductor
CLP = capacitance of the inductor pads
CDIFF = capacitance due to parallel traces
Figure 4. Detailed VCO model.
Rn = equivalent negative resistance of the MAX2310 tank port
Cint = internal capacitance of the MAX2310 tank port
LT = inductance of series trace to the inductor tank circuit
CDIFF = capacitance due to parallel traces
L = inductance of the coil in the tank circuit
CL = capacitance of the inductor
CLP = capacitance of inductor pads
Ccent = tank capacitor used to center oscillation frequency
Ccoup = tank capacitor used to couple the varactor to the tank
Cvar = variable capacitance of the varactor diode
Cvp = varactor-pad capacitance
LS = series inductance of the varactor
R = resistance of the varactor reverse-bias resistors
To simplify analysis, inductance LT is ignored in this design. The effects of LT are more pronounced at higher frequencies. To mathematically model the shift in frequency due to LT with the spreadsheets that follow, the value of CDIFF can be increased appropriately. Minimize inductance LT to prevent undesired series resonance. This can be accomplished by making the traces short.
Tuning Gain
Tuning gain (Kvco) must be minimized for best closed-loop phase noise. Resistors in the loop filter as well as the resistors "R" (Figure 2) will produce broadband noise. Broadband thermal noise ( ) will modulate the VCO by Kvco, which is measured in MHz/V. There are two ways to minimize Kvco. One is to minimize the frequency range over which the VCO must tune. The second way is to maximize the tuning voltage available. To minimize the frequency range over which the VCO must tune, tight tolerance components must be used, as will be shown. To maximize tuning voltage, a charge pump with a large compliance range is needed. This is usually accomplished by using a larger Vcc. The compliance range for the MAX2310 is 0.5V to Vcc-0.5V. In battery-powered applications, the compliance range is usually fixed by battery voltage or a regulator.
Basic Concept for Trimless Design
VCO design for manufacturability with real-world components will require an error budget analysis. In order to design a VCO to oscillate at a fixed frequency (fosc), the tolerance of the components must be taken into consideration. Tuning gain (Kvco) must be designed into the VCO to account for these component tolerances. The tighter the component tolerance, the smaller the possible tuning gain, and the lower the closed-loop phase noise. For worst-case error budget design, we will look at three VCO models:
- Maximum-value components (EQN5)
- Nominal tank, all components perfect (EQN2)
- Minimum-value components (EQN4)
All three VCO models must cover the desired nominal frequency. Figure 5 shows visually how the three designs must converge to provide a manufacturable design solution. Observation of EQN1 and Figure 5 reveal that minimum-value components will shift the oscillation frequency higher and that maximum-value components will shift the oscillation frequency lower.
Figure 5. Worst-case and nominal-tank centering.
Minimum tuning range must be used in order to design a tank with the best closed-loop phase noise. Therefore, the nominal tank should be designed to cover the center frequency with overlap to take into account device tolerance. The worst-case high-tune tank and worst-case low-tune tank should tune just to the edge of the desired oscillation frequency. EQN2 can be modified by component tolerance to produce a worst-case high-tune tank EQN4 and a worst-case low-tune tank EQN5.
TL = % tolerance of the inductor (L)
TCINT = % tolerance of the capacitor (CINT)
TCCENT = % tolerance of the capacitor (CCENT)
TCCOUP = % tolerance of the capacitor (CCOUP)
TCV = % tolerance of the varactor capacitance (CV)
EQN4 and EQN5 assume that the strays do not have a tolerance.
General Design Procedure
Step 1
Estimate or measure pad capacitance and other strays. The stray capacitance on the MAX2310 Rev C EV kit has been measured with a Boonton Model 72BD capacitance meter. CLP = 1.13pF, CVP = 0.82pF, CDIFF = 0.036pF.
Step 2
Determine the value for capacitance Cint. This can be found in the MAX2310/MAX2312/MAX2314/MAX2316 data sheet on Page 5. Typical operating characteristic TANKH PORT 1/S11 vs. FREQUENCY shows the equivalent parallel RC values for several popular LO frequencies. Appendix B includes tables of Cint versus frequency for the high- and low-band tank ports. Keep in mind that the LO frequency is twice the IF frequency.
Example:
For an IF frequency of 210MHz (high-band tank), the LO will operate at 420MHz. From Appendix B, Table 5, Cint = 0.959pF.
Step 3
Choose an inductor. A good starting point is using the geometric mean. This will be an iterative process.
This equation assumes L in (nH) and C in (pF) (1x10-9 x 1x10-12 = 1x10-21). L = 11.98nH for a fosc = 420MHz. This implies a total tank capacitance C = 11.98pF. An appropriate initial choice for an inductor would be 12nH Coilcraft 0805CS-12NXGBC 2% tolerance.
When choosing an inductor with finite step sizes, the following formula EQN6.1 will be useful. The total product LC should be constant for a fixed oscillation frequency fosc.
LC = 143.5 for a fosc = 420MHz. The trial-and-error process with the spreadsheet in Table 3 yielded an inductor value of 18nH 2% with a total tank capacitance of 7.9221pF. The LC product for the tank in Figure 8 is 142.59, close enough to the desired LC product of 143.5. One can see this is a useful relationship to have on hand. For best phase noise, choose a high-Q inductor like the Coilcraft 0805CS series. Alternatively, a micro-strip inductor can be used if the tolerance and Q can be controlled reasonably.
Step 4
Determine the PLL compliance range. This is the range over which the VCO tuning voltage (Vtune) will be designed to work. For the MAX2310, the compliance range is 0.5V to Vcc-0.5V. For a Vcc = 2.7V, this would set the compliance range to 0.5 to 2.2V. The charge-pump output will set this limit. The voltage swing on the tank is 1Vp-p centered at 1.6VDC. Even with large values for Ccoup, the varactor diodes will not be forward-biased. This is a condition to be avoided, as the diode will rectify the AC signal on the tank pins, producing undesirable spurious response and loss of lock in a closed-loop PLL.
Step 5
Choose a varactor. Look for a varactor with good tolerance over your specified compliance range. Keep the series resistance small. For a figure of merit, check that the self-resonant frequency of the varactor is above the desired operating point. Look at the Cv(2.5V)/Cv(0.5V) ratio at your compliance-range voltage. If the coupling capacitors Ccoup were chosen large, then the maximum tuning range can be calculated using EQN2. Smaller values of capacitor Ccoup will reduce this effective frequency tuning range. When choosing a varactor, it should have a tolerance specified at your given compliance-range mid and end points. Select a hyperabrupt varactor such as the Alpha SMV1763-079 for linear tuning response. Take the value for total tank capacitance, and use that for Cjo of the varactor. Remember, Ccoup will reduce the net capacitance coupled to the tank.
Step 6
Pick a value for Ccoup. Large values of Ccoup will increase tuning range by coupling more of the varactor into the tank at the expense of decreasing tank-loaded Q. Smaller values of Ccoup will increase the effective Q of the coupled varactor and loaded Q of the tank at the expense of reducing tuning range. Typically this will be chosen as small as possible, while still getting the desired tuning range. Another benefit of choosing Ccoup small is that it reduces the voltage swing across the varactor diode. This will help thwart forward-biasing the varactor.
Step 7
Pick a value for Ccent, usually around 2pF or greater for tolerance purposes. Use Ccent to center the VCO's nominal frequency.
Step 8
Iterate with the spreadsheet.
MAX2310 VCO Tank Designs for IF Frequencies of 85MHz, 190MHz, and 210MHz
The following spreadsheets show designs for several popular IF frequencies for the MAX2310. Keep in mind that the LO oscillates at twice the desired IF frequency.
Figure 6. 85MHz low-band IF tank schematic.
Table 1. 85MHz Low-Band IF Tank Design
Light grey indicates calculated values. |
Darker grey indicates user input. |
MAX2310 Low-Band Tank Design and Tuning Range | |||||
Total Tank Capacitance vs. V tune | |||||
V tune | Total C | Ct
(Nominal) |
Ct (Low) |
Ct (High) |
|
0.5V | Ct high | 14.1766pF | 13.3590pF | 14.9459pF | |
1.375V | Ct mid | 12.8267pF | 11.7445pF | 13.7620pF | |
2.2V | Ct low | 11.4646pF | 10.3049pF | 12.4534pF | |
Tank Components |
|
||||
C coup
|
18pF
|
0.9pF
|
5%
|
||
C cent
|
5.6pF
|
0.1pF
|
2%
|
||
C stray
|
0.70pF
|
||||
L
|
68nH
|
2.00%
|
|||
C int
|
0.902pF
|
10.00%
|
|||
Parasitics and Pads (C stray) | |||||
Due to Q |
C L
|
0.1pF
|
|||
Ind. pad |
C Lp
|
1.13pF
|
|||
Due to || |
C diff
|
0.036pF
|
|||
Var. pad |
C vp
|
0.82pF
|
|||
Varactor Specs | |||||
Alpha SMV1255-003 | |||||
Cjo |
82pF
|
Varactor Tolerance
|
|||
Vj |
17V
|
0.5V
|
19.00%
|
||
M |
14
|
1.5V
|
29.00%
|
||
Cp |
0pF
|
2.5V
|
35.00%
|
||
Rs |
1Ω
|
Reactance
|
|||
Ls |
1.7nH
|
X Ls
|
1.82 | ||
Freq |
170.00MHz
|
||||
Nominal Varactor |
X c
|
Net Cap
|
|||
Cv high
|
54.64697pF
|
-17.1319
|
61.12581pF
|
||
Cv mid
|
27.60043pF
|
-33.92
|
29.16154pF
|
||
Cv low
|
14.92387pF
|
-62.7321
|
15.36874pF
|
||
Negative Tol Varactor (Low Capacitance) | |||||
Cv high
|
44.26404pF
|
-21.1505
|
48.42117pF
|
||
Cv mid
|
19.59631pF
|
-47.7746
|
20.37056pF
|
||
Cv low
|
9.700518pF
|
-96.5109
|
9.886531pF
|
||
Positive Tol Varactor (High Capacitance) | |||||
Cv high
|
65.02989pF
|
-14.3965
|
74.41601pF
|
||
Cv mid
|
35.60456pF
|
-26.2945
|
38.24572pF
|
||
Cv low
|
20.14723pF
|
-46.4682
|
20.96654pF
|
||
Nominal
LO (Nom) Range |
Low
Tol IF (High) Range |
Nominal
IF (Nom) Range |
High
Tol IF (Low) Range |
||
F low
|
162.10MHz
|
84.34MHz
|
81.05MHz
|
78.16MHz
|
|
F mid
|
170.42MHz
|
89.95MHz
|
85.21MHz
|
81.45MHz
|
|
F high
|
180.25MHz
|
96.03MHz
|
90.13MHz
|
85.62MHz
|
|
BW
|
18.16MHz
|
11.69MHz
|
9.08MHz
|
7.46MHz
|
|
% BW
|
10.65%
|
12.99%
|
10.65%
|
9.16%
|
|
Nominal IF Frequency |
|
||||
Design
Constraints
|
|||||
Condition for bold number |
<IF
|
=IF
|
> IF
|
||
Delta |
0.66
|
-0.21
|
0.62
|
||
Test |
pass
|
pass
|
pass
|
||
Raise or lower cent freq by |
-0.21
|
MHz
|
|||
Inc or dec BW |
-1.28
|
MHz
|
|||
Cent adj for min BW |
84.98
|
MHz
|
|||
K vco |
10.68MHz/V
|

Figure 7. 190MHz high-band IF tank schematic.
Table 2. 190MHz High-Band IF Tank Design
Light grey indicates calculated values. |
Darker grey indicates user input. |
MAX2310 High-Band Tank Design and Tuning Range | |||||
Total Tank Capacitance vs. V tune | |||||
V tune
|
Total C | Ct
(Nominal) |
Ct (Low) |
Ct (High) |
|
0.5V
|
Ct high | 10.4968pF | 10.0249pF | 10.9126pF | |
1.375V
|
Ct mid | 9.6292pF | 8.8913pF | 10.2124pF | |
2.2V
|
Ct low | 8.6762pF | 7.7872pF | 9.3717pF | |
Tank Components |
|
||||
C coup
|
12pF
|
0.1pF
|
1%
|
||
C cent
|
3.4pF
|
0.1pF
|
3%
|
||
C stray
|
0.70pF
|
||||
L
|
18nH
|
2.00%
|
|||
C int
|
0.954pF
|
10.00%
|
|||
Parasitics and Pads (C stray) | |||||
Due to Q |
C L
|
0.01pF
|
|||
Ind. pad |
C Lp
|
1.13pF
|
|||
Due to || |
|
0.036pF
|
|||
Var. pad |
C vp
|
0.82pF
|
|||
Varactor Specs | |||||
Alpha SMV1255-003 | |||||
Cjo |
82pF
|
Varactor Tolerance
|
|||
Vj |
17V
|
0.5V
|
19.00%
|
||
M |
14
|
1.5V
|
29.00%
|
||
Cp |
0pF
|
2.5V
|
35.00%
|
||
Rs |
1Ω
|
Reactance
|
|||
Ls |
1.7nH
|
X Ls
|
4.06 | ||
Freq |
380.00MHz
|
||||
Nominal Varactor |
X c
|
Net Cap
|
|||
Cv high
|
54.64697pF
|
-7.66426
|
116.1695pF
|
||
Cv mid
|
27.60043pF
|
-15.1747
|
37.67876pF
|
||
Cv low
|
14.92387pF
|
-28.0643
|
17.44727pF
|
||
Negative Tol Varactor (Low Capacitance) | |||||
Cv high
|
44.26404pF
|
-9.46205
|
77.51615pF
|
||
Cv mid
|
19.59631pF
|
-21.3728
|
24.19031pF
|
||
Cv low
|
9.700518pF
|
-43.1759
|
10.70708pF
|
||
Positive Tol Varactor (High Capacitance) | |||||
Cv high
|
65.02989pF
|
-6.44056
|
175.8588pF
|
||
Cv mid
|
35.60456pF
|
-11.7633
|
54.36221pF
|
||
Cv low
|
20.14723pF
|
-20.7884
|
25.03539pF
|
||
Nominal LO (Nom) Range |
Low Tol IF (High) Range |
Nominal IF (Nom) Range |
High Tol IF (Low) Range |
||
F low
|
366.15MHz
|
189.23MHz
|
183.07MHz
|
177.78MHz
|
|
F mid
|
382.29MHz
|
200.94MHz
|
191.14MHz
|
183.78MHz
|
|
F high
|
402.74MHz
|
214.71MHz
|
201.37MHz
|
191.84MHz
|
|
BW
|
36.59MHz
|
25.47MHz
|
18.29MHz
|
14.06MHz
|
|
% BW
|
9.57%
|
12.68%
|
9.57%
|
7.65%
|
|
Nominal IF Frequency |
|
||||
Design
Constraints
|
|||||
Condition for bold number |
< IF
|
= IF
|
> IF
|
||
Delta |
0.77
|
-1.14
|
1.84
|
||
Test |
pass
|
pass
|
pass
|
||
Raise or lower cent freq by |
-1.14
|
MHz
|
|||
Inc or dec BW |
-2.61
|
MHz
|
|||
Cent adj for min BW |
190.54
|
MHz
|
|||
K vco |
21.52MHz/V
|

Figure 8. 210MHz high-band IF tank schematic.
Table 3. 210MHz High-Band IF Tank Design
Light grey indicates calculated values. |
Darker grey indicates user input. |
MAX2310 High-Band Tank Design and Tuning Range | |||||
Total Tank Capacitance vs. V tune | |||||
V tune
|
Total C | Ct (Nominal) |
Ct (Low) |
Ct (High) | |
0.5V
|
Ct high | 8.8304pF | 8.1465pF | 9.4877pF | |
1.35V
|
Ct mid | 7.9221pF | 7.0421pF | 8.6970pF | |
2.2V
|
Ct low | 6.9334pF | 5.9607pF | 7.7653pF | |
Tank Components |
|
||||
C coup
|
12pF
|
0.6pF
|
5%
|
||
C cent
|
1.6pF
|
0.1pF
|
6%
|
||
C stray
|
0.70pF
|
||||
L
|
18nH
|
2.00%
|
|||
C int
|
0.959pF
|
10.00%
|
|||
Parasitics and Pads (C stray) | |||||
Due to Q |
C L
|
0.1pF
|
|||
Ind. pad |
C Lp
|
1.13pF
|
|||
Due to || |
C diff
|
0.036pF
|
|||
Var. pad |
C vp
|
0.82pF
|
|||
Varactor Specs | |||||
Alpha SMV1255-003 | |||||
Cjo |
82pF
|
Varactor Tolerance
|
|||
Vj |
17V
|
0.5V
|
19.00%
|
||
M |
14
|
1.5V
|
29.00%
|
||
Cp |
0pF
|
2.5V
|
35.00%
|
||
Rs |
1Ω
|
Reactance
|
|||
Ls |
1.7nH
|
X Ls
|
4.49 | ||
Freq |
420.00MHz
|
||||
Nominal Varactor |
X
c
|
Net
Cap
|
|||
Cv high
|
54.64697pF
|
-6.93433
|
154.787pF
|
||
Cv mid
|
27.60043pF
|
-13.7295
|
40.99616pF
|
||
Cv low
|
14.92387pF
|
-25.3916
|
18.12647pF
|
||
Negative Tol Varactor (Low Capacitance) | |||||
Cv high
|
44.26404pF
|
-8.56091
|
92.99806pF
|
||
Cv mid
|
19.59631pF
|
-19.3373
|
25.51591pF
|
||
Cv low
|
9.700518pF
|
-39.0639
|
10.95908pF
|
||
Positive Tol Varactor (High Capacitance) | |||||
Cv high
|
65.02989pF
|
-5.82717
|
282.5852pF
|
||
Cv mid
|
35.60456pF
|
-10.643
|
61.54791pF
|
||
Cv low
|
20.14723pF
|
-18.8086
|
26.45795pF
|
||
Nominal LO (Nom) Range |
Low Tol IF (High) Range |
Nominal IF (Nom) Range |
High Tol IF (Low) Range |
||
F low
|
399.20MHz
|
209.92MHz
|
199.60MHz
|
190.67MHz
|
|
F mid
|
421.47MHz
|
225.78MHz
|
210.73MHz
|
199.14MHz
|
|
F high
|
450.52MHz
|
245.41MHz
|
225.26MHz
|
210.75MHz
|
|
BW
|
51.31MHz
|
35.49MHz
|
25.66MHz
|
20.09MHz
|
|
% BW
|
12.18%
|
15.72%
|
12.18%
|
10.09%
|
|
Nominal IF Frequency |
|
||||
Design
Constraints
|
|||||
condition for bold number |
< IF
|
= IF
|
> IF
|
||
Delta |
0.08
|
-0.73
|
0.75
|
||
Test |
pass
|
pass
|
pass
|
||
Raise or lower cent freq by |
-0.73
|
MHz
|
|||
Inc or dec BW |
-0.83
|
MHz
|
|||
Cent adj for min BW |
210.34
|
MHz
|
|||
K vco |
30.18MHz/V
|

Figure 9. High-Q 210MHz high-band IF tank schematic.
Table 4. High-Q 210MHz High-Band IF Tank Design
Light grey indicates calculated values. |
Darker grey indicates user input. |
MAX2310 High-Band Tank Design and Tuning Range | |||||
Total Tank Capacitance vs. V tune | |||||
V tune
|
Total C | Ct (Nominal) |
Ct (Low) |
Ct (High) | |
0.5V
|
Ct high | 5.8856 | 5.5289 | 6.2425 | |
1.375V
|
Ct mid | 5.2487 | 4.9113 | 5.5858 | |
2.2V
|
Ct low | 4.8371 | 4.5156 | 5.1581 | |
Tank Components
|
|||||
C coup
|
15pF
|
0.75pF
|
5%
|
||
C cent
|
1.6pF
|
0.1pF
|
6%
|
||
C stray
|
0.77pF
|
||||
L
|
27
|
2.00%
|
|||
C int
|
0.959
|
10.00%
|
|||
Parasitics and Pads (C stray) | |||||
Due to Q |
C L
|
0.17pF
|
|||
Ind. pad |
C Lp
|
1.13pF
|
|||
Due to || |
C diff
|
0.036pF
|
|||
Var. pad |
C vp
|
0.82pF
|
|||
Varactor Specs | |||||
Alpha SMV1763-079 | |||||
Cjo |
8.2pF
|
Varactor Tolerance
|
|||
Vj |
15V
|
0.5V
|
7.50%
|
||
M |
9.5
|
1.5V
|
9.50%
|
||
Cp |
0.67pF
|
2.5V
|
11.50%
|
||
Rs |
0.5Ω
|
Reactance
|
|||
Ls |
0.8nH
|
X Ls
|
2.11 | ||
Freq |
420.00MHz
|
||||
Nominal Varactor |
X
c
|
Net
Cap
|
|||
Cv high
|
6.67523pF
|
-56.7681
|
6.933064pF
|
||
Cv mid
|
4.23417pF
|
-89.4958
|
4.336464pF
|
||
Cv low
|
2.904398pF
|
-130.471
|
2.952167pF
|
||
Negative Tol Varactor (Low Capacitance) | |||||
Cv high
|
6.174588pF
|
-61.3709
|
6.39456pF
|
||
Cv mid
|
3.831924pF
|
-98.8904
|
3.915514pF
|
||
Cv low
|
2.570392pF
|
-147.425
|
2.607736pF
|
||
Positive Tol Varactor (High Capacitance) | |||||
Cv high
|
7.175873pF
|
-52.8076
|
7.474698pF
|
||
Cv mid
|
4.636416pF
|
-81.7313
|
4.759352pF
|
||
Cv low
|
3.238404pF
|
-117.015
|
3.297904pF
|
||
Nominal LO (Nom) Range |
Low Tol IF (High) Range |
Nominal IF (Nom) Range |
High Tol IF (Low) Range |
||
F low
|
399.25MHz
|
208.05MHz
|
199.62MHz
|
191.92MHz
|
|
F mid
|
422.78MHz
|
220.75MHz
|
211.39MHz
|
202.89MHz
|
|
F high
|
440.40MHz
|
230.22MHz
|
220.20MHz
|
211.14MHz
|
|
BW
|
41.15MHz
|
22.16MHz
|
20.58MHz
|
19.21MHz
|
|
% BW
|
9.73%
|
10.04%
|
9.73%
|
9.47%
|
|
Nominal IF Frequency |
|
||||
Design
Constraints
|
|||||
Condition for bold number |
< IF
|
= IF
|
> IF
|
||
Delta |
1.95
|
-1.39
|
1.14
|
||
Test |
pass
|
pass
|
pass
|
||
Raise or lower cent freq by |
-1.39
|
MHz
|
|||
Inc or dec BW |
-3.08
|
MHz
|
|||
Cent adj for min BW |
209.60
|
MHz
|
|||
K vco |
24.21MHz/V
|
Appendix A
Figure 10. Varactor model.
Alpha Application Note AN1004 has additional information on varactor models. Varactor capacitance is defined in EQN7:
![]() |
EQN7
|
Alpha SMV1255-003 | Alpha SMV1763-079 |
Cjo = 82 pF | Cjo = 8.2 pF |
Vj =17 V | Vj =15 V |
M = 14 | M = 9.5 |
Cp = 0 | Cp = 0.67 |
Rs = 1Ω | Rs = 0.5Ω |
Ls = 1.7 nH | Ls = 0.8 nH |
The series inductance of the varactor is taken into account by backing out the inductive reactance and calculating a new effective capacitance Cv:
![]() |
EQN8
|
Appendix B
Table 5. Cint vs. Frequency for the MAX2310 High-Band Tank
Frequency (MHz) | Cint (pF) | Frequency (MHz) (cont.) | Cint (pF) (cont.) |
100 | 0.708 | 360 | 0.949 |
110 | 0.759 | 370 | 0.955 |
120 | 0.800 | 380 | 0.954 |
130 | 0.809 | 390 | 0.954 |
140 | 0.839 | 400 | 0.954 |
150 | 0.822 | 410 | 0.955 |
160 | 0.860 | 420 | 0.959 |
170 | 0.869 | 430 | 0.956 |
180 | 0.880 | 440 | 0.959 |
190 | 0.905 | 450 | 0.964 |
200 | 0.917 | 460 | 0.962 |
210 | 0.920 | 470 | 0.963 |
220 | 0.926 | 480 | 0.963 |
230 | 0.924 | 490 | 0.960 |
240 | 0.928 | 500 | 0.964 |
250 | 0.935 | 510 | 0.965 |
260 | 0.932 | 520 | 0.968 |
270 | 0.931 | 530 | 0.966 |
280 | 0.933 | 540 | 0.968 |
290 | 0.927 | 550 | 0.967 |
300 | 0.930 | 560 | 0.974 |
310 | 0.933 | 570 | 0.977 |
320 | 0.943 | 580 | 0.976 |
330 | 0.944 | 590 | 0.984 |
340 | 0.945 | 600 | 0.982 |
350 | 0.956 | - | - |

Figure 11. Cint vs. frequency for the MAX2310 high-band tank (sixth-order polynomial curve fit)
Table 6. Cint vs. Frequency for the MAX2310 Low-Band Tank
Frequency (MHz) | Cint (pF) | Frequency (MHz) (cont.) | Cint (pF) (cont.) |
100 | 0.550 | 360 | 1.001 |
110 | 0.649 | 370 | 0.982 |
120 | 0.701 | 380 | 0.992 |
130 | 0.764 | 390 | 1.001 |
140 | 0.762 | 400 | 0.985 |
150 | 0.851 | 410 | 0.980 |
160 | 0.838 | 420 | 0.986 |
170 | 0.902 | 430 | 0.992 |
180 | 0.876 | 440 | 0.994 |
190 | 0.907 | 450 | 1.001 |
200 | 0.913 | 460 | 1.003 |
210 | 0.919 | 470 | 1.007 |
220 | 0.945 | 480 | 0.992 |
230 | 0.952 | 490 | 1.010 |
240 | 0.965 | 500 | 1.004 |
250 | 0.951 | 510 | 1.011 |
260 | 0.954 | 520 | 1.022 |
270 | 0.974 | 530 | 1.019 |
280 | 0.980 | 540 | 1.044 |
290 | 0.973 | 550 | 1.026 |
300 | 0.982 | 560 | 1.041 |
310 | 0.970 | 570 | 1.038 |
320 | 0.982 | 580 | 1.032 |
330 | 0.991 | 590 | 1.036 |
340 | 0.993 | 600 | 1.025 |
350 | 0.991 | - | - |

Figure 12. Cint vs. frequency for the MAX2310 low-band tank (sixth-order polynomial curve fit).
References
- Chris O'Connor, Develop Trimless Voltage-Controlled Oscillators, Microwaves and RF, July1999.
- Wes Hayward, Radio Frequency Design, Chapter 7.
- Krauss, Bostian, Raab, Solid State Radio Engineering, Chapters 2, 3, 5.
- Alpha Industries Application Note AN1004.
- Coilcraft, RF Inductors Catalog, March 1998, p.131.
- Maxim, MAX2310/MAX2312/MAX2314/MAX2316 Data Sheet, Rev 0.
- Maxim, MAX2310/MAX2314 Evaluation Kit Data Sheet, Rev 0.
- Maxim, MAX2312/MAX2316 Evaluation Kit Data Sheet, Rev 0.
Related to this Article
Products
CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer
CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer
CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer
Product Categories